89 #ifndef ti_drivers_SDFatFS__include    90 #define ti_drivers_SDFatFS__include   100 #include <third_party/fatfs/ff.h>   101 #include <third_party/fatfs/diskio.h>   146 extern SDFatFS_Handle 
SDFatFS_open(uint_least8_t idx, uint_least8_t drive);
 struct SDFatFS_Config_ SDFatFS_Config
SDFatFS Global configuration. 
FATFS filesystem
Definition: SDFatFS.h:110
SD Global configuration. 
Definition: SD.h:298
SD_Handle sdHandle
Definition: SDFatFS.h:111
uint_fast32_t driveNum
Definition: SDFatFS.h:108
SDFatFS_Handle SDFatFS_open(uint_least8_t idx, uint_least8_t drive)
Function to open a SDFatFS instance on the specified drive. 
SDFatFS Global configuration. 
Definition: SDFatFS.h:131
void SDFatFS_close(SDFatFS_Handle handle)
Function to close a SDFatFS instance specified by the SDFatFS handle. 
void * object
Definition: SDFatFS.h:133
SDFatFS Object The application must not access any member variables of this structure! ...
Definition: SDFatFS.h:107
struct SDFatFS_Config_ * SDFatFS_Handle
A handle that is returned from a SDFatFS_open() call. 
Definition: SDFatFS.h:117
struct SDFatFS_Object_ SDFatFS_Object
SDFatFS Object The application must not access any member variables of this structure! ...
DSTATUS diskState
Definition: SDFatFS.h:109