188 #ifndef ti_display_Display__include   189 #define ti_display_Display__include   210 #define Display_Type_ANY      0xFFFFFFFF      211 #define Display_Type_INVALID  0x00000000      212 #define Display_Type_LCD      0x80000000      213 #define Display_Type_UART     0x40000000      214 #define Display_Type_LOG      0x20000000      215 #define Display_Type_ITM      0x10000000      216 #define Display_Type_HOST     0x08000000      217 #define Display_Type_ANSI     0x04000000      218 #define Display_Type_GRLIB    0x00100000      222 #define Display_MAXINDEX    15   241 #define DISPLAY_CMD_RESERVED            32   255 #define DISPLAY_STATUS_RESERVED        -32   270 #define DISPLAY_STATUS_SUCCESS         0   278 #define DISPLAY_STATUS_ERROR          -1   287 #define DISPLAY_STATUS_UNDEFINEDCMD   -2   308 #define DISPLAY_CMD_TRANSPORT_CLOSE  0   318 #define DISPLAY_CMD_TRANSPORT_OPEN   1   327 #define Display_clearLine(handle, n)    Display_clearLines(handle, n, 0)   328 #define Display_isIndex(i)              (i <= Display_MAXINDEX)   329 #define Display_isMetaType(i)           (i > Display_MAXINDEX)   331 #if !defined(Display_DISABLE_ALL) || (!Display_DISABLE_ALL)   334 #  define Display_init() \   338 #  define Display_open(id, params) \   339     Display_doOpen(id, params)   342 #  define Display_Params_init(params) \   343     Display_doParamsInit(params)   346 #  define Display_clear(handle) \   347     Display_doClear(handle)   350 #  define Display_clearLines(handle, fromLine, toLine) \   351     Display_doClearLines(handle, fromLine, toLine)   354 #  define Display_printf Display_doPrintf   357 #  define Display_print0(handle, line, col, fmt) \   358     Display_printf(handle, line, col, fmt)   361 #  define Display_print1(handle, line, col, fmt, a0) \   362     Display_printf(handle, line, col, fmt, a0)   365 #  define Display_print2(handle, line, col, fmt, a0, a1) \   366     Display_printf(handle, line, col, fmt, a0, a1)   369 #  define Display_print3(handle, line, col, fmt, a0, a1, a2) \   370     Display_printf(handle, line, col, fmt, a0, a1, a2)   373 #  define Display_print4(handle, line, col, fmt, a0, a1, a2, a3) \   374     Display_printf(handle, line, col, fmt, a0, a1, a2, a3)   377 #  define Display_print5(handle, line, col, fmt, a0, a1, a2, a3, a4) \   378     Display_printf(handle, line, col, fmt, a0, a1, a2, a3, a4)   381 #  define Display_getType(handle) \   382     Display_doGetType(handle)   385 #  define Display_control(handle, cmd, arg) \   386     Display_doControl(handle, cmd, arg)   389 #  define Display_close(handle) \   390     Display_doClose(handle)   392 #  define Display_init()   393 #  define Display_open(id, params)    NULL   394 #  define Display_Params_init(params)   395 #  define Display_clear(handle)   396 #  define Display_clearLines(handle, fromLine, toLine)   397 #  define Display_printf(handle, line, col, fmt, ...)   398 #  define Display_print0(handle, line, col, fmt)   399 #  define Display_print1(handle, line, col, fmt, a0)   400 #  define Display_print2(handle, line, col, fmt, a0, a1)   401 #  define Display_print3(handle, line, col, fmt, a0, a1, a2)   402 #  define Display_print4(handle, line, col, fmt, a0, a1, a2, a3)   403 #  define Display_print5(handle, line, col, fmt, a0, a1, a2, a3, a4)   404 #  define Display_getType(handle) Display_Type_INVALID   405 #  define Display_control(handle, cmd, arg)  NULL   406 #  define Display_close(handle)   682 #endif //ti_display_Display__include void Display_doClose(Display_Handle handle)
Closes selected Display implementations. 
Display_vprintfFxn vprintfFxn
Definition: Display.h:508
struct Display_Config * Display_Handle
A handle for specific Display implementations. 
Definition: Display.h:416
struct Display_Config Display_Config
Display Global configuration. 
void(* Display_clearLinesFxn)(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
A function pointer to a specific implementation of Display_clearLines(). 
Definition: Display.h:464
void Display_doParamsInit(Display_Params *params)
Initializes parameter structure with default parameters. 
void * object
Definition: Display.h:531
void Display_doInit(void)
Function to initializes the Display driver. 
Display_Handle(* Display_openFxn)(Display_Handle handle, Display_Params *params)
A function pointer to a specific implementation of Display_open(). 
Definition: Display.h:452
unsigned int(* Display_getTypeFxn)(void)
A function pointer to a specific implementation of Display_getType(). 
Definition: Display.h:495
void Display_doClear(Display_Handle handle)
Calls the clear fxn of all opened Display implementations. 
Display Parameters. 
Definition: Display.h:443
void const  * hwAttrs
Definition: Display.h:534
uint32_t Display_doGetType(Display_Handle handle)
Gets the type of display for the handle. 
Definition: Display.h:429
void Display_doControl(Display_Handle handle, unsigned int cmd, void *arg)
Function performs implementation specific features on a given Display_Handle. 
Display_clearFxn clearFxn
Definition: Display.h:506
Display_controlFxn controlFxn
Definition: Display.h:510
void(* Display_vprintfFxn)(Display_Handle handle, uint8_t line, uint8_t column, char *fmt, va_list va)
A function pointer to a specific implementation of Display_vprintf(). 
Definition: Display.h:472
void Display_doPrintf(Display_Handle handle, uint8_t line, uint8_t column, char *fmt,...)
Calls the output function of all opened Display implementations. 
void(* Display_clearFxn)(Display_Handle handle)
A function pointer to a specific implementation of Display_clear(). 
Definition: Display.h:458
Display_initFxn initFxn
Definition: Display.h:504
Definition: Display.h:431
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:502
Display_openFxn openFxn
Definition: Display.h:505
void(* Display_initFxn)(Display_Handle handle)
A function pointer to a specific implementation of Display_initFxn(). 
Definition: Display.h:422
Definition: Display.h:430
Display_getTypeFxn getTypeFxn
Definition: Display.h:511
void Display_doClearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
Calls the clearLines fxn of all opened Display implementations. 
struct Display_FxnTable Display_FxnTable
The definition of a Display function table that contains the required set of functions to control a s...
Display_LineClearMode lineClearMode
Definition: Display.h:445
Display_Handle Display_doOpen(uint32_t id, Display_Params *params)
Initialize all the selected Display implementations. 
Display Global configuration. 
Definition: Display.h:525
struct Display_Params Display_Params
Display Parameters. 
Display_FxnTable const  * fxnTablePtr
Definition: Display.h:528
int(* Display_controlFxn)(Display_Handle handle, unsigned int cmd, void *arg)
A function pointer to a driver specific implementation of Display_control(). 
Definition: Display.h:488
Display_closeFxn closeFxn
Definition: Display.h:509
Display_LineClearMode
How to treat existing elements on a line when writing text. 
Definition: Display.h:427
Definition: Display.h:432
Display_clearLinesFxn clearLinesFxn
Definition: Display.h:507
void(* Display_closeFxn)(Display_Handle)
A function pointer to a specific implementation of Display_close(). 
Definition: Display.h:482