367 #ifndef ti_drivers_crypto_CryptoCC26XX__include   368 #define ti_drivers_crypto_CryptoCC26XX__include   379 #include <ti/devices/DeviceFamily.h>   380 #include DeviceFamily_constructPath(driverlib/crypto.h)   410 #define CRYPTOCC26XX_TIMEOUT 20    412 #define CRYPTOCC26XX_STATUS_SUCCESS        0     413 #define CRYPTOCC26XX_STATUS_ERROR         -1     414 #define CRYPTOCC26XX_STATUS_UNDEFINEDCMD  -2     416 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT             0      417 #define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY    1      418 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT             2      419 #define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY    3      420 #define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT             4      421 #define CRYPTOCC26XX_OP_AES_ECB_DECRYPT             5      422 #define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT             6      423 #define CRYPTOCC26XX_OP_AES_CBC_DECRYPT             7      426 #define CRYPTOCC26XX_OP_AES_CCM                 CRYPTOCC26XX_OP_AES_CCM_ENCRYPT   427 #define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT         CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY   428 #define CRYPTOCC26XX_OP_AES_CCMINV              CRYPTOCC26XX_OP_AES_CCM_DECRYPT   429 #define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT      CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY   430 #define CRYPTOCC26XX_OP_AES_ECB                 CRYPTOCC26XX_OP_AES_ECB_ENCRYPT   431 #define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT         CRYPTOCC26XX_OP_AES_ECB_DECRYPT   434 #include <ti/drivers/dpl/HwiP.h>   435 #include <ti/drivers/dpl/SemaphoreP.h>   846 int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, 
const uint32_t *keySrc);
 int CryptoCC26XX_allocateKey(CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key...
CryptoCC26XX Transaction. 
Definition: CryptoCC26XX.h:520
CryptoCC26XX Global Configuration. 
Definition: CryptoCC26XX.h:735
CryptoCC26XX_Transaction * currentTransact
Definition: CryptoCC26XX.h:719
void CryptoCC26XX_Params_init(CryptoCC26XX_Params *params)
Function to initialize the CryptoCC26XX_Params struct to its defaults. 
CryptoCC26XX AES-CCM Transaction. 
Definition: CryptoCC26XX.h:576
struct CryptoCC26XX_Object CryptoCC26XX_Object
CryptoCC26XX Object. 
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:651
int CryptoCC26XX_close(CryptoCC26XX_Handle handle)
Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle. 
void * msgOut
Definition: CryptoCC26XX.h:606
struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
CryptoCC26XX AES-CCM Transaction. 
CryptoCC26XX_Transaction * tailPtr
Definition: CryptoCC26XX.h:723
CryptoCC26XX Parameters. 
Definition: CryptoCC26XX.h:500
uint8_t keyIndex
Definition: CryptoCC26XX.h:653
void * msgIn
Definition: CryptoCC26XX.h:639
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:577
Definition: CryptoCC26XX.h:486
SemaphoreP_Struct waitSem
Definition: CryptoCC26XX.h:731
HwiP_Struct hwi
Definition: CryptoCC26XX.h:729
SemaphoreP_Struct transSem
Definition: CryptoCC26XX.h:730
uint8_t CryptoCC26XX_Operation
CryptoCC26XX Operation Type. 
Definition: CryptoCC26XX.h:476
uint8_t fieldLength
Definition: CryptoCC26XX.h:612
Power notify object structure. 
Definition: Power.h:115
Definition: CryptoCC26XX.h:489
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:521
Definition: CryptoCC26XX.h:453
CryptoCC26XX_Transaction * headPtr
Definition: CryptoCC26XX.h:722
CryptoCC26XX_Operation opType
Definition: CryptoCC26XX.h:635
int CryptoCC26XX_loadKey(CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
Function that writes a given key into a key store. 
void * msgOut
Definition: CryptoCC26XX.h:655
uint8_t keyIndex
Definition: CryptoCC26XX.h:579
char * nonce
Definition: CryptoCC26XX.h:582
void * msgOut
Definition: CryptoCC26XX.h:640
struct CryptoCC26XX_Config CryptoCC26XX_Config
CryptoCC26XX Global Configuration. 
void CryptoCC26XX_Transac_init(CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
Function to initialize the CryptoCC26XX_Transaction struct to its defaults. 
int CryptoCC26XX_releaseKey(CryptoCC26XX_Handle handle, int *keyIndex)
Function that releases the specified CryptoCC26XX Key. 
Definition: CryptoCC26XX.h:492
char * header
Definition: CryptoCC26XX.h:605
CryptoCC26XX Hardware Attributes. 
Definition: CryptoCC26XX.h:687
Power_NotifyObj cryptoNotiObj
Definition: CryptoCC26XX.h:726
int openCnt
Definition: CryptoCC26XX.h:716
Definition: CryptoCC26XX.h:491
void const  * hwAttrs
Definition: CryptoCC26XX.h:740
uint16_t headerLength
Definition: CryptoCC26XX.h:625
Definition: CryptoCC26XX.h:459
uint16_t msgInLength
Definition: CryptoCC26XX.h:623
struct CryptoCC26XX_Params CryptoCC26XX_Params
CryptoCC26XX Parameters. 
struct CryptoCC26XX_Config * CryptoCC26XX_Handle
A handle that is returned from a CryptoCC26XX_open() call. 
Definition: CryptoCC26XX.h:440
void * msgIn
Definition: CryptoCC26XX.h:654
uint32_t timeout
Definition: CryptoCC26XX.h:717
Definition: CryptoCC26XX.h:493
CryptoCC26XX_Mode
CryptoCC26XX Mode Settings. 
Definition: CryptoCC26XX.h:448
CryptoCC26XX AES-ECB Transaction. 
Definition: CryptoCC26XX.h:650
char * msgIn
Definition: CryptoCC26XX.h:599
void CryptoCC26XX_init(void)
Function to initializes bios modules needed by CryptoCC26XX module. 
uint8_t intPriority
Crypto Peripheral's interrupt priority. 
Definition: CryptoCC26XX.h:706
int CryptoCC26XX_transact(CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
Function to do a Crypto operation (encryption or decryption) in blocking mode. 
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:636
CryptoCC26XX_KeyStore keyStore
Definition: CryptoCC26XX.h:718
uint8_t keyIndex
Definition: CryptoCC26XX.h:637
uint16_t msgInLength
Definition: CryptoCC26XX.h:641
int powerMngrId
Definition: CryptoCC26XX.h:691
void * object
Definition: CryptoCC26XX.h:737
Definition: CryptoCC26XX.h:494
Definition: CryptoCC26XX.h:488
uint8_t CryptoCC26XX_KeyStore
CryptoCC26XX Key. 
Definition: CryptoCC26XX.h:509
CryptoCC26XX_Handle CryptoCC26XX_open(unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
Function to initialize a given CryptoCC26XX peripheral specified by the particular index value...
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:652
void * nonce
Definition: CryptoCC26XX.h:638
CryptoCC26XX_KeyLocation
CryptoCC26XX Key Store Location. 
Definition: CryptoCC26XX.h:484
int intNum
Definition: CryptoCC26XX.h:693
struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
CryptoCC26XX Hardware Attributes. 
CryptoCC26XX_Mode mode
Definition: CryptoCC26XX.h:522
Definition: CryptoCC26XX.h:490
struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
CryptoCC26XX Transaction. 
uint32_t timeout
Definition: