Bluetooth SIG Developer Studio Plugin for TI
Table of Contents
Texas Instruments, Inc.
Bluetooth Developer Studio Plugin Readme
TI-BDS-PLUGIN Version 1.0.9 July 20th, 2017
Getting Started
NOTE: We recommend you follow the steps outlined in the SimpleLink Academy BDS Plugin Workshop to get started easily.
You will need Bluetooth Developer Studio in order to use this plugin. See CHANGELOG for information about implemented features, known issues, etc.
The files in the downloaded Texas Instruments -- Embedded Profiles
folder should be copied into: C:\Program Files (x86)\Bluetooth SIG\Bluetooth Developer Studio\Plugins\Texas Instruments -- Embedded Profiles\*.*
Open Bluetooth Developer Studio and create your profile. When you want to generate the code, click on TOOLS->GENERATE CODE. Note For best variable name generation, use spaces in your service and characteristic names, for examle “my cool service”, as the generated names will split on spaces.
The files that are created in the output folder selected in BDS are: Profile_Name_TI_cc2640r2sdk_M_mm/ — service_name.c
per service — service_name.h
per service — project_zero_bds.c
, using the generated services — log.txt
, replica of the BDS plugin log
For support and feedback, please visit www.ti.com/ble-forum.
Test output using TI SimpleLink CC2640R2 SDK 1.40
Required software:
- SimpleLink CC2640R2 SDK 1.40 from www.ti.com/ble-stack.
- IAR Embedded Workbench for ARM, or Code Composer Studio v7.2
Required extras for Project Zero:
- Find Project Zero on
dev.ti.com/tirex
or via Resource Explorer inside Code Composer Studio.
Using CCS
Project Zero
Either import the project into CCS Cloud IDE from Resource Explorer online or find the project in Resource Explorer inside CCS and import it there. Note that to import locally you must also make available offline the CC2640R2 SDK and SimpleLink Academy.
After importing, drag+drop
project_zero_bds.c
and the generated service source files directly from the BDS output directory into theApplication
folder and select ‘Copy files’.Right click on the original
project_zero.c
file in Project Explorer and clickExclude from build
. Also exclude from build the 3 services Project Zero has by default underPROFILES
in the IDE:led_service.c
,button_service.c
anddata_service.c
.Build and program
Custom parameters for TI plugin
Some functionality is added to the plugin on top of what’s available in the Bluetooth Developer Studio GUI. This is currently only utilized by the generated ProjectZero application file.
The purpose of these custom properties is to generate application code that utilize a characteristic in a specific way.
To use these, expand the properties of a Characteristic
in the BDS GUI and click on CUSTOM PROPERTIES
at the bottom of this view.
Property INBUTTON
This property can be used to generate debounce logic for a pin, and after debounce set the first byte of the characteristic value to the state of the pin.
Property INPIN
This property can be used to generate code that directly connects a pin interrupt to the SetParameter
API of the service, setting the first byte of the value to the state of the pin.
Property OUTPIN
This property can be used to generate code that will set the pin state when an over the air write is received for the selected characteristic. The first byte of the received data will be used to set the pin state.
Examples
Note that the value must correspond to a #define
which exists globally. This can be either from the board file like Board_LED0
or a generic IO reference like IOID_21
.
Property | Value |
---|---|
OUTPIN | Board_LED0 |
INBUTTON | Board_BUTTON0 |
INPIN | IOID_02 |
See also the BDS example project for Project Zero that is bundled with this plugin.
Bluetooth Developer Studio Plugin downloads
Title | Description | Size |
---|---|---|
TI-BDS-PLUGIN 1.0.9 | Plugin compatible with TI CC2640R2 SDK v1.40 | 188kb |