14.3. AprilTag ROS Node

AprilTag is a robust visual fiducial system used in various applications such as Robotics, localization, and SLAM. For more information on AprilTag, it is recommended to visit https://april.eecs.umich.edu/software/apriltag and http://wiki.ros.org/apriltag_ros.
This document describes how to install and run the AprilTag ROS node in the ROS 1 Docker container. It consists of two steps:
Install the AprilTag library from source.
Run the AprilTag ROS node with a monochrome camera.
14.3.1. Install AprilTag Library
Launch the Docker image. For setting up the ROS 1 environment on J7, please follow Docker Setup for ROS 1.
root@am6x-sk:~/j7ros_home# ./docker_run_ros1.sh
Before launching
docker_run_ros1.sh, remove ‘–rm’ flag indocker runcommand in it since we need to commit the changes after installing AprilTag library.Clone AprilTag.
root@j7-docker:~/j7ros_home/ros_ws$ export APRILTAG_SOURCE_DIR=$HOME/j7ros_home/apriltag root@j7-docker:~/j7ros_home/ros_ws$ git clone https://github.com/AprilRobotics/apriltag.git $APRILTAG_SOURCE_DIR
Build and Install AprilTag library.
root@j7-docker:~/j7ros_home/ros_ws$ cd $APRILTAG_SOURCE_DIR root@j7-docker:~/j7ros_home/ros_ws$ cmake -B build -DCMAKE_BUILD_TYPE=Release root@j7-docker:~/j7ros_home/ros_ws$ cmake --build build --target install
Exit docker and update an image from the container’s changes.
# Check container_id root@am6x-sk:~/j7ros_home# docker ps --all # Update Docker image root@am6x-sk:~/j7ros_home# docker commit container_id j7-ros-noetic:8.6
14.3.2. Run April ROS Node
Launch the Docker image.
root@am6x-sk:~/j7ros_home# ./docker_run_ros1.sh
Clone and build the AprilTag ROS package.
root@j7-docker:~/j7ros_home/ros_ws$ mkdir src root@j7-docker:~/j7ros_home/ros_ws$ git clone git clone https://github.com/AprilRobotics/apriltag_ros.git src/apriltag_ros root@j7-docker:~/j7ros_home/ros_ws$ catkin_make --source src/apriltag_ros
Launch the AprilTag ROS node.
root@j7-docker:~/j7ros_home/ros_ws$ source devel/setup.bash root@j7-docker:~/j7ros_home/ros_ws$ roslaunch apriltag_ros continuous_detection.launch
Note that
tags.yamlandsettings.yamlcan be configurable for tag definition and tag detection algorithm, respectively. A various types of AprilTags can be downloaded from https://github.com/AprilRobotics/apriltag-imgs.Launch USB camera.
Connect a USB camera to the SK board. Logitech C920 camera is used for test. Since AprilTag ROS node does not support YUV422 format, we update the following line of
mono_capture.launchunder/opt/robotics_sdk/ros1/drivers/mono_capture/launch:<arg name="encoding" default="bgr8"/>
Then launch the camera as follows:
root@j7-docker:~/j7ros_home/ros_ws$ source devel/setup.bash root@j7-docker:~/j7ros_home/ros_ws$ roslaunch mono_capture mono_capture.launch
As shown in Figure 1, we can visualize the AprilTag detection outputs along with their poses with respect to the camera using RViz on PC.