Vision Object Detection with 3D Spatial Information
This ROS node processes the outputs from ti_vision_cnn (vision CNN for object detection) and ti_sde (stereo vision processing), and does the following operations:
For each of 2D bounding boxes detected by the object detection CNN node, this node extracts spatial information from the stereo disparity map, and attaches the XYZ coordinates (for the center portion of the bounding box).
To provide more spatial information, this node scans the stereo disparity map horizontally, and applies filtering, converts and publishes XYZ point-cloud data. This point-cloud data provides spatial information for potential obstacles that the CNN object detection model may not able to detect (e.g, wall or structure of buildings).
Demo: 2D Object Detection with XYZ Information
This demo takes stereo camera raw images either from ROSBAG file or live ZED camera with zed_capture node, does stereo vision processing in ti_sde node, does CNN 2D object detection (with YOLO, SSD, or any other detection model of choice from the Edge AI model zoo) in ti_vision_cnn node, followed by ti_objdet_range (this node) taking the outputs from the two nodes and does two operations described above. Figure 1 shows the block diagram of the demo with ZED camera.
This demo runs currently in ROS 1 only. Launch the following launch file in the TDA4 ROS1 Docker container. [TDA4] With stereo camera images from ROSBAG file:
roslaunch ti_objdet_range bag_objdet_range.launch
With a live ZED stereo camera as input:
roslaunch ti_objdet_range zed_objdet_range.launch zed_sn:=SNxxxxx
[Visualization on Ubuntu PC] Launch the following launch file in the remote PC ROS1 Docker container.
roslaunch ti_viz_nodes rviz_objdet_range.launch
Launch File Parameters
| Parameter | Description | Value |
|---|---|---|
| disparity_topic | Input topic name for the stereo disparity map (output topic from ti_sed) |
string |
| vision_cnn_tensor_topic | Input topic name for the vision CNN tensor (output topic from ti_vision_cnn) |
string |
| camera_info_topic | Input topic name for camera_info | string |
| output_topic | Output topic name for bounding boxes with XYZ spatial information attached | string |
| camera_baseline | Baseline (in m) of the stereo camera | float |
| band_height | Band height (in pixels). A horizontal band with height of band_height around the vertical center of each bounding box is defined for extracting spatial info for each bounding box |
int |
| confidenceTh | Confidence threshold value. Only disparity pixels are used that has confidence > confidenceTh |
0,1,..., or 7 |
| disparity_filter | Filtering method applied to disparity pixels in the horizontal band | 0 (max), 1 (median), 2 (average) |
Following parameters are for horizontal scan point-cloud:
| Parameter | Description | Value |
|---|---|---|
| pcl_topic | Output topic name for point-cloud data generated by horizontally scanning the disparity map | string |
| pcl_frame | frame_id for pcl_topic |
string |
| disparity_width | Width (in pixels) of the input disparity map | int |
| pixels_to_exclude | Number of pixels to exclude in the right side of the disparity map | int |
| patch_size | Patches (patch_size x patch_size in pixels) are defined along with next two parameters for extracting XYZ information. Filtering is applied to the patches |
int |
| patch_stride | Stride (in pixels) for the patches when horizontally scanning the disparity map | int |
| patch_row_to_use | This determines where to place the patches vertically. Patches are defined in patch_size rows from row patch_row_to_use x patch_size |
int |
| pcl_disparity_filter | Filtering method applied to disparity pixels in a patch | 0 (max), 1 (median), 2 (average) |
| valid_pixel_ratio_th | Publish XYZ point only for patches in which the ratio of valid disparity pixels (defined by confidenceTh) is larger than valid_pixel_ratio_th. |
float |