- Description:
- Computes the sobel image filter kernel over a 3x3 window of imput image, for each pixel.
- Method:
- Produces only the X output plane in a single pass through the image. The sobel X operator is defined as:
| -1 0 +1 |
Gx = | -2 0 +2 |
| -1 0 +1 |
- Parameters
-
| [in] | src[] | Pointer to array containing input image (UQ8.0) |
| [in] | src_addr[] | Pointer to structure containing dimensional information of src |
| [out] | dst[] | Pointer to array containing output image (SQ15.0) |
| [in] | dst_addr[] | Pointer to structure containing dimensional information of dst |
- Assumptions:
- I/O buffer pointers are assumed to be not aliased.
- Output height should be == (Input height - 2)
- Output width should be == (Input width - 2) OR (Input width)
- Performance Considerations:
- For best performance, the following parameter settings are recommended:
- Set output width values to a multiple of 8
- Set widths equal to each other and equal to strides (allows processing over whole image in single loop)
- If both x and y gradients are needed instead of only X, one should use VXLIB_sobel_3x3_i8u_o16s_o16s.