Functions
VXLIB_fastCornersScore_i8u

Functions

VXLIB_STATUS VXLIB_fastCornersScore_i8u (const uint8_t src[], const VXLIB_bufParams2D_t *src_addr, const uint32_t corners[], uint8_t strengths[], uint8_t strength_thresh, uint32_t num_corners, uint8_t scratch[], uint32_t scratch_size)
 
VXLIB_STATUS VXLIB_fastCornersScore_i8u_checkParams (const uint8_t src[], const VXLIB_bufParams2D_t *src_addr, const uint32_t corners[], const uint8_t strengths[], uint8_t strength_thresh, uint32_t num_corners, const uint8_t scratch[], uint32_t scratch_size)
 

Detailed Description

Function Documentation

◆ VXLIB_fastCornersScore_i8u()

VXLIB_STATUS VXLIB_fastCornersScore_i8u ( const uint8_t  src[],
const VXLIB_bufParams2D_t *  src_addr,
const uint32_t  corners[],
uint8_t  strengths[],
uint8_t  strength_thresh,
uint32_t  num_corners,
uint8_t  scratch[],
uint32_t  scratch_size 
)
Description:
Computes the FAST9 strenghts for each corner in the corner list.
Method:
FAST9 algorithm.
Parameters
[in]src[]Pointer to array containing input image (UQ8.0)
[in]src_addr[]Pointer to structure containing dimensional information of src
[in]corners[]Pointer to array containing corner keypoint list (UQ32.0)
[out]strengths[]Pointer to array containing strength list corresponding to corners[] (UQ8.0)
[in]strength_threshThreshold on difference between intensity of the central pixel and pixels on the Bresenham's circlue of radius 3.
[in]num_cornersTotal number of corners in the corners list.
[in]scratch[]Pointer to scratch buffer of at least 463 bytes (UQ8.0)
[in]scratch_sizeSize of scratch buffer in number of bytes (for parameter checking)
Assumptions:
  • I/O buffer pointers are assumed to be not aliased.
  • Each 32-bit word in corners[] array is composed of 2 16-bit half words representing x and y coordinates, such that corners[i] = (y(i) << 16) | x(i);
  • The scratch buffer should be at least 463 bytes
Performance Considerations:
  • For best performance, the following parameter settings are recommended:
    • When the num_corners parameter is a multiple of 8.

◆ VXLIB_fastCornersScore_i8u_checkParams()

VXLIB_STATUS VXLIB_fastCornersScore_i8u_checkParams ( const uint8_t  src[],
const VXLIB_bufParams2D_t *  src_addr,
const uint32_t  corners[],
const uint8_t  strengths[],
uint8_t  strength_thresh,
uint32_t  num_corners,
const uint8_t  scratch[],
uint32_t  scratch_size 
)
Description:
Checks the parameters for programming errors for the VXLIB_fastCornersScore_i8u function.
Method:
The following checks are made:
  • There shall be no NULL pointers
  • The strides of the image shall be equal to or greater than the x dimension
  • The scratch_size shall be >= 463
Parameters
[in]src[]Pointer to array containing input image (UQ8.0)
[in]src_addr[]Pointer to structure containing dimensional information of src
[in]corners[]Pointer to array containing corner keypoint list (UQ32.0)
[out]strengths[]Pointer to array containing strength list corresponding to corners[] (UQ8.0)
[in]strength_threshThreshold on difference between intensity of the central pixel and pixels on the Bresenham's circlue of radius 3.
[in]num_cornersTotal number of corners in the corners list.
[in]scratch[]Pointer to scratch buffer (UQ8.0)
[in]scratch_sizeSize of scratch buffer in number of bytes (for parameter checking)

Copyright 2024, Texas Instruments Incorporated