- Description:
- Accumulates an input image into output image.
- Method:
- Accumulation is computed by using the following equation:
dst(x,y) = dst(x,y) + src(x,y)
- Parameters
-
[in] | src[] | Pointer to array containing first input image (UQ8.0) |
[in] | src_addr[] | Pointer to structure containing dimensional information of src |
[in,out] | dst[] | Pointer to array containing output image (SQ15.0) |
[in] | dst_addr[] | Pointer to structure containing dimensional information of dst |
- Assumptions:
- I/O buffer pointers are assumed to be not aliased.
- Performance Considerations:
- For best performance, the following parameter settings are recommended:
- Set widths equal to strides
- Align all pointers to 8 byte boundaries
- Set all stride values to a multiple of 8
- Set all width values to a multiple of 8