![]() |
TIOVX User Guide
|
The configuration data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More...
#include <hwa_vpac_msc.h>
Data Fields | |
| uint32_t | horz_coef_src |
| uint32_t | horz_coef_sel |
| uint32_t | vert_coef_src |
| uint32_t | vert_coef_sel |
The configuration data structure used by the TIVX_KERNEL_VPAC_MSC kernel.
Definition at line 316 of file hwa_vpac_msc.h.
| uint32_t tivx_vpac_msc_single_phase_params_t::horz_coef_src |
Single-phase horizontal filter coefficient source 0 : Use one of the dedicated single-phase coefficient sets 1 : Use one of the phases from the multi-phase coefficient set 0 (specified using 'horz_coef_sel')
Definition at line 322 of file hwa_vpac_msc.h.
| uint32_t tivx_vpac_msc_single_phase_params_t::horz_coef_sel |
Single-phase horizontal filter coefficient selection if (horz_coef_src == 0) Choose which single-phase coefficient set to use [Range (0-1)] else Choose which phase to use among multi-phase coefficient set 0 [Range (0-31)]
Definition at line 330 of file hwa_vpac_msc.h.
| uint32_t tivx_vpac_msc_single_phase_params_t::vert_coef_src |
Single-phase vertical filter coefficient source 0 : Use one of the dedicated single-phase coefficient sets 1 : Use one of the phases from the multi-phase coefficient set 0 (specified using 'vert_coef_sel')
Definition at line 336 of file hwa_vpac_msc.h.
| uint32_t tivx_vpac_msc_single_phase_params_t::vert_coef_sel |
Single-phase vertical filter coefficient selection if (vert_coef_src == 0) Choose which single-phase coefficient set to use [Range (0-1)] else Choose which phase to use among multi-phase coefficient set 0 [Range (0-31)]
Definition at line 344 of file hwa_vpac_msc.h.