TIOVX User Guide

The coefficients input data structure used by the TIVX_KERNEL_VPAC_MSC kernel. More...

#include <hwa_vpac_msc.h>

Data Fields

int32_t single_phase [TIVX_VPAC_MSC_MAX_SP_COEFF_SET][TIVX_VPAC_MSC_MAX_TAP]
 
int32_t multi_phase [TIVX_VPAC_MSC_MAX_MP_COEFF_SET][TIVX_VPAC_MSC_MAX_TAP *TIVX_VPAC_MSC_32_PHASE_COEFF]
 

Detailed Description

The coefficients input data structure used by the TIVX_KERNEL_VPAC_MSC kernel.

Definition at line 302 of file hwa_vpac_msc.h.

Field Documentation

◆ single_phase

int32_t tivx_vpac_msc_coefficients_t::single_phase[TIVX_VPAC_MSC_MAX_SP_COEFF_SET][TIVX_VPAC_MSC_MAX_TAP]

2 Sets of Single phase coefficient set 0, signed 10-bit

Definition at line 304 of file hwa_vpac_msc.h.

◆ multi_phase

int32_t tivx_vpac_msc_coefficients_t::multi_phase[TIVX_VPAC_MSC_MAX_MP_COEFF_SET][TIVX_VPAC_MSC_MAX_TAP *TIVX_VPAC_MSC_32_PHASE_COEFF]

4 Sets of Multi phase coefficient, signed 10-bit

Definition at line 307 of file hwa_vpac_msc.h.


The documentation for this struct was generated from the following file: