![]() |
TIOVX User Guide
|
Enumerations for VPAC VISS error events.
| #define TIVX_VPAC_VISS_RAWFE_AEW_PULSE_INTR (0x2U) |
H3A AEW interrupt
Definition at line 261 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_RAWFE_AF_PULSE_INTR (0x4U) |
H3A AF interrupt
Definition at line 263 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_RAWFE_H3A_PULSE_INTR (0x8U) |
H3A interrupt
Definition at line 265 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_RAWFE_H3A_BUF_OVRFLOW_PULSE_INTR (0x10U) |
H3A output buffer overflow
Definition at line 267 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_NSF4V_LINEMEM_CFG_ERR_INTR (0x20U) |
VBUSP diagnostic read access of, while NSF data using RAM for functional purpose
Definition at line 269 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_NSF4V_HBLANK_ERR_INTR (0x40U) |
Horzontal Blanking too short between lines
Definition at line 271 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_NSF4V_VBLANK_ERR_INTR (0x80U) |
Vertical Blanking too short between frames
Definition at line 273 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_GLBCE_CFG_ERR_INTR (0x100U) |
Either non-shadowed registers written or statastic memories are accessed during active window
Definition at line 275 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_GLBCE_FILT_START_INTR (0x200U) |
GLBCE started filtering. This interrupt is issued at the rising edge of filtering signal
Definition at line 277 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_GLBCE_FILT_DONE_INTR (0x400U) |
GLBCE ended filtering. This interrupt is issued at the falling edge of filtering signal
Definition at line 279 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_GLBCE_HSYNC_ERR_INTR (0x800U) |
Generated when delayed HS/HE signals does not match with derived signals from GLBCE core.
Definition at line 281 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_GLBCE_VSYNC_ERR_INTR (0x1000U) |
Generated when delayed VS/VE signals does not match with derived signals from GLBCE core
Definition at line 283 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_GLBCE_VP_ERR_INTR (0x2000U) |
This interrupt is issued, if there is a data input while filtering is high
Definition at line 285 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_FCFA_CFG_ERR_INTR (0x4000U) |
Either non-shadowed registers written or line memories are accessed during active window
Definition at line 287 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_FCC_CFG_ERR_INTR (0x8000U) |
Configuration access to registers/memories has corrupted functional operation. Configuration read or write memory acccess occurred during functional operation. Merged independent error sources at VISS. Refer to Section VISS Flexible Color Processing (FCP) for all sources.
Definition at line 292 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_FCC_OUTIF_OVF_ERR_INTR (0x10000U) |
FIFO overflow on FIFO for Y12 LSE I/F. Merged all FCC output overflow error sources at VISS. Refer to Section VISS Flexible Color Processing (FCP) for all sources.
Definition at line 295 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_FCC_HIST_READ_ERR_INTR (0x20000U) |
Host was not able to read the entire histogram mem between VS-VE window (triggered when the first access to histogram has been performed but the last has not been performed).
Definition at line 299 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_EE_CFG_ERR (0x40000U) |
Configuration happened to EE regions causing corruption during frame processing
Definition at line 301 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_EE_SYNCOVF_ERR (0x80000U) |
EE horizontal synchronization FIFO overflow interrupt
Definition at line 303 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_LSE_FR_DONE_EVT_INTR (0x100000U) |
LSE frame done interrupt
Definition at line 305 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_LSE_SL2_RD_ERR_INTR (0x200000U) |
Set whenever there is an error response on VBUSM read command for any input channel.
Definition at line 307 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_LSE_SL2_WR_ERR_INTR (0x400000U) |
Set whenever there is an error response on VBUSM write command for any output channel.
Definition at line 309 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_LSE_CAL_VP_ERR_INTR (0x800000U) |
Set whenever one of the following input frame errors is detected at VPORT_INPUT brief Output Frame Start (from VISS top level)
Definition at line 311 of file hwa_vpac_viss.h.
| #define TIVX_VPAC_VISS_WDTIMER_ERR (0x40000000U) |
Watchdog Timeout Error for VISS
Definition at line 327 of file hwa_vpac_viss.h.