![]() |
TIOVX User Guide
|
APIs for creating and managing user-defined data objects in OpenVX.
Defines | |
| #define | VX_TYPE_USER_DATA_OBJECT 0x816 |
| The object type enumeration for user data object. More... | |
Typedefs | |
| typedef struct _vx_user_data_object * | vx_user_data_object |
| The User Data Object. User Data Object is a strongly-typed container for other data structures. | |
Enumerations | |
| enum | vx_user_data_object_attribute_e { VX_USER_DATA_OBJECT_NAME = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_USER_DATA_OBJECT) + 0x0, VX_USER_DATA_OBJECT_SIZE = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_USER_DATA_OBJECT) + 0x1, VX_USER_DATA_OBJECT_VALID_SIZE = VX_ATTRIBUTE_BASE(VX_ID_KHRONOS, VX_TYPE_USER_DATA_OBJECT) + 0x2 } |
| The user data object attributes. More... | |
Functions | |
| VX_API_ENTRY vx_user_data_object VX_API_CALL | vxCreateUserDataObject (vx_context context, const vx_char *type_name, vx_size size, const void *ptr) |
| Creates a reference to a User Data Object. More... | |
| VX_API_ENTRY vx_user_data_object VX_API_CALL | vxCreateVirtualUserDataObject (vx_graph graph, const vx_char *type_name, vx_size size) |
| Creates an opaque reference to a virtual User Data Object with no direct user access. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxReleaseUserDataObject (vx_user_data_object *user_data_object) |
| Releases a reference of a User data object. The object may not be garbage collected until its total reference count is zero. After returning from this function the reference is zeroed. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxQueryUserDataObject (vx_user_data_object user_data_object, vx_enum attribute, void *ptr, vx_size size) |
| Queries the User data object for some specific information. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxSetUserDataObjectAttribute (vx_user_data_object user_data_object, vx_enum attribute, const void *ptr, vx_size size) |
| Sets an attribute in the User data object. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxCopyUserDataObject (vx_user_data_object user_data_object, vx_size offset, vx_size size, void *user_ptr, vx_enum usage, vx_enum user_mem_type) |
| Allows the application to copy a subset from/into a user data object. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxMapUserDataObject (vx_user_data_object user_data_object, vx_size offset, vx_size size, vx_map_id *map_id, void **ptr, vx_enum usage, vx_enum mem_type, vx_uint32 flags) |
| Allows the application to get direct access to a subset of the user data object. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | vxUnmapUserDataObject (vx_user_data_object user_data_object, vx_map_id map_id) |
| Unmap and commit potential changes to a user data object subset that was previously mapped. Unmapping a user data object subset invalidates the memory location from which the subset could be accessed by the application. Accessing this memory location after the unmap function completes is implementation specific. More... | |
| #define VX_TYPE_USER_DATA_OBJECT 0x816 |
The object type enumeration for user data object.
Definition at line 43 of file vx_khr_user_data_object.h.
The user data object attributes.
| Enumerator | |
|---|---|
| VX_USER_DATA_OBJECT_NAME | The type name of the user data object. Read-only. Use a |
| VX_USER_DATA_OBJECT_SIZE | The number of bytes in the user data object. Read-only. Use a |
| VX_USER_DATA_OBJECT_VALID_SIZE | The number of valid bytes in the user data object. Must be less than or equal to the value of VX_USER_DATA_OBJECT_SIZE. By default, upon object creation, this value is set to be equal to VX_USER_DATA_OBJECT_SIZE, and may be modified by either the application or a node connected to this object. Read-write. Use a vx_size parameter. |
Definition at line 48 of file vx_khr_user_data_object.h.
| VX_API_ENTRY vx_user_data_object VX_API_CALL vxCreateUserDataObject | ( | vx_context | context, |
| const vx_char * | type_name, | ||
| vx_size | size, | ||
| const void * | ptr | ||
| ) |
Creates a reference to a User Data Object.
User data objects can be used to pass a user kernel defined data structure or blob of memory as a parameter to a user kernel.
| [in] | context | The reference to the overall Context. |
| [in] | type_name | Pointer to the '\0' terminated string that identifies the type of object. The string is copied by the function so that it stays the property of the caller. The length of the string shall be lower than VX_MAX_REFERENCE_NAME bytes. The string passed here is what shall be returned when passing the VX_USER_DATA_OBJECT_NAME attribute enum to the vxQueryUserDataObject function. In the case where NULL is passed to type_name, then the query of the VX_USER_DATA_OBJECT_NAME attribute enum will return a single character '\0' string. |
| [in] | size | The number of bytes required to store this instance of the user data object. |
| [in] | ptr | The pointer to the initial value of the user data object. If NULL, then entire size bytes of the user data object is initialized to all 0s, otherwise, size bytes is copied into the object from ptr to initialize the object |
vx_user_data_object. Any possible errors preventing a successful creation should be checked using vxGetStatus. | VX_API_ENTRY vx_user_data_object VX_API_CALL vxCreateVirtualUserDataObject | ( | vx_graph | graph, |
| const vx_char * | type_name, | ||
| vx_size | size | ||
| ) |
Creates an opaque reference to a virtual User Data Object with no direct user access.
Virtual User Data Objects are useful when the User Data Object is used as internal graph edge. Virtual User Data Objects are scoped within the parent graph only.
| [in] | graph | The reference to the parent graph. |
| [in] | type_name | Pointer to the '\0' terminated string that identifies the type of object. The string is copied by the function so that it stays the property of the caller. The length of the string shall be lower than VX_MAX_REFERENCE_NAME bytes. The string passed here is what shall be returned when passing the VX_USER_DATA_OBJECT_NAME attribute enum to the vxQueryUserDataObject function. In the case where NULL is passed to type_name, then the query of the VX_USER_DATA_OBJECT_NAME attribute enum will return a single character '\0' string. |
| [in] | size | The number of bytes required to store this instance of the user data object. |
vx_user_data_object. Any possible errors preventing a successful creation should be checked using vxGetStatus. | VX_API_ENTRY vx_status VX_API_CALL vxReleaseUserDataObject | ( | vx_user_data_object * | user_data_object | ) |
Releases a reference of a User data object. The object may not be garbage collected until its total reference count is zero. After returning from this function the reference is zeroed.
| [in] | user_data_object | The pointer to the User Data Object to release. |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_ERROR_INVALID_REFERENCE | If user_data_object is not a vx_user_data_object. |
| VX_API_ENTRY vx_status VX_API_CALL vxQueryUserDataObject | ( | vx_user_data_object | user_data_object, |
| vx_enum | attribute, | ||
| void * | ptr, | ||
| vx_size | size | ||
| ) |
Queries the User data object for some specific information.
| [in] | user_data_object | The reference to the User data object. |
| [in] | attribute | The attribute to query. Use a vx_user_data_object_attribute_e. |
| [out] | ptr | The location at which to store the resulting value. |
| [in] | size | The size in bytes of the container to which ptr points. |
vx_status_e enumeration. | VX_SUCCESS | No errors; any other value indicates failure. |
| VX_ERROR_INVALID_REFERENCE | user_data_object is not a valid vx_user_data_object reference. |
| VX_ERROR_NOT_SUPPORTED | If the attribute is not a value supported on this implementation. |
| VX_ERROR_INVALID_PARAMETERS | If any of the other parameters are incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL vxSetUserDataObjectAttribute | ( | vx_user_data_object | user_data_object, |
| vx_enum | attribute, | ||
| const void * | ptr, | ||
| vx_size | size | ||
| ) |
Sets an attribute in the User data object.
| [in] | user_data_object | The reference to the User data object. |
| [in] | attribute | The attribute to set. Use a vx_user_data_object_attribute_e. |
| [in] | ptr | The pointer to the data to which to set the attribute. |
| [in] | size | The size in bytes of the data to which ptr points. |
vx_status_e enumeration. | VX_SUCCESS | No errors; any other value indicates failure. |
| VX_ERROR_INVALID_REFERENCE | user_data_object is not a valid vx_user_data_object reference. |
| VX_ERROR_NOT_SUPPORTED | If the attribute is not a value supported on this implementation. |
| VX_ERROR_INVALID_PARAMETERS | If any of the other parameters are incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL vxCopyUserDataObject | ( | vx_user_data_object | user_data_object, |
| vx_size | offset, | ||
| vx_size | size, | ||
| void * | user_ptr, | ||
| vx_enum | usage, | ||
| vx_enum | user_mem_type | ||
| ) |
Allows the application to copy a subset from/into a user data object.
| [in] | user_data_object | The reference to the user data object that is the source or the destination of the copy. |
| [in] | offset | The byte offset into the user data object to copy. |
| [in] | size | The number of bytes to copy. The size must be within the bounds of the user data object: 0 <= (offset + size) <= size of the user data object. If zero, then copy until the end of the object. |
| [in] | user_ptr | The address of the memory location where to store the requested data if the copy was requested in read mode, or from where to get the data to store into the user data object if the copy was requested in write mode. The accessible memory must be large enough to contain the specified size. |
| [in] | usage | This declares the effect of the copy with regard to the user data object using the vx_accessor_e enumeration. Only VX_READ_ONLY and VX_WRITE_ONLY are supported:
|
| [in] | user_mem_type | A vx_memory_type_e enumeration that specifies the memory type of the memory referenced by the user_addr. |
vx_status_e enumeration. | VX_ERROR_OPTIMIZED_AWAY | This is a reference to a virtual user data object that cannot be accessed by the application. |
| VX_ERROR_INVALID_REFERENCE | The user_data_object reference is not actually a user data object reference. |
| VX_ERROR_INVALID_PARAMETERS | Another parameter is incorrect. |
| VX_API_ENTRY vx_status VX_API_CALL vxMapUserDataObject | ( | vx_user_data_object | user_data_object, |
| vx_size | offset, | ||
| vx_size | size, | ||
| vx_map_id * | map_id, | ||
| void ** | ptr, | ||
| vx_enum | usage, | ||
| vx_enum | mem_type, | ||
| vx_uint32 | flags | ||
| ) |
Allows the application to get direct access to a subset of the user data object.
| [in] | user_data_object | The reference to the user data object that contains the subset to map. |
| [in] | offset | The byte offset into the user data object to map. |
| [in] | size | The number of bytes to map. The size must be within the bounds of the user data object: 0 <= (offset + size) <= size of the user data object. If zero, then map until the end of the object. |
| [out] | map_id | The address of a vx_map_id variable where the function returns a map identifier.
|
| [out] | ptr | The address of a pointer that the function sets to the address where the requested data can be accessed. The returned (*ptr) address is only valid between the call to the function and the corresponding call to vxUnmapUserDataObject. |
| [in] | usage | This declares the access mode for the user data object subset, using the vx_accessor_e enumeration.
|
| [in] | mem_type | A vx_memory_type_e enumeration that specifies the type of the memory where the user data object subset is requested to be mapped. |
| [in] | flags | An integer that allows passing options to the map operation. Use the vx_map_flag_e enumeration. |
vx_status_e enumeration. | VX_ERROR_OPTIMIZED_AWAY | This is a reference to a virtual user data object that cannot be accessed by the application. |
| VX_ERROR_INVALID_REFERENCE | The user_data_object reference is not actually a user data object reference. |
| VX_ERROR_INVALID_PARAMETERS | An other parameter is incorrect. |
vxUnmapUserDataObject with same (*map_id) value. | VX_API_ENTRY vx_status VX_API_CALL vxUnmapUserDataObject | ( | vx_user_data_object | user_data_object, |
| vx_map_id | map_id | ||
| ) |
Unmap and commit potential changes to a user data object subset that was previously mapped. Unmapping a user data object subset invalidates the memory location from which the subset could be accessed by the application. Accessing this memory location after the unmap function completes is implementation specific.
| [in] | user_data_object | The reference to the user data object to unmap. |
| [in] | map_id | The unique map identifier that was returned when calling vxMapUserDataObject . |
vx_status_e enumeration. | VX_ERROR_INVALID_REFERENCE | The user_data_object reference is not actually a user data object reference. |
| VX_ERROR_INVALID_PARAMETERS | Another parameter is incorrect. |
vxMapUserDataObject returning the same map_id value