![]() |
TIOVX User Guide
|
APIs for querying and manipulating the OpenVX graph.
Functions | |
| vx_status VX_API_CALL | tivxSetGraphPipelineDepth (vx_graph graph, vx_uint32 pipeline_depth) |
| Indicates to the implementation the depth of the graph pipeline. More... | |
| vx_node | tivxGraphGetNode (vx_graph graph, uint32_t idx) |
| This API is used to get a reference to a node within a graph at a given index within the graph. More... | |
| vx_status VX_API_CALL tivxSetGraphPipelineDepth | ( | vx_graph | graph, |
| vx_uint32 | pipeline_depth | ||
| ) |
Indicates to the implementation the depth of the graph pipeline.
| [in] | graph | Graph reference |
| [in] | pipeline_depth | Pipeline depth; Max value is (TIVX_GRAPH_MAX_PIPELINE_DEPTH-1) else it will return an error |
This API is used to get a reference to a node within a graph at a given index within the graph.
Use vxQueryGraph with attribute VX_GRAPH_NUMNODES to get number of nodes within a graph. This API can be called only on a verified graph. Node returned by this API is not reference counted and should not be released by the user.
| [in] | graph | graph handle |
| [in] | idx | node index, value from 0 .. value returned by vxQueryGraph(VX_GRAPH_NUMNODES) - 1 |