Perception Toolkit (PTk) Release Notes

BETA Version: 01.05.00.00


Contents

  1. Introduction
  2. Licensing
  3. Getting Started
  4. Documentation
  5. Device Support
  6. Validation Information
  7. Known Issues
  8. Technical Support
  9. Package Versioning


Introduction

The Texas Instruments Perception Toolkit (PTk) is a software package for accelerating sensing and perception capabilities, particularly for prototyping automotive and robotic applications.

PTk provides a cross-platform API that delivers identical behavior on both PC and embedded platforms.


Licensing

The licensing information of this library, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed in the table below under "Software Manifest".


Getting Started

Currently Unavailable


Documentation

Refer to following documentation for further details:

PTK User Guide Build instructions, API Guide [HTML]
Software Manifest Licenses, terms of use [HTML]

This beta release reflects on-going development of library components, algorithms, and example applications; as such, detailed documentation is somewhat limited.


Device Support

SoC HOST (OS) Target (OS) Test Plaform
J7 x86_64 (Linux) x86_64 (Linux) x86_64 Linux with Ubuntu 18.04
J7 A72 (Linux) C6x, A72 running Linux v4.19 J721e-evm, J721e-sk

Validation Information

This release was built and validated using the following tools:

Dependencies (NOT included in Processor SDK RTOS Automotive):


Known Issues

  1. None


Technical Support

For technical support and additional assistance, contact your local TI Field Application Engineer.


Package Versioning

Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.

Digit Meaning Description
1 (M=Major) Major revision Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered.
2 (m=minor) Minor revision Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set.
3 (p=patch) Patch number Incremented for all other source code changes. This include any packaging support code.
4 (b=build) Build number Incremented for each release delivery to CM. Reset for any change to M, m or p

Copyright 2022, Texas Instruments Incorporated