1.2. Release Notes - 11_00_00¶
1.2.1. Introduction¶
This release notes provides important information that will assist you in using the SDL software package for the J721E family of devices. This document provides the product information and known issues that are specific to the SDL software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
1.2.2. What’s New¶
Bug fixes
R5 ECC cache example for performing single error correction (SEC) for MCUR5F0 (In R5 ECC cache currently we are performing only error injection, error detection related things are still pending this will come in next release.)
CORE name has been changed from r5f to mcu1_0. This change is made to add support of multicore image for performing testing of R5f related ECC aggregators.
1.2.3. Supported Modules¶
SDL support for the following modules are available:
R5F PMU, MPU, RAT and VIM
ESM
PBIST
LBIST
POK
VTM
TOG
ECC
RTI
R5F CCM
DCC
MCRC
ROM CHECKSUM
Safety Examples for the following modules:
ESM
POK
VTM
TOG
DCC
RTI
ECC
BIST
ROM CHECKSUM
1.2.4. Upgrade and Compatibility¶
None
1.2.5. Supported Devices¶
Platform |
Supported Devices |
Supported EVMs |
|---|---|---|
J721E SR1.1 and SR2.0 |
Functional safety Devices:
DRA829
TDA4VM
|
DRA829Vx Evaluation Module
(DRA829VXEVM)
|
1.2.6. Fixed Defects¶
ID |
Summary |
Comments |
|---|---|---|
PROC_SDL-8249 |
SDL ECC error injection test for CSI ECC aggregators failure |
None. |
1.2.7. Open Defects¶
ID |
Summary |
Workaround |
|---|---|---|
PROC_SDL-6298 |
sdl_pok_test_app fails for SDL_POK_VMON_EXT_OV_ID instance |
None - This issue is under investigation. Root cause may be hardware configuration and/or pre-test sequence in the application. |
PROC_SDL-7421 |
ECC DED test is failing for certain RAM ID’s in SDL_ECC_MEMTYPE_MAIN_MSMSC_AGGR0. |
None - This issues is under investigation |
PROC_SDL-8258 |
SDL ECC error injection test for DSS ECC aggregators failure |
None - This issue is under investigation. Accessing some DSS ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-8943 |
SDL application does not work with safertos BUILD_OS_TYPE |
None - This issue is under investigation. |
PROC_SDL-8248 |
SDL ECC error injection test for PCIE ECC aggregators failure |
None - This issue is under investigation. Accessing some PCIE ECC Aggregator leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-8317 |
SDL PBIST test is failing for HC instance in PG 2.0 board |
None - This issues is under investigation |
1.2.8. Migration Information¶
None
1.2.9. Tool Chain Information¶
Component |
Version |
|---|---|
TI ARM R5F Clang Compiler tools |
3.2.2.LTS |