1.4. Release Notes - 01_04_00¶
1.4.1. Introduction¶
This release notes provides important information that will assist you in using the SDL software package for the J721E family of devices. This document provides the product information and known issues that are specific to the SDL software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
1.4.2. What’s New¶
Bug fixes
1.4.3. Supported Modules¶
SDL support for the following modules are available:
R5F PMU, MPU, RAT and VIM
ESM
PBIST
LBIST
POK
VTM
TOG
ECC
RTI
R5F CCM
DCC
MCRC
ROM CHECKSUM
Safety Examples for the following modules:
ESM
POK
VTM
TOG
DCC
RTI
ECC
BIST
ROM CHECKSUM
1.4.4. Upgrade and Compatibility¶
None
1.4.5. Supported Devices¶
Platform |
Supported Devices |
Supported EVMs |
|---|---|---|
J721E SR1.1 |
Functional safety Devices:
DRA829
TDA4VM
|
DRA829Vx Evaluation Module
(DRA829VXEVM)
|
1.4.6. Fixed Defects¶
ID |
Summary |
Comments |
|---|---|---|
PROC_SDL-7612 |
Remove ESM Error Pin Counter Value Register from static register read API |
None. |
PROC_SDL-7487 |
Duplicate macro definitoin SDL_IP_TOG_TOP_H_ in the SDL header files (STOG and MTOG) |
None. |
PROC_SDL-7402 |
Mismatch between function declaration and definition for SDL_PBIST_{start, startNeg} and SDL_LBIST_programConfig |
None. |
PROC_SDL-6348 |
SDL ECC error injection test fails for certain IPs in ecc_func_app SDL_ECC_MEMTYPE_MCU_CBASS_ECC_AGGR0 |
None. |
PROC_SDL-8316 |
SDL MCRC test is failing for MAIN NAVSS instance in release mode |
None. |
1.4.7. Open Defects¶
ID |
Summary |
Workaround |
|---|---|---|
PROC_SDL-6298 |
sdl_pok_test_app fails for SDL_POK_VMON_EXT_OV_ID instance |
None - This issue is under investigation. Root cause may be hardware configuration and/or pre-test sequence in the application. |
PROC_SDL-6349 |
SDL ECC error injection test fails for certain IPs in ecc_func_app SDL_CBASS_ECC_AGGR0 |
None - This issue is under investigation. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-6297 |
SDL ECC error injection test fails for certain IPs in ecc_func_app SDL_MAIN_RC_ECC_AGGR0 |
None - This issue is under investigation. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-7421 |
ECC DED test is failing for certain RAM ID’s in SDL_ECC_MEMTYPE_MAIN_MSMSC_AGGR0. |
None - This issues is under investigation |
PROC_SDL-8258 |
SDL ECC error injection test for DSS ECC aggregators failure |
None - This issue is under investigation. Accessing some DSS ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-8249 |
SDL ECC error injection test for CSI ECC aggregators failure |
None - This issue is under investigation. Accessing some CSI ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-8248 |
SDL ECC error injection test for PCIE ECC aggregators failure |
None - This issue is under investigation. Accessing some PCIE ECC Aggregator leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. |
PROC_SDL-8317 |
SDL PBIST test is failing for HC instance in PG 2.0 board |
None - This issues is under investigation |
PROC_SDL-8318 |
SDL POK is failing for SDL_POR_POKHV_OV_ID instance in PG2.0 board |
None - This issues is under investigation |
1.4.8. Migration Information¶
Dependency on C7X image is removed for compute cluster instances. PBIST example, pbist_test_app and sdl_pbist_test_app can be tested as standalone images.
1.4.9. Tool Chain Information¶
Component |
Version |
|---|---|
TI ARM R5F Clang Compiler tools |
3.2.2.LTS |