![]() |
PDK API Guide for J721E
|
Typedefs | |
typedef uint64_t(* | EnetTrace_TraceTsFunc) (void) |
Callback function used to get trace timestamps. More... | |
typedef void(* | EnetTrace_ExtTraceFunc) (uint32_t errCode) |
Callback function called to report errors. More... | |
Enumerations | |
enum | EnetTrace_TraceLevel { ENET_TRACE_NONE = 0U, ENET_TRACE_ERROR = 1U, ENET_TRACE_WARN = 2U, ENET_TRACE_INFO = 3U, ENET_TRACE_DEBUG = 4U, ENET_TRACE_VERBOSE = 5U } |
Enumerates the types of trace level. More... | |
Build-Time Trace Levels | |
Enet LLD supports two types of trace levels: build-time and runtime. Build time trace level is specified via ENET_CFG_TRACE_LEVEL and can be any of the levels in this group. The runtime trace level is set through Enet_setTraceLevel(). The runtime trace level should be set equal to or less than the build-time trace level. | |
#define | ENET_CFG_TRACE_LEVEL_NONE (0U) |
All traces disabled at build-time. More... | |
#define | ENET_CFG_TRACE_LEVEL_ERROR (1U) |
Build-time error level. More... | |
#define | ENET_CFG_TRACE_LEVEL_WARN (2U) |
Build-time warning level. More... | |
#define | ENET_CFG_TRACE_LEVEL_INFO (3U) |
Build-time information level. More... | |
#define | ENET_CFG_TRACE_LEVEL_DEBUG (4U) |
Build-time debug level. More... | |
#define | ENET_CFG_TRACE_LEVEL_VERBOSE (5U) |
Build-time verbose level. More... | |
Trace Formats | |
The following trace formats are supported:
Any of these trace formats can also be prefixed with a timestamp. | |
#define | ENET_CFG_TRACE_FORMAT_FUNC (0U) |
Trace prefix: "<func>: string". More... | |
#define | ENET_CFG_TRACE_FORMAT_FILE (1U) |
Trace prefix: "<file>: <line>: string". More... | |
#define | ENET_CFG_TRACE_FORMAT_FULL (2U) |
Trace prefix: "<file>: <line>: <func>: string". More... | |
#define | ENET_CFG_TRACE_FORMAT_FUNC_TS (3U) |
Trace prefix: "<timestamp>: <func>: string". More... | |
#define | ENET_CFG_TRACE_FORMAT_FILE_TS (4U) |
Trace prefix: "<timestamp>: <file>: <line>: string". More... | |
#define | ENET_CFG_TRACE_FORMAT_FULL_TS (5U) |
Trace prefix: "<timestamp>: <file>: <line>: <func>: string". More... | |
Enet Trace Configuration Parameters | |
The default values of the Enet Trace configuration parameters if none is provided via enet_cfg.h. | |
#define | ENET_CFG_TRACE_LEVEL (ENET_CFG_TRACE_LEVEL_INFO) |
Default trace level if none is set. More... | |
#define | ENET_CFG_TRACE_FORMAT (ENET_CFG_TRACE_FORMAT_FUNC) |
Default trace format if none is specified. More... | |
Enet Trace Error Code | ||||||||||||||||||||||
Enet Trace is capable of generating unique error codes from module id (Enet core, soc, per, mod, phy, etc), line number (where error code was reported) and status (error value reported by the module). The error code is a 32-bit value which is generated as follows:
Each individual source file in the locations shown in previous table is considered a module and is tagged with a unique | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_OFFSET (20U) | |||||||||||||||||||||
Module id offset in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MAJ_OFFSET (28U) | |||||||||||||||||||||
Module id (major number) offset in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MIN_OFFSET (20U) | |||||||||||||||||||||
Module id (minor number) offset in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_LINE_OFFSET (8U) | |||||||||||||||||||||
Line number offset in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_STATUS_OFFSET (0U) | |||||||||||||||||||||
Status offset in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MASK (0xFFF00000U) | |||||||||||||||||||||
Module id mask in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MAJ_MASK (0xF0000000U) | |||||||||||||||||||||
Module id (major number) mask in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MIN_MASK (0x0FF00000U) | |||||||||||||||||||||
Module id (minor number) mask in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_LINE_MASK (0x000FFF00U) | |||||||||||||||||||||
Line number mask in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_STATUS_MASK (0x000000FFU) | |||||||||||||||||||||
Status mask in the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD(x) | |||||||||||||||||||||
Helper macro to extract the module id from the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MAJ(x) | |||||||||||||||||||||
Helper macro to extract the module id (major number) from the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_MOD_MIN(x) | |||||||||||||||||||||
Helper macro to extract the module id (minor number) from the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_LINE(x) | |||||||||||||||||||||
Helper macro to extract the line number from the error code value. More... | ||||||||||||||||||||||
#define | ENET_TRACE_ERRCODE_STATUS(x) | |||||||||||||||||||||
Helper macro to extract the status value from the error code value. More... | ||||||||||||||||||||||
#define ENET_CFG_TRACE_LEVEL_NONE (0U) |
All traces disabled at build-time.
#define ENET_CFG_TRACE_LEVEL_ERROR (1U) |
Build-time error level.
#define ENET_CFG_TRACE_LEVEL_WARN (2U) |
Build-time warning level.
#define ENET_CFG_TRACE_LEVEL_INFO (3U) |
Build-time information level.
#define ENET_CFG_TRACE_LEVEL_DEBUG (4U) |
Build-time debug level.
#define ENET_CFG_TRACE_LEVEL_VERBOSE (5U) |
Build-time verbose level.
#define ENET_CFG_TRACE_FORMAT_FUNC (0U) |
Trace prefix: "<func>: string".
#define ENET_CFG_TRACE_FORMAT_FILE (1U) |
Trace prefix: "<file>: <line>: string".
#define ENET_CFG_TRACE_FORMAT_FULL (2U) |
Trace prefix: "<file>: <line>: <func>: string".
#define ENET_CFG_TRACE_FORMAT_FUNC_TS (3U) |
Trace prefix: "<timestamp>: <func>: string".
#define ENET_CFG_TRACE_FORMAT_FILE_TS (4U) |
Trace prefix: "<timestamp>: <file>: <line>: string".
#define ENET_CFG_TRACE_FORMAT_FULL_TS (5U) |
Trace prefix: "<timestamp>: <file>: <line>: <func>: string".
#define ENET_CFG_TRACE_LEVEL (ENET_CFG_TRACE_LEVEL_INFO) |
Default trace level if none is set.
#define ENET_CFG_TRACE_FORMAT (ENET_CFG_TRACE_FORMAT_FUNC) |
Default trace format if none is specified.
#define ENET_TRACE_ERRCODE_MOD_OFFSET (20U) |
Module id offset in the error code value.
#define ENET_TRACE_ERRCODE_MOD_MAJ_OFFSET (28U) |
Module id (major number) offset in the error code value.
#define ENET_TRACE_ERRCODE_MOD_MIN_OFFSET (20U) |
Module id (minor number) offset in the error code value.
#define ENET_TRACE_ERRCODE_LINE_OFFSET (8U) |
Line number offset in the error code value.
#define ENET_TRACE_ERRCODE_STATUS_OFFSET (0U) |
Status offset in the error code value.
#define ENET_TRACE_ERRCODE_MOD_MASK (0xFFF00000U) |
Module id mask in the error code value.
#define ENET_TRACE_ERRCODE_MOD_MAJ_MASK (0xF0000000U) |
Module id (major number) mask in the error code value.
#define ENET_TRACE_ERRCODE_MOD_MIN_MASK (0x0FF00000U) |
Module id (minor number) mask in the error code value.
#define ENET_TRACE_ERRCODE_LINE_MASK (0x000FFF00U) |
Line number mask in the error code value.
#define ENET_TRACE_ERRCODE_STATUS_MASK (0x000000FFU) |
Status mask in the error code value.
#define ENET_TRACE_ERRCODE_MOD | ( | x | ) |
Helper macro to extract the module id from the error code value.
#define ENET_TRACE_ERRCODE_MOD_MAJ | ( | x | ) |
Helper macro to extract the module id (major number) from the error code value.
#define ENET_TRACE_ERRCODE_MOD_MIN | ( | x | ) |
Helper macro to extract the module id (minor number) from the error code value.
#define ENET_TRACE_ERRCODE_LINE | ( | x | ) |
Helper macro to extract the line number from the error code value.
#define ENET_TRACE_ERRCODE_STATUS | ( | x | ) |
Helper macro to extract the status value from the error code value.
typedef uint64_t(* EnetTrace_TraceTsFunc) (void) |
Callback function used to get trace timestamps.
Callback function called when ENET_CFG_TRACE_FORMAT is set to ENET_CFG_TRACE_FORMAT_FUNC_TS, ENET_CFG_TRACE_FORMAT_FILE_TS or ENET_CFG_TRACE_FORMAT_FULL_TS.
The timestamp value must be in microseconds.
typedef void(* EnetTrace_ExtTraceFunc) (uint32_t errCode) |
Callback function called to report errors.
Callback function called by EnetTrace when Enet driver has reported an error. A unique 32-bit error code is passed to the callback, which encodes information about the module where error occurred, line of code and the status value.
Application can use the helper macros ENET_TRACE_ERRCODE_MOD, ENET_TRACE_ERRCODE_MOD_MAJ, ENET_TRACE_ERRCODE_MOD_MIN, ENET_TRACE_ERRCODE_LINE and ENET_TRACE_ERRCODE_STATUS to decode the error code.
enum EnetTrace_TraceLevel |
Enumerates the types of trace level.
Enumerator | |
---|---|
ENET_TRACE_NONE | All traces are disabled at runtime |
ENET_TRACE_ERROR | Error trace level |
ENET_TRACE_WARN | Warning trace level |
ENET_TRACE_INFO | Info trace level: enables only important informational messages for the user (i.e. PHY link is up or down, NIMU layer is ready, etc). The amount of info logs is not invasive in nature so this trace level may be enabled by applications at init time. |
ENET_TRACE_DEBUG | Debug trace level: enables further information messages about operations taking place in the driver (i.e. a module is being opened, PHY auto-negotiation is started, etc). The debug level should be enabled by the user on a need basis (i.e. for debugging or tracing execution flow, etc) as the number of messages will increase considerably with respect to ENET_TRACE_INFO level. This trace level can be enabled at runtime only in 'debug' builds. |
ENET_TRACE_VERBOSE | Verbose trace level: enables even further messages about operations taking place in the driver (i.e. PHY state transitions, DMA transfer completion, etc) that are periodic in nature or simply happen very often during normal execution. The amount of messages will increase drastically when the verbose level is enabled, so it's recommended to set it only if really needed. This trace level can be enabled at runtime only in 'debug' builds. |