![]() |
PDK API Guide for J721E
|
Data Structures | |
struct | EnetRm_NodeInfo |
Enet RM node information. More... | |
struct | EnetRm_ResourceInfo |
Enet RM resource information. More... | |
struct | EnetRm_ResPrms |
Enet RM resource parameters. More... | |
struct | EnetRm_IoctlPermissionEntry |
Enet RM IOCTL permission entry. More... | |
struct | EnetRm_IoctlPermissionTable |
Enet RM IOCTL permission table. More... | |
struct | EnetRm_MacAddressPool |
Enet RM MAC address pool. More... | |
struct | EnetRm_AllocRxFlowInArgs |
Input args for ENET_RM_IOCTL_ALLOC_RX_FLOW command. More... | |
struct | EnetRm_AllocRxFlow |
Output args for ENET_RM_IOCTL_ALLOC_RX_FLOW command. More... | |
struct | EnetRm_AllocTxChInArgs |
Input args for ENET_RM_IOCTL_ALLOC_TX_CH_PEERID command. More... | |
struct | EnetRm_AllocMacAddrOutArgs |
Input args for ENET_RM_IOCTL_ALLOC_MAC_ADDR command. More... | |
struct | EnetRm_FreeTxChInArgs |
Input args for ENET_RM_IOCTL_FREE_TX_CH_PEERID command. More... | |
struct | EnetRm_FreeRxFlowInArgs |
Input args for ENET_RM_IOCTL_FREE_RX_FLOW command. More... | |
struct | EnetRm_FreeMacAddrInArgs |
Input args for ENET_RM_IOCTL_FREE_MAC_ADDR command. More... | |
struct | EnetRm_ResCfg |
Resource manager configuration parameters. More... | |
struct | EnetRm_ValidatePermissionInArgs |
Input args for ENET_RM_IOCTL_VALIDATE_PERMISSION command. More... | |
struct | EnetRm_AllocInternalRxFlowInArgs |
Input args for ENET_RM_IOCTL_INTERNAL_ALLOC_RX_FLOW command. More... | |
struct | EnetRm_FreeInternalRxFlowInArgs |
Input args for ENET_RM_IOCTL_FREE_RX_FLOW command. More... | |
struct | EnetRm_Cfg |
Enet RM configuration parameters. More... | |
struct | EnetRm_ResEntry_t |
Resource manager entry. More... | |
struct | EnetRm_CoreResInfo_t |
Resources of a given core. More... | |
struct | EnetRm_CoreResTbl_t |
Resource table of all cores. More... | |
struct | EnetRm_TxChObj |
TX resources. More... | |
struct | EnetRm_RxFlowIdxObj |
RX resources. More... | |
struct | EnetRm_MacAddressObj |
MAC address resources. More... | |
struct | EnetRm_CoreAttachInfo |
Information about attached cores. More... | |
struct | EnetRm_Obj |
Enet Resource Manager driver object. More... | |
Functions | |
int32_t | EnetRm_open (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize) |
Open and initialize Enet RM module. More... | |
int32_t | EnetRm_rejoin (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId) |
Rejoin Enet RM module for a running peripheral. More... | |
int32_t | EnetRm_ioctl (EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms) |
Run an IOCTL operation on Enet RM. More... | |
void | EnetRm_close (EnetMod_Handle hMod) |
Close Enet RM module. More... | |
Typedefs | |
typedef EnetRm_FreeRxFlowInArgs | EnetRm_ValidateRxFlowInArgs |
Input args for ENET_RM_IOCTL_VALIDATE_RX_FLOW command. More... | |
typedef EnetRm_Obj * | EnetRm_Handle |
Enet RM module handle. More... | |
Macros | |
#define | ENET_RM_PUBLIC_IOCTL(x) |
Helper macro to create IOCTL commands for Enet RM module. More... | |
#define | ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX (16U) |
Maximum number of entries for IOCTL permission. More... | |
#define | ENET_RM_NUM_MACADDR_MAX (10U) |
Maximum number of macaddress to be managed by RM. More... | |
#define | ENET_RM_NUM_RXCHAN_MAX (1U) |
Maximum number of RX channels (i.e. sets of flows) More... | |
#define | ENET_RM_PRIVATE_IOCTL(x) |
Helper macro to create private IOCTL commands for Enet RM module. More... | |
Resource Manager Error Codes | |
#define | ENET_RM_TXCHNUM_INVALID (0xABCDABCDU) |
Enet RM invalid TX channel number. More... | |
#define | ENET_RM_RXFLOWIDX_INVALID (0xABCDABCDU) |
Enet RM invalid RX flow id. More... | |
#define | ENET_RM_UNDEFINED_NODEID (0xABCDABCDU) |
Enet RM undefined node id. More... | |
#define | ENET_RM_INVALIDCORE (0x5562AEFEU) |
Enet RM invalid core. More... | |
#define ENET_RM_PUBLIC_IOCTL | ( | x | ) |
Helper macro to create IOCTL commands for Enet RM module.
#define ENET_RM_TXCHNUM_INVALID (0xABCDABCDU) |
Enet RM invalid TX channel number.
#define ENET_RM_RXFLOWIDX_INVALID (0xABCDABCDU) |
Enet RM invalid RX flow id.
#define ENET_RM_UNDEFINED_NODEID (0xABCDABCDU) |
Enet RM undefined node id.
#define ENET_RM_INVALIDCORE (0x5562AEFEU) |
Enet RM invalid core.
#define ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX (16U) |
Maximum number of entries for IOCTL permission.
#define ENET_RM_NUM_MACADDR_MAX (10U) |
Maximum number of macaddress to be managed by RM.
#define ENET_RM_NUM_RXCHAN_MAX (1U) |
Maximum number of RX channels (i.e. sets of flows)
#define ENET_RM_PRIVATE_IOCTL | ( | x | ) |
Helper macro to create private IOCTL commands for Enet RM module.
Input args for ENET_RM_IOCTL_VALIDATE_RX_FLOW command.
typedef EnetRm_Obj* EnetRm_Handle |
Enet RM module handle.
enum EnetRm_Ioctls |
Enet RM IOCTL commands.
Enumerator | |
---|---|
ENET_RM_IOCTL_ALLOC_MAC_ADDR | Alloc MAC address. IOCTL parameters:
|
ENET_RM_IOCTL_FREE_MAC_ADDR | Free MAC address. IOCTL parameters:
|
ENET_RM_IOCTL_ALLOC_RX_FLOW | Alloc RX flow. IOCTL parameters:
|
ENET_RM_IOCTL_FREE_RX_FLOW | Free RX flow. IOCTL parameters:
|
ENET_RM_IOCTL_ALLOC_TX_CH_PEERID | Alloc TX channel peer id. IOCTL parameters:
|
ENET_RM_IOCTL_FREE_TX_CH_PEERID | Free TX channel peer id. IOCTL parameters:
|
enum EnetRm_TxCh |
RM tx channel.
This enum holds the number of tx channel.
enum EnetRm_NodeType |
enum EnetRm_PrivIoctls |
Enet RM private IOCTL commands.
Enumerator | |
---|---|
ENET_RM_IOCTL_VALIDATE_PERMISSION | Validate IOCTL permission. IOCTL parameters:
|
ENET_RM_IOCTL_ATTACH | Attach core. IOCTL parameters:
|
ENET_RM_IOCTL_DETACH | Detach core. IOCTL parameters:
|
ENET_RM_IOCTL_INTERNAL_ALLOC_RX_FLOW | Internal RX flow allocation. IOCTL parameters:
|
ENET_RM_IOCTL_INTERNAL_FREE_RX_FLOW | Internal RX flow free. IOCTL parameters:
|
ENET_RM_IOCTL_VALIDATE_RX_FLOW | Validate RX flow is allocated resource and is from a attached core. IOCTL parameters:
|
int32_t EnetRm_open | ( | EnetMod_Handle | hMod, |
Enet_Type | enetType, | ||
uint32_t | instId, | ||
const void * | cfg, | ||
uint32_t | cfgSize | ||
) |
Open and initialize Enet RM module.
hMod | Enet Module handle |
enetType | Enet Peripheral type |
instId | Enet Peripheral instance id |
cfg | Configuration parameters |
cfgSize | Size of the configuration parameters |
int32_t EnetRm_rejoin | ( | EnetMod_Handle | hMod, |
Enet_Type | enetType, | ||
uint32_t | instId | ||
) |
Rejoin Enet RM module for a running peripheral.
hMod | Enet Module handle |
enetType | Enet Peripheral type |
instId | Enet Peripheral instance id |
int32_t EnetRm_ioctl | ( | EnetMod_Handle | hMod, |
uint32_t | cmd, | ||
Enet_IoctlPrms * | prms | ||
) |
Run an IOCTL operation on Enet RM.
hMod | Enet Module handle |
cmd | IOCTL command Id |
prms | IOCTL parameters |
void EnetRm_close | ( | EnetMod_Handle | hMod | ) |
Close Enet RM module.
hMod | Enet Module handle |