PDK API Guide for J721E
SPI Driver API

Introduction

SPI driver interface

Files

file  SPI.h
 SPI driver interface.
 

Data Structures

struct  SPI_Transaction
 A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK. More...
 
struct  SPI_Params
 SPI Parameters. More...
 
struct  SPI_FxnTable
 The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation. More...
 
struct  SPI_Config
 SPI Global configuration. More...
 
struct  OSPI_Transaction
 A SPI_Transaction data structure is used with OSPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK. More...
 
struct  OSPI_Params
 OSPI Parameters. More...
 
struct  OSPI_FxnTable
 The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation. More...
 
struct  OSPI_Config
 OSPI Global configuration. More...
 

Functions

void SPI_close (SPI_Handle handle)
 Function to close a SPI peripheral specified by the SPI handle. More...
 
int32_t SPI_control (SPI_Handle handle, uint32_t cmd, void *arg)
 Function performs implementation specific features on a given SPI_Handle. More...
 
void SPI_init (void)
 This function initializes the SPI module. More...
 
SPI_Handle SPI_open (uint32_t domain, uint32_t idx, SPI_Params *params)
 This function opens a given SPI peripheral. More...
 
void OSPI_close (OSPI_Handle handle)
 Function to close a OSPI peripheral specified by the OSPI handle. More...
 
int32_t OSPI_control (OSPI_Handle handle, uint32_t cmd, void *arg)
 Function performs implementation specific features on a given OSPI_Handle. More...
 
void OSPI_init (void)
 This function initializes the SPI module. More...
 
OSPI_Handle OSPI_open (uint32_t domain, uint32_t idx, OSPI_Params *params)
 This function opens a given OSPI peripheral. More...
 
void OSPI_Params_init (OSPI_Params *params)
 Function to initialize the OSPI_Params struct to its defaults. More...
 
bool OSPI_transfer (OSPI_Handle handle, OSPI_Transaction *spiTrans)
 Function to perform SPI transactions. More...
 
void SPI_Params_init (SPI_Params *params)
 Function to initialize the SPI_Params struct to its defaults. More...
 
void SPI_serviceISR (SPI_Handle handle)
 Function to service the SPI module's interrupt service routine. More...
 
bool SPI_transfer (SPI_Handle handle, SPI_Transaction *spiTrans)
 Function to perform SPI transactions. More...
 
void SPI_transferCancel (SPI_Handle handle)
 Function to cancel SPI transactions. More...
 

Typedefs

typedef struct SPI_Config_s * SPI_Handle
 A handle that is returned from a SPI_open() call. More...
 
typedef void(* SPI_CallbackFxn) (SPI_Handle handle, SPI_Transaction *transaction)
 The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK. More...
 
typedef void(* SPI_CloseFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_close(). More...
 
typedef int32_t(* SPI_ControlFxn) (SPI_Handle handle, uint32_t cmd, const void *arg)
 A function pointer to a driver specific implementation of SPI_control(). More...
 
typedef void(* SPI_InitFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_init(). More...
 
typedef SPI_Handle(* SPI_OpenFxn) (SPI_Handle handle, const SPI_Params *params)
 A function pointer to a driver specific implementation of SPI_open(). More...
 
typedef void(* SPI_ServiceISRFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_serviceISR(). More...
 
typedef bool(* SPI_TransferFxn) (SPI_Handle handle, SPI_Transaction *transaction)
 A function pointer to a driver specific implementation of SPI_transfer(). More...
 
typedef void(* SPI_TransferCancelFxn) (SPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_transferCancel(). More...
 
typedef SPI_Config SPI_config_list[SPI_MAX_DOMAIN_CNT][SPI_MAX_CONFIG_CNT]
 
typedef struct OSPI_Config_s * OSPI_Handle
 A handle that is returned from a SPI_open() call. More...
 
typedef void(* OSPI_CallbackFxn) (OSPI_Handle handle, OSPI_Transaction *transaction)
 The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK. More...
 
typedef void(* OSPI_CloseFxn) (OSPI_Handle handle)
 A function pointer to a driver specific implementation of OSPI_close(). More...
 
typedef int32_t(* OSPI_ControlFxn) (OSPI_Handle handle, uint32_t cmd, const void *arg)
 A function pointer to a driver specific implementation of OSPI_control(). More...
 
typedef void(* OSPI_InitFxn) (OSPI_Handle handle)
 A function pointer to a driver specific implementation of OSPI_init(). More...
 
typedef OSPI_Handle(* OSPI_OpenFxn) (OSPI_Handle handle, const OSPI_Params *params)
 A function pointer to a driver specific implementation of SPI_open(). More...
 
typedef void(* OSPI_ServiceISRFxn) (OSPI_Handle handle)
 A function pointer to a driver specific implementation of SPI_serviceISR(). More...
 
typedef bool(* OSPI_TransferFxn) (OSPI_Handle handle, OSPI_Transaction *transaction)
 A function pointer to a driver specific implementation of OSPI_transfer(). More...
 
typedef void(* OSPI_TransferCancelFxn) (OSPI_Handle handle)
 A function pointer to a driver specific implementation of OSPI_transferCancel(). More...
 
typedef OSPI_Config OSPI_config_list[OSPI_MAX_DOMAIN_CNT][OSPI_MAX_CONFIG_CNT]
 

Enumerations

enum  SPI_Status {
  SPI_TRANSFER_COMPLETED = 0, SPI_TRANSFER_STARTED, SPI_TRANSFER_CANCELED, SPI_TRANSFER_FAILED,
  SPI_TRANSFER_CSN_DEASSERT, SPI_TRANSFER_TIMEOUT
}
 Status codes that are set by the SPI driver. More...
 
enum  SPI_Mode { SPI_MASTER = 0, SPI_SLAVE = 1 }
 Definitions for various SPI modes of operation. More...
 
enum  SPI_FrameFormat {
  SPI_POL0_PHA0 = 0, SPI_POL0_PHA1 = 1, SPI_POL1_PHA0 = 2, SPI_POL1_PHA1 = 3,
  SPI_TI = 4, SPI_MW = 5
}
 Definitions for various SPI data frame formats. More...
 
enum  SPI_TransferMode { SPI_MODE_BLOCKING, SPI_MODE_CALLBACK }
 SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK SPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed. More...
 
enum  OSPI_Status {
  OSPI_TRANSFER_COMPLETED = 0, OSPI_TRANSFER_STARTED, OSPI_TRANSFER_CANCELED, OSPI_TRANSFER_FAILED,
  OSPI_TRANSFER_CSN_DEASSERT, OSPI_TRANSFER_TIMEOUT
}
 Status codes that are set by the SPI driver. More...
 
enum  OSPI_Mode { OSPI_MASTER = 0, OSPI_SLAVE = 1 }
 Definitions for various SPI modes of operation. More...
 
enum  OSPI_FrameFormat {
  OSPI_POL0_PHA0 = 0, OSPI_POL0_PHA1 = 1, OSPI_POL1_PHA0 = 2, OSPI_POL1_PHA1 = 3,
  OSPI_TI = 4, OSPI_MW = 5
}
 Definitions for various SPI data frame formats. More...
 
enum  OSPI_TransferMode { OSPI_MODE_BLOCKING, OSPI_MODE_CALLBACK }
 SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK OSPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed. More...
 

Macros

#define SPI_CMD_RESERVED   (32U)
 
#define OSPI_CMD_RESERVED   (32U)
 
#define SPI_STATUS_RESERVED   (-((int32_t)32))
 
#define SPI_STATUS_SUCCESS   (int32_t)(0)
 Successful status code returned by SPI_control(). More...
 
#define SPI_STATUS_ERROR   (-((int32_t)1))
 Generic error status code returned by SPI_control(). More...
 
#define SPI_STATUS_UNDEFINEDCMD   (-((int32_t)2))
 An error status code returned by SPI_control() for undefined command codes. More...
 
#define SPI_WAIT_FOREVER   (~(0U))
 Wait forever define. More...
 
#define SPI_MAX_CONFIG_CNT   (CSL_MCSPI_PER_CNT)
 
#define SPI_MAX_DOMAIN_CNT   (CSL_MCSPI_DOMAIN_CNT)
 
#define OSPI_MAX_CONFIG_CNT   (CSL_OSPI_PER_CNT)
 
#define OSPI_MAX_DOMAIN_CNT   (CSL_OSPI_DOMAIN_CNT)
 

Macro Definition Documentation

◆ SPI_CMD_RESERVED

#define SPI_CMD_RESERVED   (32U)

Common SPI_control command code reservation offset. SPI driver implementations should offset command codes with SPI_CMD_RESERVED growing positively

Example implementation specific command codes:

#define SPIXYZ_COMMAND0 SPI_CMD_RESERVED + 0
#define SPIXYZ_COMMAND1 SPI_CMD_RESERVED + 1

◆ OSPI_CMD_RESERVED

#define OSPI_CMD_RESERVED   (32U)

◆ SPI_STATUS_RESERVED

#define SPI_STATUS_RESERVED   (-((int32_t)32))

Common SPI_control status code reservation offset. SPI driver implementations should offset status codes with SPI_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define SPIXYZ_STATUS_ERROR0 SPI_STATUS_RESERVED - 0
#define SPIXYZ_STATUS_ERROR1 SPI_STATUS_RESERVED - 1
#define SPIXYZ_STATUS_ERROR2 SPI_STATUS_RESERVED - 2

◆ SPI_STATUS_SUCCESS

#define SPI_STATUS_SUCCESS   (int32_t)(0)

Successful status code returned by SPI_control().

SPI_control() returns SPI_STATUS_SUCCESS if the control code was executed successfully.

◆ SPI_STATUS_ERROR

#define SPI_STATUS_ERROR   (-((int32_t)1))

Generic error status code returned by SPI_control().

SPI_control() returns SPI_STATUS_ERROR if the control code was not executed successfully.

◆ SPI_STATUS_UNDEFINEDCMD

#define SPI_STATUS_UNDEFINEDCMD   (-((int32_t)2))

An error status code returned by SPI_control() for undefined command codes.

SPI_control() returns SPI_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.

◆ SPI_WAIT_FOREVER

#define SPI_WAIT_FOREVER   (~(0U))

Wait forever define.

◆ SPI_MAX_CONFIG_CNT

#define SPI_MAX_CONFIG_CNT   (CSL_MCSPI_PER_CNT)

◆ SPI_MAX_DOMAIN_CNT

#define SPI_MAX_DOMAIN_CNT   (CSL_MCSPI_DOMAIN_CNT)

◆ OSPI_MAX_CONFIG_CNT

#define OSPI_MAX_CONFIG_CNT   (CSL_OSPI_PER_CNT)

◆ OSPI_MAX_DOMAIN_CNT

#define OSPI_MAX_DOMAIN_CNT   (CSL_OSPI_DOMAIN_CNT)

Typedef Documentation

◆ SPI_Handle

typedef struct SPI_Config_s* SPI_Handle

A handle that is returned from a SPI_open() call.

◆ SPI_CallbackFxn

typedef void(* SPI_CallbackFxn) (SPI_Handle handle, SPI_Transaction *transaction)

The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.

Parameters
SPI_HandleSPI_Handle
SPI_Transaction*SPI_Transaction*

◆ SPI_CloseFxn

typedef void(* SPI_CloseFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_close().

◆ SPI_ControlFxn

typedef int32_t(* SPI_ControlFxn) (SPI_Handle handle, uint32_t cmd, const void *arg)

A function pointer to a driver specific implementation of SPI_control().

◆ SPI_InitFxn

typedef void(* SPI_InitFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_init().

◆ SPI_OpenFxn

typedef SPI_Handle(* SPI_OpenFxn) (SPI_Handle handle, const SPI_Params *params)

A function pointer to a driver specific implementation of SPI_open().

◆ SPI_ServiceISRFxn

typedef void(* SPI_ServiceISRFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_serviceISR().

◆ SPI_TransferFxn

typedef bool(* SPI_TransferFxn) (SPI_Handle handle, SPI_Transaction *transaction)

A function pointer to a driver specific implementation of SPI_transfer().

◆ SPI_TransferCancelFxn

typedef void(* SPI_TransferCancelFxn) (SPI_Handle handle)

A function pointer to a driver specific implementation of SPI_transferCancel().

◆ SPI_config_list

◆ OSPI_Handle

typedef struct OSPI_Config_s* OSPI_Handle

A handle that is returned from a SPI_open() call.

◆ OSPI_CallbackFxn

typedef void(* OSPI_CallbackFxn) (OSPI_Handle handle, OSPI_Transaction *transaction)

The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.

Parameters
OSPI_HandleOSPI_Handle
OSPI_Transaction*OSPI_Transaction*

◆ OSPI_CloseFxn

typedef void(* OSPI_CloseFxn) (OSPI_Handle handle)

A function pointer to a driver specific implementation of OSPI_close().

◆ OSPI_ControlFxn

typedef int32_t(* OSPI_ControlFxn) (OSPI_Handle handle, uint32_t cmd, const void *arg)

A function pointer to a driver specific implementation of OSPI_control().

◆ OSPI_InitFxn

typedef void(* OSPI_InitFxn) (OSPI_Handle handle)

A function pointer to a driver specific implementation of OSPI_init().

◆ OSPI_OpenFxn

typedef OSPI_Handle(* OSPI_OpenFxn) (OSPI_Handle handle, const OSPI_Params *params)

A function pointer to a driver specific implementation of SPI_open().

◆ OSPI_ServiceISRFxn

typedef void(* OSPI_ServiceISRFxn) (OSPI_Handle handle)

A function pointer to a driver specific implementation of SPI_serviceISR().

◆ OSPI_TransferFxn

typedef bool(* OSPI_TransferFxn) (OSPI_Handle handle, OSPI_Transaction *transaction)

A function pointer to a driver specific implementation of OSPI_transfer().

◆ OSPI_TransferCancelFxn

typedef void(* OSPI_TransferCancelFxn) (OSPI_Handle handle)

A function pointer to a driver specific implementation of OSPI_transferCancel().

◆ OSPI_config_list

Enumeration Type Documentation

◆ SPI_Status

enum SPI_Status

Status codes that are set by the SPI driver.

Enumerator
SPI_TRANSFER_COMPLETED 
SPI_TRANSFER_STARTED 
SPI_TRANSFER_CANCELED 
SPI_TRANSFER_FAILED 
SPI_TRANSFER_CSN_DEASSERT 
SPI_TRANSFER_TIMEOUT 

◆ SPI_Mode

enum SPI_Mode

Definitions for various SPI modes of operation.

Enumerator
SPI_MASTER 

SPI in master mode

SPI_SLAVE 

SPI in slave mode

◆ SPI_FrameFormat

Definitions for various SPI data frame formats.

Enumerator
SPI_POL0_PHA0 

SPI mode Polarity 0 Phase 0

SPI_POL0_PHA1 

SPI mode Polarity 0 Phase 1

SPI_POL1_PHA0 

SPI mode Polarity 1 Phase 0

SPI_POL1_PHA1 

SPI mode Polarity 1 Phase 1

SPI_TI 

TI mode

SPI_MW 

Micro-wire mode

◆ SPI_TransferMode

SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK SPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed.

Enumerator
SPI_MODE_BLOCKING 

SPI_transfer() blocks execution. This mode can only be used when called within a Task context

SPI_MODE_CALLBACK 

SPI_transfer() does not block code execution and will call a SPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context.

◆ OSPI_Status

Status codes that are set by the SPI driver.

Enumerator
OSPI_TRANSFER_COMPLETED 
OSPI_TRANSFER_STARTED 
OSPI_TRANSFER_CANCELED 
OSPI_TRANSFER_FAILED 
OSPI_TRANSFER_CSN_DEASSERT 
OSPI_TRANSFER_TIMEOUT 

◆ OSPI_Mode

enum OSPI_Mode

Definitions for various SPI modes of operation.

Enumerator
OSPI_MASTER 

SPI in master mode

OSPI_SLAVE 

SPI in slave mode

◆ OSPI_FrameFormat

Definitions for various SPI data frame formats.

Enumerator
OSPI_POL0_PHA0 

SPI mode Polarity 0 Phase 0

OSPI_POL0_PHA1 

SPI mode Polarity 0 Phase 1

OSPI_POL1_PHA0 

SPI mode Polarity 1 Phase 0

OSPI_POL1_PHA1 

SPI mode Polarity 1 Phase 1

OSPI_TI 

TI mode

OSPI_MW 

Micro-wire mode

◆ OSPI_TransferMode

SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously. In SPI_MODE_BLOCKING mode SPI_transfer() blocks code execution until the SPI transaction has completed. In SPI_MODE_CALLBACK OSPI_transfer() does not block code execution and instead calls a SPI_CallbackFxn callback function when the transaction has completed.

Enumerator
OSPI_MODE_BLOCKING 

SPI_transfer() blocks execution. This mode can only be used when called within a Task context

OSPI_MODE_CALLBACK 

SPI_transfer() does not block code execution and will call a SPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context.

Function Documentation

◆ SPI_close()

void SPI_close ( SPI_Handle  handle)

Function to close a SPI peripheral specified by the SPI handle.

Precondition
SPI_open() has to be called first.
Parameters
handleA SPI handle returned from SPI_open()
See also
SPI_open()

◆ SPI_control()

int32_t SPI_control ( SPI_Handle  handle,
uint32_t  cmd,
void *  arg 
)

Function performs implementation specific features on a given SPI_Handle.

Precondition
SPI_open() has to be called first.
Parameters
handleA SPI handle returned from SPI_open()
cmdA command value defined by the driver specific implementation
argAn optional R/W (read/write) argument that is accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
SPI_open()

◆ SPI_init()

void SPI_init ( void  )

This function initializes the SPI module.

Precondition
The SPI_config structure must exist and be persistent before this function can be called. This function must also be called before any other SPI driver APIs. This function call does not modify any peripheral registers.

◆ SPI_open()

SPI_Handle SPI_open ( uint32_t  domain,
uint32_t  idx,
SPI_Params params 
)

This function opens a given SPI peripheral.

Precondition
SPI controller has been initialized using SPI_init()
Parameters
domainLogical domain number of domain where SPI IP is present
idxLogical peripheral number for the SPI indexed into the SPI_config table
paramsPointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only).
Returns
A SPI_Handle on success or a NULL on an error or if it has been opened already.
See also
SPI_init()
SPI_close()

◆ OSPI_close()

void OSPI_close ( OSPI_Handle  handle)

Function to close a OSPI peripheral specified by the OSPI handle.

Precondition
OSPI_open() has to be called first.
Parameters
handleA OSPI handle returned from OSPI_open()
See also
OSPI_open()

◆ OSPI_control()

int32_t OSPI_control ( OSPI_Handle  handle,
uint32_t  cmd,
void *  arg 
)

Function performs implementation specific features on a given OSPI_Handle.

Precondition
OSPI_open() has to be called first.
Parameters
handleA OSPI handle returned from OSPI_open()
cmdA command value defined by the driver specific implementation
argAn optional R/W (read/write) argument that is accompanied with cmd
Returns
Implementation specific return codes. Negative values indicate unsuccessful operations.
See also
OSPI_open()

◆ OSPI_init()

void OSPI_init ( void  )

This function initializes the SPI module.

Precondition
The OSPI_config structure must exist and be persistent before this function can be called. This function must also be called before any other OSPI driver APIs. This function call does not modify any peripheral registers.

◆ OSPI_open()

OSPI_Handle OSPI_open ( uint32_t  domain,
uint32_t  idx,
OSPI_Params params 
)

This function opens a given OSPI peripheral.

Precondition
OSPI controller has been initialized using OSPI_init()
Parameters
domaindomain where OSPI IP is located
idxLogical peripheral number for the SPI indexed into the SPI_config table
paramsPointer to an parameter block, if NULL it will use default values. All the fields in this structure are RO (read-only).
Returns
A SPI_Handle on success or a NULL on an error or if it has been opened already.
See also
OSPI_init()
OSPI_close()

◆ OSPI_Params_init()

void OSPI_Params_init ( OSPI_Params params)

Function to initialize the OSPI_Params struct to its defaults.

Parameters
paramsAn pointer to OSPI_Params structure for initialization

Defaults values are: transferMode = OSPI_MODE_BLOCKING transferTimeout = OSPI_WAIT_FOREVER transferCallbackFxn = NULL mode = OSPI_MASTER bitRate = 1000000 (Hz) dataSize = 8 (bits) frameFormat = OSPI_POL0_PHA0

◆ OSPI_transfer()

bool OSPI_transfer ( OSPI_Handle  handle,
OSPI_Transaction spiTrans 
)

Function to perform SPI transactions.

If the SPI is in SPI_MASTER mode, it will immediately start the transaction. If the SPI is in SPI_SLAVE mode, it prepares itself for a transaction with a SPI master.

In OSPI_MODE_BLOCKING, OSPI_transfer will block task execution until the transaction has completed.

In OSPI_MODE_CALLBACK, OSPI_transfer() does not block task execution and calls a SPI_CallbackFxn. This makes the OSPI_tranfer() safe to be used within a Task, Swi, or Hwi context. The SPI_Transaction structure must stay persistent until the OSPI_transfer function has completed!

Parameters
handleA OSPI_Handle
spiTransA pointer to a SPI_Transaction. All of the fields within transaction except SPI_Transaction.count and SPI_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occured, SPI_Transaction.count will contain the number of frames that were transferred.
Returns
BTRUE if started successfully; else BFALSE
See also
OSPI_open
OSPI_transferCancel

◆ SPI_Params_init()

void SPI_Params_init ( SPI_Params params)

Function to initialize the SPI_Params struct to its defaults.

Parameters
paramsAn pointer to SPI_Params structure for initialization

Defaults values are: transferMode = SPI_MODE_BLOCKING transferTimeout = SPI_WAIT_FOREVER transferCallbackFxn = NULL mode = SPI_MASTER bitRate = 1000000 (Hz) dataSize = 8 (bits) frameFormat = SPI_POL0_PHA0

◆ SPI_serviceISR()

void SPI_serviceISR ( SPI_Handle  handle)

Function to service the SPI module's interrupt service routine.

Parameters
handleA SPI_Handle

◆ SPI_transfer()

bool SPI_transfer ( SPI_Handle  handle,
SPI_Transaction spiTrans 
)

Function to perform SPI transactions.

If the SPI is in SPI_MASTER mode, it will immediately start the transaction. If the SPI is in SPI_SLAVE mode, it prepares itself for a transaction with a SPI master.

In SPI_MODE_BLOCKING, SPI_transfer will block task execution until the transaction has completed.

In SPI_MODE_CALLBACK, SPI_transfer() does not block task execution and calls a SPI_CallbackFxn. This makes the SPI_tranfer() safe to be used within a Task, Swi, or Hwi context. The SPI_Transaction structure must stay persistent until the SPI_transfer function has completed!

Parameters
handleA SPI_Handle
spiTransA pointer to a SPI_Transaction. All of the fields within transaction except SPI_Transaction.count and SPI_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occured, SPI_Transaction.count will contain the number of frames that were transferred.
Returns
BTRUE if started successfully; else BFALSE
See also
SPI_open
SPI_transferCancel

◆ SPI_transferCancel()

void SPI_transferCancel ( SPI_Handle  handle)

Function to cancel SPI transactions.

In SPI_MODE_BLOCKING, SPI_transferCancel has no effect.

In SPI_MODE_CALLBACK, SPI_transferCancel() will stop an SPI transfer if if one is in progress. If a transaction was in progress, its callback function will be called in context from which this API is called from. The SPI_CallbackFxn function can determine if the transaction was successful or not by reading the SPI_Status status value in the SPI_Transaction structure.

Parameters
handleA SPI_Handle
See also
SPI_open
SPI_transfer