PDK API Guide for J721E
CacheP

Introduction

CacheP interface

Files

file  CacheP.h
 Cache Handling routines for the RTOS Porting Interface.
 

Functions

void CacheP_wb (const void *addr, uint32_t size)
 Function to write back cache lines. More...
 
void CacheP_Inv (const void *addr, uint32_t size)
 Function to invalidate cache lines. More...
 
void CacheP_wbInv (const void *addr, uint32_t size)
 Function to write back and invalidate cache lines. More...
 
void CacheP_setMar (void *baseAddr, uint32_t size, uint32_t value)
 Set MAR attribute for a memory range. More...
 
uint32_t CacheP_getMar (uintptr_t baseAddr)
 Get MAR attribute for a region of 16MB. More...
 

Cache coherent type definitions

typedef uint32_t Osal_CacheP_isCoherent
 This enumerator defines the cache coherent types. More...
 
#define OSAL_CACHEP_COHERENT   ((uint32_t) 0U)
 
#define OSAL_CACHEP_NOT_COHERENT   ((uint32_t) 1U)
 

Set Cache MAR register

typedef uint32_t CacheP_Mar
 This enumerator defines the MAR register setting types. More...
 
#define CacheP_Mar_DISABLE   ((uint32_t) 0U)
 
#define CacheP_Mar_ENABLE   ((uint32_t) 1U)
 

Macro Definition Documentation

◆ OSAL_CACHEP_COHERENT

#define OSAL_CACHEP_COHERENT   ((uint32_t) 0U)

Cache is coherent on this CPU

◆ OSAL_CACHEP_NOT_COHERENT

#define OSAL_CACHEP_NOT_COHERENT   ((uint32_t) 1U)

Cache is not coherent on this CPU

◆ CacheP_Mar_DISABLE

#define CacheP_Mar_DISABLE   ((uint32_t) 0U)

Cache MAR register disabled

◆ CacheP_Mar_ENABLE

#define CacheP_Mar_ENABLE   ((uint32_t) 1U)

Cache MAR register is enabled

Typedef Documentation

◆ Osal_CacheP_isCoherent

typedef uint32_t Osal_CacheP_isCoherent

This enumerator defines the cache coherent types.

◆ CacheP_Mar

typedef uint32_t CacheP_Mar

This enumerator defines the MAR register setting types.

Function Documentation

◆ CacheP_wb()

void CacheP_wb ( const void *  addr,
uint32_t  size 
)

Function to write back cache lines.

Parameters
addrStart address of the cache line/s
sizesize (in bytes) of the memory to be written back

◆ CacheP_Inv()

void CacheP_Inv ( const void *  addr,
uint32_t  size 
)

Function to invalidate cache lines.

Parameters
addrStart address of the cache line/s
sizesize (in bytes) of the memory to invalidate

◆ CacheP_wbInv()

void CacheP_wbInv ( const void *  addr,
uint32_t  size 
)

Function to write back and invalidate cache lines.

Parameters
addrStart address of the cache line/s
sizesize (in bytes) of the memory to be written back and invalidate

◆ CacheP_setMar()

void CacheP_setMar ( void *  baseAddr,
uint32_t  size,
uint32_t  value 
)

Set MAR attribute for a memory range.

[C66x Only] The API will set the MAR attribute for the range, start_addr = floor(baseAddr, 16MB) .. end_addr = ceil(baseAddr+size, 16MB)

Parameters
baseAddrRegion start address. Recommended to be 16MB aligned
sizeRegion size in bytes. Recommended to be multiple of 16MB aligned
valuevalue for setting MAR register CacheP_Mar

◆ CacheP_getMar()

uint32_t CacheP_getMar ( uintptr_t  baseAddr)

Get MAR attribute for a region of 16MB.

[C66x Only] The API will return the MAR attribute of the region with start addr as start_addr = floor(baseAddr, 16MB)

Parameters
baseAddrregion start address, recommended to be 16MB aligned
Returns
MAR attribute for this 16MB region