2.14. Release Notes - 06_01_00

2.14.1. Introduction

This release notes provides important information that will assist you in using the PDK software package. This document provides the product information and known issues that are specific to the PDK software package.

2.14.2. What’s New

  • CPSW
    • Support for MCU2_1 core on CPSW2G

    • RMII mode

    • PHY bootstrap mode support

    • Support for Port ready callback (port link up)

    • Traffic Shaping/TSN 802.1Qav - Transmit/Receive Rate Limiting: Committed Info Rate/Excess Info Rate

    • QoS/Packet Priority mapping

    • Policer and Network security support

    • Debug and diagnostic features
      • ALE register dump

      • CPSW DMA packet Statistics

      • Debug GEL files - mdio, stats, config

  • DSS
    • BT601 output format support

  • Board
    • Leo PMIC
      • Support for programming Buck and LDO voltage for AVS Class 0

      • Support for Voltage and Thermal Monitorring

      • Support for programming Leo GPIO

      • Support for ESM, RTC and WDT Programming

  • SBL
    • Added AVS support

  • ECC/ESM sample application

2.14.3. Upgrade and Compatibility

  • CPSW
    • Cpsw_Config.CpswAle_Config - Removed host address unicast entry from ALE_open

    • Cpsw_Config.CpswPhy_Config - Removed resetEnable.

    • Cpsw_MacCommonConfig - merged into Cpsw_Config.

    • CpswDma_OpenTxChPrms - Removed CpswDma_EventCfg and replaced with CpswDma_PktNotifyCb. Variable name change for proxyflag, callback argument

    • CpswDma_OpenRxFlowPrms - Removed CpswDma_EventCfg and replaced with CpswDma_PktNotifyCb. Variable name change for proxyflag, callback argument

    • Cpsw_LinkStateChangeInfo is changed Cpsw_MdioLinkStateChangeInfo

    • CPSW Resource manager - Replaced earlier RM

    • CPSW_CFG_DEV_ERROR is enabled/disabled through build system

    • Below APIs are removed ++ Cpsw_isPhyLinked ++ Cpsw_getLinkStatus

2.14.4. Device Support

  • J721E EVM (BOARD=j721e_evm)

2.14.5. Validation Information

This release is validated on J721E EVM for the applicable components. For details on the validated examples refer to the platform specific test report present in PDK_INSTALL_DIR/docs/test_report folder.

2.14.6. Tool Chain Information

Refer to SDK level documentation for Tool Chain and dependent component version used to validate this release.

2.14.7. Fixed Issues

ID

Head Line

Module

Affected Versions

Affected Platforms

PDK-4385

QSPI NOR Flash diagnostic test failure

BOARD

PDK_J7_00.09.00_Bringup

J721E

PDK-4380

[UNIFLASH] Flash speed is slow

BOARD

PDK_J7_00.09.00_Bringup

J721E

PDK-4379

[UNIFLASH] Flash of 14MB app image to OSPI results in failure

BOARD

PDK_J7_00.09.00_Bringup

J721E

PDK-4374

Board UART STDIO read/write API doesn’t work from C7x core

BOARD

PDK_J7_00.09.00_Bringup

J721E

PDK-4509

CSL: DSS: Transperency enable with color key not working

CSL

PDK_J7_00.09.00_Bringup

J721E

PDK-4616

[DSS DRV]DSS reports false error on calling VP Stop IOCTL

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4601

Display port does not initiate link if cable is plugged in after usecase is started

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4580

Dss_convModuletoNode returns wrong value if node is not a pipe

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4571

eDP does not work with all monitors

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4405

DSS: eDP: when eDP init fails it should return error rathar than trying forever

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4398

eDP display broken in release mode, works in debug mode

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4396

DSS has intermittent init failures with eDP enabled

DSS

PDK_J7_00.09.00_Bringup

J721E

PDK-4632

IPC mailbox handling will not handle pending messages if interrupts are missed

IPC

PDK_J7_00.09.00_Bringup

J721E

PDK-4606

Incorrect check for Pitch for RGB format in VISS

VHWA

PDK_J7_00.09.00_Bringup

J721E

PDK-4597

Incorrect Condition check in VISS in GLBCE Init Sequence

VHWA

PDK_J7_00.09.00_Bringup

J721E

PDK-4410

Incorrect MSC output when run along with the NF

VHWA

PDK_J7_00.09.00_Bringup

J721E

PDK-4329

LDC Performance is ~450 Mp/s under system load

VHWA

PDK_J7_00.09.00_Bringup

J721E

PDK-4322

VHWA Integration app crashes in release mode with print disabled

VHWA

PDK_J7_00.09.00_Bringup

J721E

PDK-4271

In multi-channel mode, VISS asserts in ISR

VHWA

PDK_J7_00.08.00_EA8

J721E

PDK-4356

NDK example Rx failing intermittently

CPSW

PDK_J7_00.09.00_Bringup

J721E

PDK-4223

MAC speed test no link up in manual mode

CPSW

PDK_J7_00.09.00_Bringup

J721E

PDK-4474

Interrupt assignment not correct in cpsw_soc

CPSW

PDK_J7_00.09.00_Bringup

J721E

2.14.8. Known Issues

ID

Head Line

Module

Reported in Release

Affected Platforms

Workaround in this release

PDK-4738

Output mismatch when each region requiring 3 TRs

VHWA_LDC

PDK_J7_01.00.00_RTM

J721E

None

PDK-4694

DMPAC DOF driver doesn’t handle certain SOF case properly

VHWA_DOF

PDK_J7_00.09.01

J721E

This issue is due to shift in flowvector out buffer. While generating the SOF binary map make sure that Paxel rows without any pixel enabled should be in consecutive pair.

PDK-4698

Active DP -> HDMI adapter doesn’t work

DSS

PDK_J7_00.09.01

J721E

Use the display that supports Active DP

PDK-4224

Max Length test Tx completion hangs if cpswHostPort maxRxMtu is exceeded

CPSW

PDK_J7_00.09.00_Bringup

J721E

Host core should not send packet more than maxRxMtu

PDK-4770

Cpsw2G - Interrupts won’t work for main domain cores(mcu2_1, mpu1_0)

CPSW

PDK_J7_01.00.00_RTM

J721E

Use polling mode for mdio interrupts.

PDK-4633

CPSW RGMII loopback fails at RGMII 100Mbps & RMII mode

CPSW

PDK_J7_00.09.00_Bringup

J721E

Internal loopback works at 1Gbps

PROC_BRDS-658

J7 GESI DB - MAC PORT 0 packet drop seen of 1Gbps Speed

CPSW

PDK_J7_00.09.00_Bringup

J721E

MAC port 0 configured at 100Mbps

PDK-4673

Using PROXY 1 for Pinmux cause crash in SDK use cases

BOARD

PDK_TDA_01.09.00

J721E

Use Proxy 0. (Already taken care in driver)

PDK-4367

Noisy output for digital audio diagnostic test

BOARD

PDK_J7_00.09.00_Bringup

J721E

None

PDK-4732

Audio diagnostic test failure

BOARD

PDK_J7_01.00.00_RTM

J721E

Run the McASP driver example

PDK-4731

R5 diag test hang while running framework

BOARD

PDK_J7_01.00.00_RTM

J721E

run diagnostic tests without famework

PDK-4724

CPSW RGMII diagnostic test failure

BOARD

PDK_J7_01.00.00_RTM

J721E

None

PDK-4767

QSPI flash writer and diagnostic test failure

BOARD

PDK_J7_01.00.00_RTM

J721E

None

2.14.9. Limitations

  • None