MMALIB User Guide
MMALIB

MMALIB is the software library implementing low-level Convolultional Neural Network (CNN), Linear Algebra (LINALG) and Digital Signal Processing (DSP) functions using the Matrix Multiplication Accelerator (MMA) and C7x ISA available on TI's Keystone 3 devices.

The top-level block diagram of MMALIB is shown below.

Top-level illustration of MMALIB

The main parts in MMALIB are listed below:

MMALIB Module Description
CNN Low-level Convolutional Neural Network kernels
LINALG Low-level Linear Algebra kernels
DSP Low-level Digital Signal Processing kernels



Disclaimer

See also TI Disclaimer.