![]() |
MCUSW
|
Structure defining the CAN FD data phase baud rate configuration.
Data Fields | |
| uint16 | Baud |
| uint8 | PropSeg |
| uint8 | Pseg1 |
| uint8 | Pseg2 |
| uint8 | Sjw |
| uint16 | TimingValues |
| uint16 | BrpValue |
| uint16 | TrcvCompDelay |
| boolean | BrsSwitch |
| uint16 Can_FdBaudConfigType::Baud |
In Kbps
| uint8 Can_FdBaudConfigType::PropSeg |
Prop Segment value
| uint8 Can_FdBaudConfigType::Pseg1 |
Phase Segment 1
| uint8 Can_FdBaudConfigType::Pseg2 |
Phase Segment 2
| uint8 Can_FdBaudConfigType::Sjw |
Sync jump width
| uint16 Can_FdBaudConfigType::TimingValues |
Sum of all timing parameters *
| uint16 Can_FdBaudConfigType::BrpValue |
Controller BRP value for Baud
| uint16 Can_FdBaudConfigType::TrcvCompDelay |
Specifies the Transceiver Delay Compensation Offset in ns
| boolean Can_FdBaudConfigType::BrsSwitch |
Specifies if the bit rate switching shall be used for transmissions.