112 #define WDG_VARIANT_PRE_COMPILE (STD_ON) 117 #define WDG_INIT_CONFIG_PC WdgSettingsConfig 122 #define WDG_DEV_ERROR_DETECT (STD_ON) 125 #define WDG_GET_VERSION_INFO_API (STD_ON) 128 #define WDG_REGISTER_READBACK_API (STD_ON) 132 #define WDG_MAX_TIMEOUT ((uint16)65535) 136 #define WDG_RTI_FREQUENCY ((uint32)12500000) 139 #define WDG_DISABLE_ALLOWED (STD_OFF) 148 #define WdgConf_WdgGeneral_WdgIndex_0 (0U) 164 #ifndef WDG_E_MODE_FAILED 165 #define WDG_E_MODE_FAILED (DemConf_DemEventParameter_WDG_E_MODE_FAILED) 168 #ifndef WDG_E_DISABLE_REJECTED 169 #define WDG_E_DISABLE_REJECTED (DemConf_DemEventParameter_WDG_E_DISABLE_REJECTED) 173 #define WDG_NUM_INSTANCE (12U) 188 extern CONST(uint32, WDG_CONST)
const struct Wdg_ConfigType_s WdgSettingsConfig
WDG Configuration struct declaration.
const struct Wdg_ConfigType_PC_s WdgSettingsConfig_PC
WDG Configuration pre compile struct declaration.
#define WDG_NUM_INSTANCE
Definition: Wdg_Cfg.h:173
const uint32 RTIHwUnit_BaseAddr[WDG_NUM_INSTANCE]
Base Address of the watchdog instances.