102 #include "EthTrcv_Types.h" 122 #define ETHTRCV_SW_MAJOR_VERSION (11U) 124 #define ETHTRCV_SW_MINOR_VERSION (0U) 126 #define ETHTRCV_SW_PATCH_VERSION (2U) 139 #define ETHTRCV_AR_RELEASE_MAJOR_VERSION (4U) 141 #define ETHTRCV_AR_RELEASE_MINOR_VERSION (3U) 143 #define ETHTRCV_AR_RELEASE_REVISION_VERSION (1U) 151 #define ETHTRCV_VENDOR_ID (44U) 153 #define ETHTRCV_MODULE_ID (73U) 155 #define ETHTRCV_INSTANCE_ID (0U) 171 #define ETHTRCV_INIT_ID ((uint8) 0x01U) 174 #define ETHTRCV_CONTROLLER_INIT_ID ((uint8) 0x02U) 177 #define ETHTRCV_SETTRCVMODE_ID ((uint8) 0x03U) 180 #define ETHTRCV_GETTRCVMODE_ID ((uint8) 0x04U) 183 #define ETHTRCV_SRTAUTONEGOTIA_ID ((uint8) 0x05U) 186 #define ETHTRCV_GETLNKSTATE_ID ((uint8) 0x06U) 189 #define ETHTRCV_GETBAUD_ID ((uint8) 0x07U) 192 #define ETHTRCV_GETDPLXMODE_ID ((uint8) 0x08U) 195 #define ETHTRCV_READMIIIND_ID ((uint8) 0x09U) 198 #define ETHTRCV_WRITEMIIIND_ID ((uint8) 0x0AU) 201 #define ETHTRCV_VERSION_ID ((uint8) 0x0BU) 204 #define ETHTRCV_MAINFCT_WRITE_ID ((uint8) 0x0CU) 207 #define ETHTRCV_GETTRCVWKUPMODE_ID ((uint8) 0x0DU) 210 #define ETHTRCV_SETTRCVWKUPMODE_ID ((uint8) 0x0EU) 213 #define ETHTRCV_CHKWKUP_ID ((uint8) 0x0FU) 216 #define ETHTRCV_SETPHYTESTMODE_ID ((uint8) 0x10U) 219 #define ETHTRCV_SETPHYLOOPBACKMODE_ID ((uint8) 0x11U) 222 #define ETHTRCV_GETPHYSIGNALQUALITY_ID ((uint8) 0x12U) 225 #define ETHTRCV_SETPHYTXMODE_ID ((uint8) 0x13U) 228 #define ETHTRCV_GETCABLEDIAGNOSTICSRESULT_ID ((uint8) 0x014U) 231 #define ETHTRCV_GETPHYIDENTIFIER_ID ((uint8) 0x015U) 246 #ifndef ETHTRCV_E_INV_TRCV_IDX 248 #define ETHTRCV_E_INV_TRCV_IDX ((uint8) 0x01U) 251 #ifndef ETHTRCV_E_UNINIT 253 #define ETHTRCV_E_UNINIT ((uint8) 0x02U) 256 #ifndef ETHTRCV_E_PARAM_POINTER 258 #define ETHTRCV_E_PARAM_POINTER ((uint8) 0x03U) 261 #ifndef ETHTRCV_E_INIT_FAILED 263 #define ETHTRCV_E_INIT_FAILED ((uint8) 0x04U) 266 #ifndef ETHTRCV_E_NOT_SUPPORTED 268 #define ETHTRCV_E_NOT_SUPPORTED ((uint8) 0x05U) 303 FUNC(
void, ETHTRCV_CODE)
304 EthTrcv_Init(P2CONST(EthTrcv_ConfigType, AUTOMATIC, ETHTRCV_PBCFG) CfgPtr);
329 FUNC(Std_ReturnType, ETHTRCV_CODE)
333 #if (STD_ON == ETHTRCV_SETTRANSCEIVERMODE_API) 360 FUNC(Std_ReturnType, ETHTRCV_CODE)
362 EthTrcv_ModeType CtrlMode);
365 #if (STD_ON == ETHTRCV_GETTRANSCEIVERMODE_API) 389 FUNC(Std_ReturnType, ETHTRCV_CODE)
391 EthTrcv_ModeType *TrcvModePtr);
394 #if (ETHTRCV_WAKEUPSUPPORT_API != ETHTRCV_WAKEUP_NOT_SUPPORTED) 426 FUNC(Std_ReturnType, ETHTRCV_CODE)
427 EthTrcv_SetTransceiverWakeupMode(uint8 TrcvIdx,
428 EthTrcv_WakeupModeType TrcvWakeupMode);
431 #if (ETHTRCV_WAKEUPSUPPORT_API != ETHTRCV_WAKEUP_NOT_SUPPORTED) 458 FUNC(Std_ReturnType, ETHTRCV_CODE)
459 EthTrcv_GetTransceiverWakeupMode(uint8 TrcvIdx,
460 EthTrcv_WakeupModeType *TrcvWakeupModePtr);
463 #if (ETHTRCV_WAKEUPSUPPORT_API != ETHTRCV_WAKEUP_NOT_SUPPORTED) 489 FUNC(Std_ReturnType, ETHTRCV_CODE)
490 EthTrcv_CheckWakeup(uint8 TrcvIdx);
496 #if (STD_ON == ETHTRCV_STARTAUTONEGOTIATION_API) 521 FUNC(Std_ReturnType, ETHTRCV_CODE)
525 #if (STD_ON == ETHTRCV_GETLINKSTATE_API) 551 FUNC(Std_ReturnType, ETHTRCV_CODE)
553 EthTrcv_LinkStateType *LinkStatePtr);
561 #if (STD_ON == ETHTRCV_GETBAUDRATE_API) 588 FUNC(Std_ReturnType, ETHTRCV_CODE)
590 EthTrcv_BaudRateType *BaudRatePtr);
593 #if (STD_ON == ETHTRCV_GETDUPLEXMODE_API) 619 FUNC(Std_ReturnType, ETHTRCV_CODE)
621 EthTrcv_DuplexModeType *DuplexModePtr);
624 #if (STD_ON == ETHTRCV_SETPHYTESTMODE_API) 647 FUNC(Std_ReturnType, ETHTRCV_CODE)
649 EthTrcv_PhyTestModeType Mode);
652 #if (STD_ON == ETHTRCV_SETPHYLOOPBACKMODE_API) 676 FUNC(Std_ReturnType, ETHTRCV_CODE)
678 EthTrcv_PhyLoopbackModeType Mode);
681 #if (STD_ON == ETHTRCV_GETPHYSIGNALQUALITY_API) 706 FUNC(Std_ReturnType, ETHTRCV_CODE)
708 uint32* SignalQualityPtr);
711 #if (STD_ON == ETHTRCV_SETPHYTXMODE_API) 735 FUNC(Std_ReturnType, ETHTRCV_CODE)
737 EthTrcv_PhyTxModeType Mode);
740 #if (STD_ON == ETHTRCV_GETCABLEDIAGNOSTICSRESULT_API) 765 FUNC(Std_ReturnType, ETHTRCV_CODE)
767 EthTrcv_CableDiagResultType * ResultPtr);
770 #if (STD_ON == ETHTRCV_GETPHYIDENTIFIER_API) 803 FUNC(Std_ReturnType, ETHTRCV_CODE)
805 uint32* OrgUniqueIdPtr,
807 uint8* RevisionNrPtr);
810 #if (STD_ON == ETHTRCV_VERSION_INFO_API) 832 FUNC(
void, ETHTRCV_CODE)
872 FUNC(
void, ETHTRCV_CODE)
907 FUNC(
void, ETHTRCV_CODE)
931 FUNC(
void, ETHTRCV_CODE)
void EthTrcv_GetVersionInfo(Std_VersionInfoType *VersionInfoPtr)
Function returns the version information of this module.
Std_ReturnType EthTrcv_GetCableDiagnosticsResult(uint8 TrcvIdx, EthTrcv_CableDiagResultType *ResultPtr)
This function Retrieves the cable diagnostics result of a given transceiver.
Std_ReturnType EthTrcv_SetPhyTxMode(uint8 TrcvIdx, EthTrcv_PhyTxModeType Mode)
This function Activates a given transmission mode.
void EthTrcv_MainFunction(void)
This function is used for polling state changes and wakeup reasons. It calls EthIf_TrcvModeIndication...
Std_ReturnType EthTrcv_StartAutoNegotiation(uint8 TrcvIdx)
This function restarts the negotiation of the transmission parameters used by the indexed.
Std_ReturnType EthTrcv_GetTransceiverMode(uint8 TrcvIdx, EthTrcv_ModeType *TrcvModePtr)
This function obtains the state of the indexed transceiver.
Std_ReturnType EthTrcv_GetBaudRate(uint8 TrcvIdx, EthTrcv_BaudRateType *BaudRatePtr)
This function obtains the baud rate of the indexed transceiver.
void EthTrcv_ReadMiiIndication(uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 RegVal)
This function is called when information has been read out via MII interface. Triggered by previous E...
Std_ReturnType EthTrcv_SetPhyTestMode(uint8 TrcvIdx, EthTrcv_PhyTestModeType Mode)
This function Activates a given test mode.
Std_ReturnType EthTrcv_TransceiverInit(uint8 TrcvIdx)
This function initializes the Ethernet Transceiver controller. All the required initialization for th...
Std_ReturnType EthTrcv_SetTransceiverMode(uint8 TrcvIdx, EthTrcv_ModeType CtrlMode)
This function enables / disables the indexed transceiver.
Std_ReturnType EthTrcv_GetPhyIdentifier(uint8 TrcvIdx, uint32 *OrgUniqueIdPtr, uint8 *ModelNrPtr, uint8 *RevisionNrPtr)
This function Obtains the PHY identifier of the Ethernet Transceiver according to IEEE 802....
void EthTrcv_Init(const EthTrcv_ConfigType *CfgPtr)
This function initializes the Ethernet Transceiver controller. All the required initialization for th...
Std_ReturnType EthTrcv_SetPhyLoopbackMode(uint8 TrcvIdx, EthTrcv_PhyLoopbackModeType Mode)
This function Activates a given loopback mode.
Std_ReturnType EthTrcv_GetLinkState(uint8 TrcvIdx, EthTrcv_LinkStateType *LinkStatePtr)
This function obtains the link state of the indexed transceiver.
Std_ReturnType EthTrcv_GetPhySignalQuality(uint8 TrcvIdx, uint32 *SignalQualityPtr)
This function Obtains the current signal quality of the link of the indexed transceiver.
void EthTrcv_WriteMiiIndication(uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegId)
This function is called when information has been written via MII interface. Triggered by previous Et...
Std_ReturnType EthTrcv_GetDuplexMode(uint8 TrcvIdx, EthTrcv_DuplexModeType *DuplexModePtr)
This function obtains the duplex mode of the indexed transceiver.