The rsqrtsp function returns the reciprocal square root function of a real floating-point argument a. The return value is the reciprocal value of the square root of a.
Parameters:
[in]
a
= Input float
Returns:
Resultant float
Special Cases:
If a <= 0, the return value is Inf for C/Inline/Vector.
If a <= 0, the return value is NaN or rsqrt(|a|) for Asm.