The rsqrtdp function returns the reciprocal square root function of a real floating-point argument a. The return value is the reciprocal value of the square root of a.
Parameters:
[in]
a
= Input double
Returns:
Resultant double
Special Cases:
If a <= 0, the return value is 8.99E307 for C/Inline/Vector and rsqrt(|a|) for Asm.