The coshdp function returns the hyperbolic cosine function of a real floating-point argument a. If the magnitude of a is too large, infinity is returned.
Parameters:
[in]
a
= Input double
Returns:
Resultant double
Special Cases:
If a > +710.475860073944, then the return value is INF