Asindp
Detailed Description
Function Documentation
double asindp_c |
( |
double |
a |
) |
|
- Description:
- The asindp function returns the arc sine of a floating-point argument a. The return value is an angle in the range [-PI/2, PI/2] radians.
- Parameters:
-
- Returns:
- Resultant float
- Special Cases:
- If a is not in the range [-1, 1], the return value is NaN (Not a Number).
- If a is NaN, the return value is NaN.
- See also:
-
- Implementation Notes:
- The code supports both big and little endian modes.
double asindp |
( |
double |
a |
) |
|
Copyright 2016, Texas Instruments Incorporated