![]() |
ETHFW API Guide
|
PPS config parameters.
Data Fields | |
uint32_t | tsrIn |
uint32_t | tsrOut |
uint64_t | ppsFreqHz |
uint32_t | genfIdx |
uint32_t EthFwTsn_PpsConfig::tsrIn |
TSR input interrupt num
uint32_t EthFwTsn_PpsConfig::tsrOut |
TSR output interrupt num
uint64_t EthFwTsn_PpsConfig::ppsFreqHz |
Frequency of PPS signal in Hz
uint32_t EthFwTsn_PpsConfig::genfIdx |
CPTS GenF instance to be used to generate PPS signal