ETHFW API Guide
EthFwMcast_RsvdMcast Struct Reference

Detailed Description

Reserved multicast.

Data Fields

uint8_t macAddr [ENET_MAC_ADDR_LEN]
 
uint16_t vlanId
 
uint32_t portMask
 

Field Documentation

◆ macAddr

uint8_t EthFwMcast_RsvdMcast::macAddr[ENET_MAC_ADDR_LEN]

Multicast address

◆ vlanId

uint16_t EthFwMcast_RsvdMcast::vlanId

VLAN id

◆ portMask

uint32_t EthFwMcast_RsvdMcast::portMask

Hardware port mask (Ethernet port and host port):

  • Use CPSW_ALE_MACPORT_TO_ALEPORT() to set the MAC port bitmask
  • Use CPSW_ALE_HOST_PORT_MASK to set the host port bitmask