![]() |
ETHFW API Guide
|
Data Structures | |
| struct | EthFwIET_Config |
| Ethernet Firmware IET config parameters. More... | |
Functions | |
| void | EthFwIET_notifyLinkChange (const Enet_MacPort macPort, const bool isLinkUp) |
| Notify Link Up down Event. More... | |
| void | EthFwIET_init (const EthFwIET_Config *ietCfg, Enet_Handle hEnet, uint32_t coreId) |
| API to updated the global object with params. More... | |
Macros | |
| #define | ETHFW_NUM_IET_VERIFY_ATTEMPTS (20U) |
| #define | CPSW_MACPORT_FIFO (8) |
| #define ETHFW_NUM_IET_VERIFY_ATTEMPTS (20U) |
No of Iteration to run to verify IET capability before timeout
| #define CPSW_MACPORT_FIFO (8) |
Number of FIFO queues per macPort
| void EthFwIET_notifyLinkChange | ( | const Enet_MacPort | macPort, |
| const bool | isLinkUp | ||
| ) |
Notify Link Up down Event.
Callback function to notify about mac port link up/down.
| macPort | macPort on which link changes is detected |
| isLinkUp | link is up or down |
| void EthFwIET_init | ( | const EthFwIET_Config * | ietCfg, |
| Enet_Handle | hEnet, | ||
| uint32_t | coreId | ||
| ) |
API to updated the global object with params.
| ietCfg | Params passed from application layer |
| hEnet | Ethernet handle |
| coreId | caller core id |