![]() |
![]() |
Collaboration diagram for DSPF_sp_cholesky_cmplx:
|
Modules | |
| DSPF_sp_cholesky_in_place_cmplx | |
| int | DSPF_sp_cholesky_cmplx (const int enable_test, const int Nrows, float *restrict A, float *restrict L) |
| int | DSPF_sp_cholesky_in_place_cmplx (const int enable_test, const int Nrows, float *restrict A) |
| int | DSPF_sp_cholesky_solver_cmplx (const int Nrows, float *restrict L, float *restrict y, float *restrict b, float *restrict x) |
| int DSPF_sp_cholesky_cmplx | ( | const int | enable_test, | |
| const int | Nrows, | |||
| float *restrict | A, | |||
| float *restrict | L | |||
| ) |
This function tests the square complex matrix A for a symmetric positive definite and decomposes the matrix A into a lower triangular matrix L where A=L*U and U=Hermitian of L. The values stored in the matrices are assumed to be single precision floating point values. This code is suitable for dense matrices. No optimizations are made for sparse matrices.
| enable_test | = enables test for symmetric positive definite matrix | |
| Nrows | = Nrows of square matrix A | |
| A | = pointer to square matrix A[Nrows*2*Nrows] | |
| L | = pointer to lower triangular matrix L[Nrows*2*Nrows] |
| int DSPF_sp_cholesky_in_place_cmplx | ( | const int | enable_test, | |
| const int | Nrows, | |||
| float *restrict | A | |||
| ) |
This function tests the square matrix A for a symmetric positive definite and decomposes the square matrix A into a lower triangular matrix L where A=L*U and U=transpose of L. The processing is done in place of the matrix A. The values stored in the matrices are assumed to be float precision floating point values. This code is suitable for dense matrices. No optimizations are made for sparse matrices.
| enable_test | = enables test for symmetric positive definite matrix | |
| Nrows | = Nrows of square matrix A | |
| A | = pointer to input square matrix A[Nrows*2*Nrows] and output matrix L[Nrows*2*Nrows] |
| int DSPF_sp_cholesky_solver_cmplx | ( | const int | Nrows, | |
| float *restrict | L, | |||
| float *restrict | y, | |||
| float *restrict | b, | |||
| float *restrict | x | |||
| ) |
This function solves A*x=b for x using forward and backward substitution using the decomposed lower triangular matrix L as shown in the following steps. The values stored in the matrices are assumed to be float precision floating point values. 1. A*x = L*U*b = L*L_transpose*x = b 2. y = inverse(L)*b - done using forward substitution 3. x = inverse(L_transpose)*y - done using backward substitution
| Nrows | = Nrows of square matrix A | |
| L | = pointer to input square matrix A[Nrows*2*Nrows] | |
| y | = pointer to intermediate vector y[2*Nrows] | |
| b | = pointer to input vector b[2*Nrows] | |
| x | = pointer to output vector x[2*Nrows] |