![]() |
![]() |
#include "assert.h"
#include "C6xSimulator.h"
#include "C6xSimulator_type_modifiers.h"
Include dependency graph for c66/DSPF_sp_vecadd.h:

Go to the source code of this file.
Defines | |
| #define | DSPF_SP_VECADD_H_ 1 |
Functions | |
| void | DSPF_sp_vecadd (float *restrict x, float *restrict y, float *restrict r, int nx) |
| #define DSPF_SP_VECADD_H_ 1 |
Definition at line 40 of file c66/DSPF_sp_vecadd.h.