![]() |
![]() |
#include "assert.h"
#include "C6xSimulator.h"
#include "C6xSimulator_type_modifiers.h"
Include dependency graph for c66/DSPF_sp_svd.h:

Go to the source code of this file.
Defines | |
| #define | MAX_ITERATION_COUNT 30 |
Functions | |
| int | DSPF_sp_svd (const int Nrows, const int Ncols, float *restrict A, float *restrict U, float *restrict V, float *restrict U1, float *restrict diag, float *restrict superdiag) |
| #define MAX_ITERATION_COUNT 30 |
Definition at line 42 of file c66/DSPF_sp_svd.h.