![]() |
![]() |
#include "assert.h"
#include "C6xSimulator.h"
#include "C6xSimulator_type_modifiers.h"
Include dependency graph for c66/DSP_mul32.h:

Go to the source code of this file.
Defines | |
| #define | DSP_MUL32_H_ 1 |
Functions | |
| void | DSP_mul32 (const int *restrict x, const int *restrict y, int *restrict r, int nx) |
| #define DSP_MUL32_H_ 1 |
Definition at line 40 of file c66/DSP_mul32.h.