105 #define CAN_VARIANT_PRE_COMPILE (STD_ON) 114 #define CAN_ISR_VOID (0x00U) 116 #define CAN_ISR_CAT1 (0x01U) 118 #define CAN_ISR_CAT2 (0x02U) 127 #define CAN_VERSION_INFO_API (STD_ON) 130 #define CAN_DEV_ERROR_DETECT (STD_ON) 133 #define CAN_SAFETY_DIAGNOSTIC (STD_ON) 136 #define CAN_LOOPBACK_ENABLE (STD_ON) 139 #define CAN_REGISTER_READBACK_API (STD_ON) 142 #define CAN_SET_BAUDRATE_API (STD_ON) 145 #define CAN_WAKEUP_FUNCTIONALITY_API (STD_OFF) 148 #define CAN_MULTIPLEXED_TRANSMISSION_ENABLE (STD_ON) 156 #define CAN_INIT_CONFIG_PC CanConfigSet 164 #define CAN_TX_POLLING (STD_OFF) 166 #define CAN_RX_POLLING (STD_OFF) 168 #define CAN_BUSOFF_POLLING (STD_OFF) 170 #define CAN_WAKEUP_POLLING (STD_OFF) 175 #define CAN_NUM_CONTROLLER (3U) 178 #define CAN_NUM_MAILBOXES (9U) 181 #define CAN_MAX_CONTROLLER (16U) 184 #define CAN_MAX_MAILBOXES (64U) 187 #define CAN_ISR_TYPE (CAN_ISR_CAT1) 190 #define CLK_CAN_FD_FREQ (80U) 199 #define CanConf_CanController_CanController_0 (0U) 200 #define CanConf_CanController_CanController_1 (1U) 201 #define CanConf_CanController_CanController_2 (2U) 207 #define CAN_CONTROLLER_MCU_MCAN0 210 #define CAN_CONTROLLER_MCU_MCAN1 213 #define CAN_CONTROLLER_MCAN0 302 #define CanConf_CanHardwareObject_CanHardwareObject_0 (0U) 303 #define CAN_HTRH_0 (CanConf_CanHardwareObject_CanHardwareObject_0) 305 #define CanConf_CanHardwareObject_CanHardwareObject_1 (1U) 306 #define CAN_HTRH_1 (CanConf_CanHardwareObject_CanHardwareObject_1) 308 #define CanConf_CanHardwareObject_CanHardwareObject_2 (2U) 309 #define CAN_HTRH_2 (CanConf_CanHardwareObject_CanHardwareObject_2) 311 #define CanConf_CanHardwareObject_CanHardwareObject_3 (3U) 312 #define CAN_HTRH_3 (CanConf_CanHardwareObject_CanHardwareObject_3) 314 #define CanConf_CanHardwareObject_CanHardwareObject_4 (4U) 315 #define CAN_HTRH_4 (CanConf_CanHardwareObject_CanHardwareObject_4) 317 #define CanConf_CanHardwareObject_CanHardwareObject_5 (5U) 318 #define CAN_HTRH_5 (CanConf_CanHardwareObject_CanHardwareObject_5) 320 #define CanConf_CanHardwareObject_CanHardwareObject_6 (6U) 321 #define CAN_HTRH_6 (CanConf_CanHardwareObject_CanHardwareObject_6) 323 #define CanConf_CanHardwareObject_CanHardwareObject_7 (7U) 324 #define CAN_HTRH_7 (CanConf_CanHardwareObject_CanHardwareObject_7) 326 #define CanConf_CanHardwareObject_CanHardwareObject_8 (8U) 327 #define CAN_HTRH_8 (CanConf_CanHardwareObject_CanHardwareObject_8) 334 #define CAN_OS_COUNTER_ID ((CounterType)OsCounter_0) 341 #define CAN_TIMEOUT_DURATION (10000U) 350 #ifndef CAN_E_HARDWARE_ERROR 352 #define CAN_E_HARDWARE_ERROR (DemConf_DemEventParameter_CAN_E_HARDWARE_ERROR) 376 extern const struct Can_ControllerStruct_PC
380 extern const struct Can_MailboxStruct_PC
409 extern CONST(uint32, CAN_CONST)
412 extern CONST(uint32, CAN_CONST)
415 extern CONST(uint32, CAN_CONST)
418 extern CONST(uint32, CAN_CONST)
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_1
CAN Controller Configuration Pre Compile struct declaration.
const uint32 Can_MsgmemRAMBaseAddr[CAN_MAX_CONTROLLER]
Base Address of the can peripherals.
#define CAN_NUM_CONTROLLER
Definition: Can_Cfg.h:175
Definition: Can_Cfg.h:400
#define CAN_NUM_MAILBOXES
Definition: Can_Cfg.h:178
void Can_2_Int0ISR(void)
MCAN0 Controller Instance ISR.
void Can_1_Int0ISR(void)
MCU_MCAN1 Controller Instance ISR.
const uint32 Can_MCANSSBaseAddr[CAN_MAX_CONTROLLER]
Can_ControllerInstance
Can Controller Instances enum.
Definition: Can_Cfg.h:389
void Can_0_Int0ISR(void)
MCU_MCAN0 Controller Instance ISR.
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_0
CAN Controller Configuration Pre Compile struct declaration.
Definition: Can_Cfg.h:391
#define CAN_MAX_CONTROLLER
Definition: Can_Cfg.h:181
const uint32 Can_MCANECCAggrRegBaseAddr[CAN_MAX_CONTROLLER]
const struct Can_ConfigType_s CanConfigSet
CAN Configuration struct declaration.
const struct Can_ControllerStruct_PC * CanConfigSet_CanController_List_PC[CAN_NUM_CONTROLLER]
CAN Controller Pre Compile Configuration List.
const struct Can_ControllerStruct_PC CanConfigSet_PC_CanController_2
CAN Controller Configuration Pre Compile struct declaration.
Definition: Can_Cfg.h:395
const struct Can_MailboxStruct_PC * CanConfigSet_CanHardwareObject_List_PC[CAN_NUM_MAILBOXES]
CAN Mailbox Pre Compile Configuration List.
const uint32 Can_MCANCoreRegBaseAddr[CAN_MAX_CONTROLLER]