99 #if (STD_ON == ADC_GROUP_LOG) 131 #if (STD_ON == ADC_FIFO_ERR_LOG) 164 #if (STD_ON == ADC_GROUP_LOG) 169 #if (STD_ON == ADC_FIFO_ERR_LOG) Adc_GroupType groupId
Definition: Adc_Dbg.h:108
Adc_GroupLogType Adc_GroupLogObj
ADC group log object.
Adc_HWUnitType hwUnitId
Definition: Adc_Dbg.h:142
Adc_FifoErrLogType Adc_FifoErrLogObj
ADC FIFO error log object.
uint32 timeStamp
Definition: Adc_Dbg.h:137
uint32 totalLog
Definition: Adc_Dbg.h:124
uint32 isReScheduled
Definition: Adc_Dbg.h:112
ADC FIFO error log structure.
Definition: Adc_Dbg.h:149
Adc_GroupType groupId
Definition: Adc_Dbg.h:140
uint8 Adc_HWUnitType
Specifies the identification (ID) for a ADC Hardware microcontroller peripheral (unit)
Definition: Adc.h:388
ADC log structure per FIFO error entry.
Definition: Adc_Dbg.h:135
Adc_HWUnitType hwUnitId
Definition: Adc_Dbg.h:110
#define ADC_MAX_GROUP_LOG
Maximum group log entries when logging is ON.
Definition: Adc_Cfg.h:143
#define ADC_MAX_FIFO_ERR_LOG
Maximum FIFO error log entries when logging is ON.
Definition: Adc_Cfg.h:149
uint8 Adc_GroupType
Numeric ID of an ADC channel group.
Definition: Adc.h:313
This file contains interface header for ADC MCAL driver.
uint32 totalLog
Definition: Adc_Dbg.h:153
uint32 logIndex
Definition: Adc_Dbg.h:151
ADC log structure per group entry.
Definition: Adc_Dbg.h:103
ADC group log structure.
Definition: Adc_Dbg.h:120
uint32 timeStamp
Definition: Adc_Dbg.h:105
uint32 logIndex
Definition: Adc_Dbg.h:122