4.7.5.1. Enet LLD LLDP User’s Guide

4.7.5.1.1. Pre-requisites

Reader are expected to have basic knowledge on below IEEE specifications - Standard ethernet (IEEE 802.1)

  • Link Layer Discovery Protocol - LLDP (IEEE 802.1AB-2016)

  • LLDP Amenment 1: YANG Data Model (IEEE 802.1ABcu-2021)

4.7.5.1.2. Introduction

This guide is intended to enhance user’s understanding of the LLDP stack and provide guidance on how to seamlessly integrate LLDP modules into their own applications.

4.7.5.1.3. TSN Stack

4.7.5.1.3.1. LLDP source modules

The TSN library is composed of the following source modules:

  • tsn_unibase: Universal utility libraries that are platform-independent.

  • tsn_combase: Communication utility libraries that provide support for functions like sockets, mutexes, and semaphores.

  • tsn_uniconf: Universal configuration daemon for Yang, provides APIs for developing a client application which retreives/writes yang parameters from/to database

  • tsn_lldp: Implementation of the IEEE 802.1 AB lldp protocol.

  • enet_tsn_lldp_example: Example application for LLDP

4.7.5.1.3.2. Stack Initialization

See Enet LLD TSN User’s Guide for detail LLDP stack initialization

4.7.5.1.4. LLDP Logging

See Enet LLD TSN User’s Guide for detail of how to configure LLDP log level

4.7.5.1.5. Integration

4.7.5.1.5.1. Source integration

See Enet LLD TSN User’s Guide for detail of how to integrate the lldp stack into your application

4.7.5.1.5.2. Uniconf configuration

See Enet LLD TSN User’s Guide for detail Uniconf’s configuration params which are used to configure LLDP

4.7.5.1.5.3. LLDP configuration parameters

This section describes the standard Yang parameters utilized for LLDP. The LLDP Yang structure is defined in IEEE 802.1ABcu 2021 Amendment 1: YANG Data Model.

To configure LLDP params, refer EnetApp_setLldpRtConfig which is generating per-system and per-port configurations.

For ex, to configure LLDP global timer values like tx-interval, fast init, …. User can update the table accordingly:

static EnetApp_DbNameVal_t gLldpGlobalData[] =
{
    {"message-fast-tx" , "1"},
    {"message-tx-hold-multiplier" , "4"},
    {"message-tx-interval" , "30"},
    {"reinit-delay" , "2"},
    {"tx-credit-max" , "5"},
    {"tx-fast-init" , "2"},
};

To update local information data which is use to build LLDPDU, User can update the table below accordingly:

static EnetApp_DbNameVal_t gLldpLocalSysData[] =
{
    // local system data
    {"chassis-id-subtype" , "7"}, // '7' mean local filled, in case of more than one ports, subtype='4' MAC address cannot apply.
    {"chassis-id" , "00-01-02-03-04-05"}, // Just a simple string in case of subtype is 'local (7)'
    {"system-name" , "tilld"},
    {"system-description" , "tilld"},
    {"system-capabilities-supported" , "11111111111"},
    {"system-capabilities-enabled" , "11110111011"},
};

Current LLDP application support up to 3 destination MAC Addresses per one port. The supported destination MAC Addresses should be match with LLDP 802.1AB specification :

  • Nearest bridge 01-80-C2-00-00-0E

  • Nearest non-TPMR bridge 01-80-C2-00-00-03

  • Nearest Customer Bridge 01-80-C2-00-00-00

To configure per-port/dest-mac information, User can update the table gLldpPortCfgData accordingly. These Destination MAC Addresses are corresponding to below configuration value:

static EnetApp_LldpPortCfg_t gLldpPortCfgData[] =
{
    {
        .dest_mac = "01-80-c2-00-00-0e",
        .cfg_kv =
        {
            {"admin-status", "3"},
            {"tlvs-tx-enable", "1111"},
            {"port-id-subtype", "3"},               // If PortId subtype = P_MAC_Address (3), MAC addr will be re-correct follow hw info.
            {"port-id", "3c-e0-64-62-e3-03"},       // <- this value will be correct in runtime
            {"port-desc", "tilld"},
            {"message-fast-tx", "2"},               // <- In case of any field missing, global value gLldpGlobalData will be used
            {"message-tx-hold-multiplier" , "4"},   // <- In case of any field missing, global value gLldpGlobalData will be used
            {"message-tx-interval" , "30"},         // <- In case of any field missing, global value gLldpGlobalData will be used
            {"reinit-delay" , "2"},                 // <- In case of any field missing, global value gLldpGlobalData will be used
            {"tx-credit-max" , "5"},                // <- In case of any field missing, global value gLldpGlobalData will be used
            {"tx-fast-init" , "2"},                 // <- In case of any field missing, global value gLldpGlobalData will be used
        }
    },
    {
        .dest_mac = "01-80-c2-00-00-03",
        .cfg_kv =
        {
            {"admin-status", "3"},
            {"tlvs-tx-enable", "1111"},
            {"port-id-subtype", "3"},               // If PortId subtype = P_MAC_Address (3), MAC addr will be re-correct follow hw info.
            {"port-id", "3c-e0-64-62-e3-03"},       // <- this value will be correct in runtime
            {"port-desc", "tilld"},
            {"message-fast-tx", "2"},               // <- In case of any field missing, global value gLldpGlobalData will be used
            {"message-tx-hold-multiplier" , "4"},   // <- In case of any field missing, global value gLldpGlobalData will be used
            {"message-tx-interval" , "20"},         // <- In case of any field missing, global value gLldpGlobalData will be used
            {"reinit-delay" , "2"},                 // <- In case of any field missing, global value gLldpGlobalData will be used
            {"tx-credit-max" , "5"},                // <- In case of any field missing, global value gLldpGlobalData will be used
            {"tx-fast-init" , "2"},                 // <- In case of any field missing, global value gLldpGlobalData will be used
        }
    },
    {
        .dest_mac = "01-80-c2-00-00-00",
        .cfg_kv =
        {
            {"admin-status", "3"},
            {"tlvs-tx-enable", "1111"},
            {"port-id-subtype", "3"},               // If PortId subtype = P_MAC_Address (3), MAC addr will be re-correct follow hw info.
            {"port-id", "3c-e0-64-62-e3-03"},       // <- this value will be correct in runtime
            {"port-desc", "tilld"},
            {"message-fast-tx", "2"},               // Diff with global system config
            {"message-tx-hold-multiplier" , "4"},   // <- In case of any field missing, global value gLldpGlobalData will be used
            {"message-tx-interval" , "25"},         // <- In case of any field missing, global value gLldpGlobalData will be used
            {"reinit-delay" , "2"},                 // <- In case of any field missing, global value gLldpGlobalData will be used
            {"tx-credit-max" , "5"},                // <- In case of any field missing, global value gLldpGlobalData will be used
            {"tx-fast-init" , "2"},                 // <- In case of any field missing, global value gLldpGlobalData will be used
        }
    },
};

In case of User want to support only one Destination MAC address, the entry of gLldpPortCfgData can be reduced accordingly.

4.7.5.1.6. Memory footprint

The memory footprint is extracted from the map file.

The size of the modules in bytes when built in release mode:

Code

RO data

RW data

unibase

4310

942

5473

combase

10256

3329

96004

lldp

22718

6345

46513

uniconf

59516

18429

127672

The size of the modules in bytes when built in debug mode:

Code

RO data

RW data

unibase

4704

1086

5473

combase

11228

2612

83039

lldp

27988

6345

46513

uniconf

63084

18422

127672