2.7. Release Notes - 08_05_00¶
2.7.1. Introduction¶
This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
2.7.2. What’s New¶
ID |
Description |
Module |
Supported Platforms |
---|---|---|---|
PDK-10979 |
UDMA : Support for scatter-gather list |
UDMA |
J721E, J784S4 |
ETHFW-1912 |
ENET LLD : support DMA Scatter gather TX functionality |
ENET |
J721E |
ETHFW-1953 |
CPSW: lwIP: Checksum offload support |
ENET |
J721E |
ETHFW-2027 |
mdio: MDIO CDC errata (i2329) workaround implementation (CPSW) |
ENET |
J721E |
2.7.3. Upgrade and Compatibility¶
2.7.3.1. CSL¶
CSL ARM R5 Cache operation APIs now accepts a third argument wait, to specify if the function should wait or not until the operation is completed.
Old
New
CSL_armR5CacheWb(const void * addr, int32_t size)
CSL_armR5CacheWb(const void * addr, int32_t size, bool wait)
CSL_armR5CacheWbInv(const void * addr, int32_t size)
CSL_armR5CacheWbInv(const void * addr, int32_t size, bool wait)
CSL_armR5CacheInv(const void * addr, int32_t size)
CSL_armR5CacheInv(const void * addr, int32_t size, bool wait)
Added new API CSL_armR5CacheWait. This can be used to wait for the previous cache wb/wbInv/inv operation to complete.
For performance optimizations, following CSL cache line operation functions will not invoke memory barrier instructions. Instead end user is supposed to handle the same after updating all the required cache lines.
CSL_armR5CacheInvalidateDcacheMva
CSL_armR5CacheCleanDcacheMva
2.7.3.2. OSAL¶
taskFxn paramater for TaskP_Create is updated from type ‘void*’ to function pointer of type TaskP_Fxn
i.e, TaskP_create expects a function pointer of prototype
void ( * TaskP_Fxn )( void *arg0, void *arg1 )
name param in TaskP_Params is updated from type uint8_t * to const char *
CycleprofilerP_getTimeStamp does not check for R5F PMU counter overflow and refresh the PMU counter higher bits.
In case of FreeRTOS, OS tick timer handles this internally by periodically checking for R5F PMU counter overflow and refresh the higher bits of PMU counter in the event of any overflow.
In SafeRTOS and Baremetal, this is not handled by default.
A new API, CycleprofilerP_refreshCounter is added to check for R5F PMU counter overflow and refresh the higher bits of PMU counter in the event of any overflow.
Baremetal/SafeRTOS applications can periodically invoke the new API CycleprofilerP_refreshCounter to handle R5F PMU counter overflow.
2.7.3.3. VHWA¶
- MSC
VHWA_M2M_MSC_MAX_INPUT_BUFF macro is removed and instead a new macro VHWA_M2M_MSC_MAX_IN_CHANNEL is added.
Following parameters in Vhwa_M2mMscSl2AllocPrms structure is updated from a single dimensional array of size VHWA_M2M_MSC_MAX_INPUT_BUFF to a multi-dimensional array of size VHWA_M2M_MSC_MAX_INST x VHWA_M2M_MSC_MAX_IN_CHANNEL
maxInWidth
inCcsf
inBuffDepth
Applications should update the initialization accordingly.
isInterleaveFormat parameter which was earlier present in CSL_MscConfig structure is now moved to Msc_ScConfig in include/msc_cfg.h
Applications should update the initialization accordingly.
2.7.3.4. Sciclient / TIFS¶
SYSFW/TIFS have added new PSIL host id verification check. Due to this RM PSIL messages from mcu1_0 should use MSG forwarding instead of sending the message to TIFS directly.
mcu1_0 will always be in secure mode when trying to send the message to TIFS directly, to avoid self blocking. And all the BoardCfg RM entries for mcu1_0 are for default non-secure host id. Hence for this case, the new PSIL host id verification will fail.
By using MSG forwarding, it retains the host id information of the non-secure/secure mode of mcu1_0. Setting forwarding ensures that the mcu1_0 uses the DM2DMSC secure proxy threads. NOTE: Forwarding always leads to forced polling.
For all other default base-port and security messages, mcu1_0 can be in secure mode and send the message to TIFS directly.
2.7.3.5. CSI¶
App can select the source CSIRX instance to re-transmit to a specific CSITX instance using newly added lpbkCsiRxInst parameter in Csitx_InstCfg structure.
Added a new parameter enableStrm in Csirx_CreateParams. Previously all supported streams were enabled by default, now this info should be provided by the application.
2.7.3.6. SBL¶
Migrated boot app (a tertiary boot loader) from MCUSW to PDK. This app can be used to boot any HLOS like QNX, Linux, etc. More details on BootApp migration at Boot App
2.7.4. Device Support¶
J721E SR1.1, J721E-HS SR1.1 (BOARD=j721e_evm)
Associated TIFS versions:
TIFS name
J721E SR revision
tifs.bin
SR1.0 & SR1.1 GP
tifs-hs-enc.bin
SR1.0 HS
tifs-sr1.1-hs-enc.bin
SR1.1 HS
2.7.5. Validation Information¶
For details on the validated examples refer to the platform specific test report available here.
2.7.6. Tool Chain Information¶
Component |
Version |
---|---|
FreeRTOS Kernel tag |
V10.4.3 |
lwIP stack |
2.1.2 |
lwIP-contrib |
2.1.0 |
TI ARM CLANG |
1.3.0.LTS |
PRU code generation tools |
2.3.3 |
GCC ARM code generation tools |
ARCH64 9.2-2019.12 |
CGT XML Processing Scripts |
2.61.00 |
System Analyzer (UIA Target) |
2_30_01_02 |
Component |
Version |
---|---|
TI C6x code generation tools |
8.3.7 |
TI C7x code generation tools |
3.0.0.STS |
2.7.7. Change Request¶
Refer to monthly roadmap slides for changes in the planned features
2.7.8. Fixed Issues¶
ID |
Head Line |
Module |
Affected Versions |
Affected Platforms |
---|---|---|---|---|
SBL SMP multicore boot test fails with SYSFW rearch |
SBL |
07.01.00 |
J721E-HS, J7200-HS |
|
SBL prebuild binary for J721E HS doesn’t work from package |
SBL |
07.03.00 |
J721E-HS |
|
SPI instance should be decided by SPI driver and not Board Module |
OSPI |
08.01.00 |
J721E, J7200 |
|
keywriter: smek gets generated even when argument not specified |
Security |
08.01.00 |
J721E, J7200 |
|
CSI-Rx UT hangs when run on mcu2_0 |
CSI2RX |
08.02.00 |
J721E, J721S2 |
|
Remove MCU Only mode demo code from MCUSW Boot App |
LPM |
08.02.00 |
J721E |
|
SBL: MCU2_0 or MCU3_0 cannot be booted in LockStep mode |
SBL |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
|
[CSIRX]: RAW12 packed output format is not working |
CSI2RX |
08.02.00 |
J721E, J721S2, J784S4 |
|
taskFxn parameter is not pointer to function in TaskP_create |
OSAL |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
|
UART performance issues in polling mode |
UART |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
|
[OSAL]: Incorrect type for TaskP_Params.name variable |
OSAL |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
|
DM: UART Traces are not working with Linux SDK |
PM |
08.02.00 |
J721E, J7200 |
|
SBL: HS boot flow should unlock ROM firewalls |
SBL |
08.02.00 |
J721E |
|
Incorrect DDR End Address with ECC enabled |
BOARD |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
|
Re-transmission should be enabled by default in CSL MCAN application |
CSL |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
|
Incorrect parameter check in Dss_m2mDrvDispPipeCfgChk API |
DSS |
08.02.00 |
J721E |
|
[CSIRX]: Incorrect powerup sequence |
CSI2RX |
08.04.00 |
J721E, J721S2, J784S4 |
|
Fix event manager pipe assignment for mutliple pipe scenario |
DSS |
08.04.00 |
J721E |
|
[CSL-R5F] Incorrect usage of DMB and DSB for cache operations |
CSL |
08.04.00 |
J721E, J7200, J721S2, J784S4 |
|
IPC RPMessage_recv() timeout issue |
IPC |
08.04.00 |
J721E, J7200, J721S2, J784S4 |
|
CSC config get over-written for DSS and DSS_M2M |
DSS |
08.04.00 |
J721E |
|
Wrong variable name in makerules_spec documentation |
COMMON |
08.04.00 |
J721E, J7200, J721S2, J784S4 |
|
Enet: SGMII TX/RX not enabled at 100Mbps |
ENET |
08.04.00 |
J721E, J7200, J784S4 |
2.7.9. Known Issues¶
ID |
Head Line |
Module |
Reported in Release |
Affected Platforms |
Impact |
Workaround in this release |
---|---|---|---|---|---|---|
Pulsar (R5F) : High priority interrupt is missed by VIM |
CSL, OSAL |
07.00.00 |
J721E, J7200 |
Baremetal implementation is pending |
Use RTOS instead of baremetal |
|
UART : Potential interrupt storm |
UART |
07.02.00 |
J7200, J721E |
Error interrupt resulting in hang. |
None |
|
[SPI] DMA mode does not work for SPI5 |
McSPI |
07.01.00 |
J721E |
Cannot use DMA with SPI5 |
Disable DMA for SPI5 OR use another instance of SPI |
|
[SPI] Transfer stalls when transfer length is not multiple of FIFO length in DMA mode |
McSPI |
07.02.00 |
J721E |
Cannot transfer data if data size is not multiple of FIFO length in DMA mode |
Use transfer size in multiple of FIFO length |
|
UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader. |
UDMA |
07.01.00 |
J721E |
Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader. |
Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5. |
|
MCU/Main NAVSS UDMA memcpy from L2SRAM fails |
UDMA |
07.00.00 |
J721E |
Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location |
Use ring memory from non-L2SRAM location |
|
Output mismatch when each region requiring 3 TRs |
VHWA |
01.00.00 |
J721E |
In multi-region mode with more then 3 TR per region can’t be used |
In multi-region mode for each region less than 3 TR should be used |
|
Sciclient Firewall Testapp Fails on HS Device |
SCICLIENT |
07.03.00 |
J721E-HS |
None |
None |
|
IPC Performance Test hangs after loading the binary |
IPC |
08.01.00 |
J721E, J7200 |
The app won’t work for this release |
None |
|
MCU Only Mode: IPC attachment with remote cores fail |
LPM |
08.02.00 |
J721E |
None |
None |
|
MCU Only Mode - Linux boot fails on A72 core |
LPM |
08.02.00 |
J721E |
None |
None |
|
USART: Spurious DMA Interrupts |
UART |
08.04.00 |
J721E, J7200, J721S2 |
None |
None |
|
USART: Erroneous clear/trigger of timeout interrupt |
UART |
08.02.00 |
J721E, J7200, J721S2 |
None |
None |
|
Heap OSAL hangs if previous allocation has buffer overflow |
OSAL |
08.02.00 |
J721E, J721S2 |
None |
None |
|
Main Domain GPIO does not service interrupts |
GPIO |
08.04.00 |
J721E, J7200 |
None |
None |
|
[DSS] HPD Pulse event is not handled in the eDP driver |
DSS |
08.02.00 |
J721E, J721S2, J784S4 |
None |
None |
|
IPC: stack corruption of taskWaiter used in RPMessage_getRemoteEndPt |
IPC |
08.00.00 |
J721E, J7200, J721S2, J784S4 |
None |
Make taskWaiter element as global |
|
SciServer: Multiple definition of Hwi Data |
SCICLIENT |
08.04.00 |
J721E, J7200, J721S2, J784S4 |
None |
None |
|
CSIRX: Incorrect DATA Shift value for RAW8 mode |
CSI2RX |
08.04.00 |
J721E, J721S2, J784S4 |
None |
None |
|
CSIRX: Incorrect Dual Pixel mode for YUV422 |
CSI2RX |
08.04.00 |
J721E, J721S2, J784S4 |
None |
None |
|
DSS: rxBuffer range check missing in DP_mailbox |
DSS |
08.04.00 |
J721E, J721S2, J784S4 |
DP sink module should not send message > 1 KB size |
None |
|
MCSPI DMA does not support 48bit address space |
MCSPI |
08.04.00 |
J721E, J7200, J721S2, J784S4 |
MCSPI is limited to 32 bit address space |
None |
|
FreeRTOS taskLoad is not proper |
OSAL |
08.02.00 |
J721E, J7200, J721S2, J784S4 |
Task load calculations could be wrong |
None |
|
Non-supported Sciclient APIs are present in header files |
SCICLIENT |
08.04.00 |
J721E, J7200, J721S2, J784S4 |
None |
None |
|
Assertion from EnetMcm_coreAttach API |
ENET |
08.01.00 |
J721E, J7200, J784S4 |
Race condition in MCM cmd handling in ETHFW usecases |
None |
|
Cable connect/disconnect can cause CPSW unrecoverable condition |
ENET |
08.00.00 |
J721E, J7200, J784S4 |
Packets will be dropped on the affected MAC port |
None. Device reboot is required |
2.7.10. Limitations¶
2.7.10.1. PDK¶
PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.
TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J721E
For Baremetal and SafeRTOS, in case of usage of CycleprofilerP APIs the R5F PMU counter overflow is not handled by default.
Applications can periodically use the CycleprofilerP_refreshCounter to check overflow and refresh the higher bits of the PMU counter.
2.7.10.2. ENET¶
Scatter-gather functionality is currently supported only for packet transmission.
2.7.10.3. SafeRTOS¶
None.