2.9. Release Notes - 08_02_00

2.9.1. Introduction

This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

2.9.2. What’s New

ID

Description

Module

Supported Platforms

PDK-10498

MCU only mode: IPC re-attached after MAIN domain restart

IPC

J721E

PDK-5377

SERDES sharing - support for configuring SERDES in R5-SBL

SBL

J721E

PDK-10808

Memory benchmark applications should be part of the standard SDK

COMMON

J721E, J7200

2.9.3. Upgrade and Compatibility

2.9.3.1. FreeRTOS

  • By default all the tasks will be created with floating point context enabled; i.e, save/restore of FPU Registers will be performed during each task switch.

  • Until last release, this was not enabled and any task that required floating point hardware had to call portTASK_USES_FLOATING_POINT.

For more details, refer Task FPU context

2.9.4. Device Support

  • J721E EVM SR1.0 and SR1.1, J721E-HS EVM (BOARD=j721e_evm)

  • Associated TIFS versions:

    TIFS name

    J721E SR revision

    tifs.bin

    SR1.0 & SR1.1 GP

    tifs-hs-enc.bin

    SR1.0 HS

    tifs-sr1.1-hs-enc.bin

    SR1.1 HS

2.9.5. Validation Information

For details on the validated examples refer to the platform specific test report available here.

2.9.6. Tool Chain Information

Component

Version

FreeRTOS Kernel tag

V10.4.3

lwIP stack

2.1.2

lwIP-contrib

2.1.0

TI ARM CLANG

1.3.0.LTS

PRU code generation tools

2.3.3

GCC ARM code generation tools

ARCH64 9.2-2019.12

CGT XML Processing Scripts

2.61.00

System Analyzer (UIA Target)

2_30_01_02

Component

Version

TI C6x code generation tools

8.3.7

TI C7x code generation tools

2.1.1.LTS

2.9.7. Change Request

ID

Head Line

Original Fix Version

New Fix Version

PDK-10708

PDK Support for XIP with ECC enabled

08.02.00

09.00.00

PDK-9473

Safety Compliance for SCICLIENT

08.02.00

08.06.00

PDK-9351

Example to configure Timer Manager module

08.02.00

09.00.00

PDK-5381

R5-SBL - Support to dump EEPROM to shared memory

08.02.00

08.06.00

PDK-9540

Defer DDR Register Write Verification to later stage

08.02.00

08.04.00

PDK-5365

Board: ECC support in BOARD OSPI Flash Driver

08.02.00

09.00.00

JACINTOREQ-2449

C7x/C66x SafeRTOS support descope

08.02.00

08.04.00

JACINTOREQ-2439

Ethernet: Defer CPSW EST and IET features in Enet LLD and EthFw

08.02.00

09.0x.00

2.9.8. Fixed Issues

ID

Head Line

Module

Affected Versions

Affected Platforms

PDK-10844

Conflicting library definitions for __mpu_init() when using Clang compiler

CSL

08.01.00

J721E, J7200, AM65xx

ETHFW-1904

Enet: High packet drop in iperf UDP test

ENET

08.01.00

J721E, J7200, AM65xx

PDK-11084

SBL should avoid hardcoding 0xBAD00000 in many places

SBL

08.01.00

J721E, J7200, AM65xx

PDK-11005

The number of McSPI instances are only 5 in SPI driver

McSPI

08.01.00

J721E, J7200, AM65xx

PDK-11011

IPC: Documentation is ambiguous w.r.t buffer size

IPC

08.01.00

J721E, J7200, AM65xx

PDK-11018

LPM module is incorrectly packaged in SDK8.1

LPM

08.01.00

J721E, J7200

PDK-11169

LPM module uses SBL_INVALID_CORE instead of SBL_INVALID_ID

LPM

08.01.00

J721E, J7200

PDK-11233

XIP memory benchmarking app fails for J721e/J7200

CSL

08.01.00

J721E, J7200

PDK-11236

DDR dual core memory benchmarking app is not working for J721e/J7200

CSL

08.01.00

J721E, J7200

PDK-11452

XIP dual core memory benchmarking app is not working for J721e/J7200

CSL

08.01.00

J721E, J7200

PDK-6549

MCU2 core diagnostic tests not running through sbl

BOARD

07.00.00

J721E

PDK-6548

Display port (eDP) diagnostic test failure

BOARD

07.00.00

J721E

PDK-10533

MCU only mode: handler for TISCI_MSG_SYS_RESET should clear current owner from ACL for MAIN cores

SCICLIENT

08.00.00

J721E

PDK-10537

[CSITX]: Infinite loop when initializing csitx driver, in lane ready function

CSI2TX

07.03.00

J721E

PDK-10518

Incorrect bin file for encrypting binary image

COMMON

07.03.00

J721E

PDK-10342

[DSSM2M] DSS M2M driver does not return error for unsupported format

DSS

07.03.00

J721E

PDK-11007

Semaphore not deleted in capture driver

CSI2RX

08.01.00

J721E

PDK-11008

Windows Build in SDK8.1 fails due to dependency on xdctools_3_61_04_40_core

COMMON

08.01.00

J721E

PDK-11010

SBL: Combined boot image: Seeing seg-fault when including all 8 remote core images

SBL

08.01.00

J721E

PDK-11015

OSAL: TimerP module restricts usage of up to max 4 DMTimer for R5Fs

OSAL

08.01.00

J721E

PDK-11176

Memory Benchmarking App does not finish on MCU2_0

CSL

08.01.00

J721E

2.9.9. Known Issues

ID

Head Line

Module

Reported in Release

Affected Platforms

Impact

Workaround in this release

PDK-6975

Pulsar (R5F) : High priority interrupt is missed by VIM

CSL, OSAL

07.00.00

J721E, J7200, AM65xx

Baremetal implementation is pending

Use RTOS instead of baremetal

PDK-8320

ICSS V1 CSL not up to date with ICSSG

CSL

07.00.00

J721E, AM65xx

None

Patch available. Will be included in next release

PDK-9676

UART : Potential interrupt storm

UART

07.02.00

J7200, J721E

Error interrupt resulting in hang.

None

PDK-9696

[SPI] DMA mode does not work for SPI5

McSPI

07.01.00

J721E

Cannot use DMA with SPI5

Disable DMA for SPI5 OR use another instance of SPI

PDK-9571

[SPI] Transfer stalls when transfer length is not multiple of FIFO length in DMA mode

McSPI

07.02.00

J721E

Cannot transfer data if data size is not multiple of FIFO length in DMA mode

Use transfer size in multiple of FIFO length

PDK-8407

J721E: MCU Timer 0 is not usable from application (sysbios) with SBL

OSAL, SBL

07.01.00

J721E

None

Use any other timer

PDK-8300

UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader.

UDMA

07.01.00

J721E

Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader.

Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5.

PDK-6789

MCU/Main NAVSS UDMA memcpy from L2SRAM fails

UDMA

07.00.00

J721E

Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location

Use ring memory from non-L2SRAM location

PDK-5228

Output mismatch when each region requiring 3 TRs

VHWA

01.00.00

J721E

In multi-region mode with more then 3 TR per region can’t be used

In multi-region mode for each region less than 3 TR should be used

PDK-9528

SBL prebuild binary for J721E HS doesn’t work from package

SBL

07.03.00

J721E-HS

None

Cleanup the SBL library and re-build the SBL image for HS. Commands: - Clean sbl_lib_uart (make sbl_lib_uart_clean) - Build for HS (make -sj sbl_uart_img_hs)

PDK-10292

Sciclient Firewall Testapp Fails on HS Device

SCICLIENT

07.03.00

J721E-HS

None

None

PDK-10925

IPC Performance Test hangs after loading the binary

IPC

08.01.00

J721E, J7200, AM65xx

The app won’t work for this release

None

PDK-10314

[DSS]: Add support for lane speed for the DSI output

DSS

07.03.00

J721E

DSI driver cannot be used for different lane speeds

None

PDK-11085

SPI instance should be decided by SPI driver and not Board Module

OSPI

08.01.00

J721E, J7200, AM65xx

None

None

PDK-11152

SPI driver does not support all instances with SPI_open

McSPI

08.02.00

J721E, J7200, AM65xx

Customer cannot use all SPI instances supported by SoC

None

PDK-11388

[SBL] SBL should not copy build folder contents to board folder during packaging

SBL

08.01.00

J721E, J7200, AM65xx

None

None

PDK-11093

ACK/NACK is send for TISCI messages without AOP flag

Sciclient

08.01.00

J721E, J7200

None

None

PDK-11240

keywriter: smek gets generated even when argument not specified

Security

08.01.00

J721E, J7200

None

None

PDK-11227

UART instances 3-9 does not work on MAIN R5 in interrupt mode

UART

08.01.00

J721E, J7200

User needs to add interrupt configuration

None

PDK-11004

DMA Utils examples are broken with SDK

UDMA

08.00.00

J721E

None

User can run example with FreeRTOS

PDK-11022

Sciclient_pmSetModuleClkFreq returns fail when called from SBL_SlaveCoreBoot for c66

SBL

08.00.00

J721E

None

None

PDK-11130

M2M colour space conversion from RGB24 to YUV420SP fails

DSS

08.02.00

J721E

None

None

PDK-11158

CSL: Sierra SerDes Instance 1 Lane Control is Incorrect

CSL

08.01.00

J721E

None

None

PDK-11238

DSS M2M testapp fails when run for scaling

DSS

08.02.00

J721E

None

None

PDK-11270

Facing issue with resolution change in DSS_M2M node

DSS

08.01.00

J721E

None

None

PDK-11457

MCU Only Mode: IPC attachment with remote cores fail

LPM

08.02.00

J721E

None

None

PDK-11458

MCU Only Mode - Linux boot fails on A72 core

LPM

08.02.00

J721E

None

None

2.9.10. Limitations

2.9.10.1. PDK

  • PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.

  • TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J721E

2.9.10.2. ENET

  • lwIP stack integration doesn’t support checksum hardware-offload feature.