2.12. Release Notes - 07_03_00

2.12.1. Introduction

This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.

New features added / supported is listed below and defects fixed are highligted in Fixed Issues also please check Upgrade and Compatibility for backward compatibility

2.12.2. What’s New

PDK-5257

Support Windows Package for Core SDK

BUILD

J721E, J7200

PDK-9312

FreeRTOS Support on R5F for CPU

OSAL

J721E, J7200

PDK-8726

OSPI Cache Support

OSPI

J721E, J7200

PDK-9263

J721E HS-EVM Support

COMMON

J721E

PDK-5179

DSS FVID2 Writeback M2M Driver

DSS

J721E

PDK-9321

DSS M2M: Single Channel Support

DSS

J721E

PDK-9320

DSS M2M: Chrominance Subsampling - YUV422 to YUV420

DSS

J721E

PDK-9319

DSS M2M: Color Space Conversion - RGB to YUV

DSS

J721E

PDK-5211

DSS M2M: Color Space Conversion - YUV to RGB

DSS

J721E

PDK-5184

DSS Writeback Pipeline Support

DSS

J721E

PDK-9317

DDR: Support for Thermal Testapp on MAIN Domain R5 cores

DDR

J721E

2.12.3. Upgrade and Compatibility

2.12.3.1. emac

  • pdk/packages/ti/drv/emac Will be deprecated in subsequent release

  • From SDK versioned v07.03.00, enet drivers support ICSSG ports too

  • emac is replaced by enet drivers

2.12.3.2. Sciclient

  • The Sciclient Sciclient_service API does not accept NULL pointers for the pRespPayload and expects the respPayloadSize to be the size of the structure pointed to by pRespPayload.

2.12.3.3. BoardCfg RM

  • Removed the shared resource allocation(entries for both secure and non_secure context) for MCU R5(mcu1_0) in default BoardCfg RM. MCU R5(mcu1_0) resource entries are only for non-secure host ID. This is because, Messages forwarded from DM must originate from a non-secure host in the system. Any secure host ID used during a forwarded request will be rejected as a spoofing attempt. Hence, Sciclient should be initialized in non-secure mode. ie, Sciclient_ConfigPrms_t->isSecureMode shouldn’t be set to 1U

2.12.3.4. ENET

  • txPktTc and txTsId fields have been added to EnetUdma_PktInfo for ICSSG peripheral usage. They are not required for CPSW. No action needed for applications using CPSW peripheral that initialize EnetUdma_PktInfo via EnetDma_initPktInfo(), otherwise must explicity set txPktTc to ENET_TRAFFIC_CLASS_INV.

  • Added ENET_TIMESYNC_IOCTL_TS_TO_NS ioctl command to convert timestamp values to nanoseconds values. This IOCTL is not required for packet timestamping in CPSW peripheral.

  • Following IOCTLs have been renamed:

    • CPSW_IOCTL_[UN]REGISTER_RX_DEFAULT_FLOW to ENET_IOCTL_[UN]REGISTER_RX_DEFAULT_FLOW.

    • CPSW_IOCTL_[UN]REGISTER_DSTMAC_RX_FLOW to ENET_IOCTL_[UN]REGISTER_DSTMAC_RX_FLOW.

  • Mdio_Cfg has added isMaster field for cases where MDIO module is shared with multiple peripherals, so only one peripheral (master) must perform the MDIO initial configuration and be skipped by the other peripherals (slaves). This is not needed by applications using CPSW.

2.12.3.5. Board Library

2.12.3.6. Board Diagnostics

Board diagnostic test framework which integrates diagnostic tests into menu based execution is no longer supported. This module is meant for board manufacturers and not validated as part of the SDK.

Board diagnostic tests serve as reference for board bring-up and they are not recommended to be used as reference for production software development.

2.12.4. Device Support

  • J721E EVM SR1.0 and SR1.1, J721E-HS EVM (BOARD=j721e_evm)

  • Associated TIFS versions: - ‘tifs.bin’ for J721E SR1.0 and SR1.1 GP devices - ‘tifs-hs-enc.bin’ for J721E-HS SR1.0 - ‘tifs-sr1.1-hs-enc.bin’ for J721E-HS SR1.1

sysfw name

AM65xx SR revision

sysfw.bin

SR1.0

sysfw-hs-enc.bin

SR1.0 HS

sysfw_sr2.bin

SR2.0 & SR2.1

sysfw_sr2-hs-enc.bin

SR2.0 HS & SR2.1 HS

2.12.5. Validation Information

For details on the validated examples refer to the platform specific test report available here.

2.12.6. Tool Chain Information

Component

Version

Sys Bios

6_83_02_07

XDC Tools

3_61_04_40_core

Network Development Kit (NDK)

3_80_00_19

Network Services for NDK (NS)

2_80_00_17

TI ARM R5F code generation tools

20.2.0.LTS

PRU code generation tools

2.3.3

GCC ARM code generation tools

ARCH64 9.2-2019.12

CGT XML Processing Scripts

2.61.00

System Analyzer (UIA Target)

2_41_00_01

Component

Version

TI C6x code generation tools

8.3.7

TI C7x code generation tools

1.4.2.LTS

2.12.7. Fixed Issues

ID

Head Line

Module

Affected Versions

Affected Platforms

PDK-5040

Display stops working if two pipelines are started back to back

DSS

06.02.00

J721E

PDK-6534

Timer osal - noos - Timer should be reset first before registering interrupts

OSAL

06.02.00

J721E

PDK-8537

Sciclient_rmIrqRelease API is failing

SCICLIENT

07.01.00

J721E

PDK-8502

Uniflash flash programmer failure in DMA mode

BOARD

07.01.00

J721E, AM65xx

PDK-8311

Recent DDR config update to 4266 MT/s causing DDR memory failures on some boards

BOARD

07.01.00

J721E

PDK-6649

Timer osal - noos - Timer delete doesn’t “free” timer

OSAL

06.02.00

J721E

PDK-7048

Master Slave: Data corruption in mode 0

McSPI

07.01.00

J7200

PDK-8586

Early CAN response measurement is beyond 50 ms for J721E

SBL

07.01.00

J721E

PDK-9240

SBL fails to initialize DDR after warm reset

BOARD, SBL

07.01.00

J721E

PDK-8945

Interrupts are disabled globally in Sciclient_service API

SCICLIENT

07.00.00

J721E

PDK-9328

OSPI tuning calculation fails in linear search algorithm

OSPI

07.02.00

J721E

PDK-8598

ospi flash test fails when the ospi memory is cachable

OSPI

07.01.00

J721E, J7200

PDK-8226

R5FSS: The same interrupt cannot be nested back-2-back within another interrupt

CSL

07.00.00

J721E, AM65xx

PDK-6848

osal - task delete function should check for deleteTerminatedTasks flag

OSAL

07.00.00

J721E, J7200

PDK-6706

McSPI : Driver Master example is not functional

McSPI

07.00.00

J721E, AM65xx

PDK-8932

PMIC: Pmic Handle Critical Section Stop Function validation check is incorrect

PMIC

07.01.00

J721E, J7VCL

PDK-8863

PMIC: Critical Section causing hang in Pmic_gpioIntrDisable API

PMIC

07.02.00

J721E, J7200

PDK-8131

PMIC: Asynchronous Interrupt tests failure on Main domain R5 Cores

BOARD

07.01.00

J7200

PDK-9050

Diag : Hyperbus : is not functional

CSL, DIAG

07.01.00

J721E

2.12.8. Known Issues

ID

Head Line

Module

Reported in Release

Affected Platforms

Impact

Workaround in this release

PDK-9748

USB : 3.0 : Hagiwara drive : fails to enumerate as 3.0 : once in 250 times average

USB 3.0

07.00.00

AM65xx

Hagiwara USB 3.0 devices may not be enumerated as 3.0

Consider operating in 2.0 mode

PDK-9750

USB: USB3.0 enumeration failing for some of the adapters

USB 3.0

07.00.00

AM65xx

Some of USB 3.0 devices may not be enumerated as 3.0

Consider operating in 2.0 mode

PDK-9751

PCIE-0 : Gen 3 : Intermittent failures during Gen 3 mode on AM65x PG2.0

PCIe

07.00.00

AM65xx

GEN 3 mode is stable

Use GEN 2 mode

PDK-8946

McSPI : All data words not transmitted in FIFO, interrupt mode when length not divisible by FIFO

McASP

07.01.00

AM65xx

In Complete data transfers

Transfer length should be multiple of FIFO depth

PDK-9717

AM65xx : SA2UL : Demo application is not functional

SA2UL

07.03.00

AM65xx

SA2UL Is not functional

None

PDK-8846

[DSS Test]Sync-lost is observed for RGB24/BGR24 test-cases

DSS

07.01.00

AM65xx

No images displayed on the screen / flicker

None

PDK-8841

csl_cbass_baremetal_test_app fails on QoS Test

CBAS

07.01.00

AM65xx

None

None

PDK-6742

McASP regression test app some tests are failing

CBAS

07.00.00

AM65xx

None

None

PDK-8166

MMCSD read/write failure with 1.8V - no I/F to program timings params

MMC/SD

07.00.00

AM65xx

Requires timing update in driver io != 3.3v

None

PDK-5224

Active DP -> HDMI adapter doesn’t work

DSS

00.09.01

J721E

DP to HDMI adapter for display cannot be used.

None

PDK-6992

Display flickers for BT601 output format

DSS

07.00.00

J721E

None

PDK-8320

ICSS V1 CSL not up to date with ICSSG

CSL

07.00.00

J721E, AM65xx

None

Patch available. Will be included in next release

PDK-9437

Increase in Boot time when DDR ECC is enabled

BOARD

07.02.00

J721E, J7200

Increase in boot time

Use UDMA for priming the DDR.

PDK-9456

I2C Driver does not return error when camera/client is not available on the I2C bus

I2C

07.02.00

J721E

Application continues even if sensors programming has failed.

None

PDK-9433

MASTER _BYPASS bit in PHY_MASTER_CONTROL should be controlled based on the clock

OSPI

07.01.00

J721E

None

None

PDK-6975

Pulsar (R5F) : High priority interrupt is missed by VIM

CSL, OSAL

07.00.00

J721E, J7200, AM65xx

Baremetal implementation is pending

Use SYSBIOS instead of baremetal

PDK-8407

J721E: MCU Timer 0 is not usable from application (sysbios) with SBL

OSAL, SBL

07.01.00

J721E

None

Use any other timer

PDK-8300

UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader.

UDMA

07.01.00

J721E

Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader.

Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5.

PDK-6789

MCU/Main NAVSS UDMA memcpy from L2SRAM fails

UDMA

07.00.00

J721E

Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location

Use ring memory from non-L2SRAM location

PDK-5228

Output mismatch when each region requiring 3 TRs

VHWA

01.00.00

J721E

In multi-region mode with more then 3 TR per region can’t be used

In multi-region mode for each region less than 3 TR should be used

PDK-5226

DOF generated wrong output with SOF if pixel in all row are not enabled

VHWA

01.00.00, 00.09.01

J721E

When using the SOF if the Paxel rows without any pixel enabled is not in consecutive pair with lead to lead to output mismatch

This issue is due to shift in flowvector out buffer. While generating the SOF binary map make sure that Paxel rows without any pixel enabled should be in consecutive pair

PDK-5217

VPAC VISS driver doesn’t support several valid mux combinations for outputs

VHWA

01.00.00, 00.09.01

J721E

VISS output with Chroma only and one of the RGB component enabled may not work

Enable YUV420 instead of Chroma only while using RGB component

ETH-1534

[CPSW] Packet drop with QSGMII ports IPerf

Enet

06.02.00

J721E, J7200

None

None

ETH-1670

mcu2_1: loopback: Test fails to setup interrupts in iteration 2

Enet

07.01.00

J721E

None

Avoid restarting Enet LLD on J721E mcu2_1 core

PRSDK-5074

McASP driver hangs with small buffer size

McASP

05.01.00

J721E, AM65xx

None

Use packet size 32 samples or greater

PDK-6549

MCU2 core diagnostic tests not running through sbl

BOARD

07.00.00

J721E

None

Use CCS/JTAG to run the tests

PDK-6548

Display port (eDP) diagnostic test failure

BOARD

07.00.00

J721E

None

Use display sample application

PDK-8577

PMIC: Asynchronous Interrupt tests failure on Main domain R5 Cores and mcu1_1 core

BOARD

07.01.00

J721E

None

Use Polled mode

PDK-9426

ECAP CSL Capture Event Counter Reset Function Fails

CSL

07.03.00

J721E, J7200

None

None

PDK-8601

CSL ECC test application fails on J721E and J7200

CSL

07.01.00

J721E, J7200

None

None

PDK-9528

SBL prebuild binary for J721E HS doesn’t work from package

SBL

07.03.00

J721E-HS

None

Cleanup the SBL library and re-build the SBL image for HS. Commands: - Clean sbl_lib_uart (make sbl_lib_uart_clean) - Build for HS (make -sj sbl_uart_img_hs)

PDK-8653

CSI2-RX: Stream FIFO Overflow observed for 4 channel input with FrameSync

CSI2-RX

06.02.00

J721E

Multi-channel capture with FrameSync cannot be used.

None

PDK-8600

SBL optimizations for OSPI boot mode

SBL

07.00.00

J721E

None

None

PDK-9490

OSPI_Baremetal_Flash_Dma_TestApp fails on mpu1_0 in release mode

OSPI

07.03.00

J7200

None

None

ETHFW-1810

icssg: RX ch teardown timed out observed in NIMU restart

ENET

07.03.00

AM65XX

Low - observed during shutdown sequence

None

ETHFW-1747

enet: icssg: Incorrect rxTxTotalByte in unicast test

ENET

07.03.00

AM65XX

Low - network statistics, no functional impact

None

ETHFW-1767

timesync: v2: TimeSync PTP restart is not supported

ENET

07.03.00

AM65XX

Impacts only applications that require stack restart

None

ETHFW-1809

DUT stopped forwarding frames in one direction

ENET

07.03.00

AM65XX

Firmware doesn’t handle long burst of packets at line rate

None

2.12.9. Limitations

2.12.9.1. PDK

  • PDK examples do not supported SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.

2.12.9.2. ENET

  • ICSSG integration with NDK is done only for ICSSG Dual-MAC. Driver level support is available for Dual-MAC and Switch.

  • TimeSync PTP integration is done only for ICSSG-Dual MAC.

  • TimeSync is possible only in one MAC port at a time.

  • Different VLAN modes are not supported in Dual-MAC mode (within given ICSSG MAC ports). Both MACs should either be in VLAN aware or VLAN unaware mode.

  • Independent VLAN learning is not supported in Dual-MAC mode.