![]() |
VXLIB User Guide
|
Kernels available within VXLIB.
Sub Modules | |
VXLIB_absDiff | |
Kernel for calculating absolute difference of two input images. | |
VXLIB_accumulateImage | |
Kernel for adding the input image to the output image. This kernel has no internel implementation. Instead, it calls the VXLIB_add kernel implementation. | |
VXLIB_accumulateSquareImage | |
Kernel for adding the square of one image to the output image. This kernel has no internel implementation. Instead, it calls the addSqure kernel implementation. | |
VXLIB_accumulateWeightImage | |
Kernel for weighted accumulation of input image and output image. This kernel has no internel implementation. Instead,it calls the VXLIB_addWeight kernel implementation. | |
VXLIB_add | |
Kernel for adding two input vector data. | |
VXLIB_addSquare | |
Kernel for adding the square of one image to another image. | |
VXLIB_addWeight | |
Kernel for weighted addition of two input vector data. | |
VXLIB_and | |
Kernel for computing bitwise and of two input vector data. | |
VXLIB_box | |
Kernel for applying kxk boxFilter on input image. | |
VXLIB_convertDepth | |
Kernel for converting bit depth of images from 16-bit to 8-bit and 8-bit to 16-bit. | |
VXLIB_convolve | |
Kernel for applying filterHeight x filterWidth convolution filter on input image, scaled by constant, and saturating the output to the output datatype numeric limits. | |
VXLIB_dilate | |
Kernel for applying an M x N dilate operation on an input image. | |
VXLIB_gaussian | |
Kernel for applying kxk gaussian filter on input image. | |
VXLIB_halfScaleGaussian | |
Kernel for applying 5x5 half scale gaussian filter on input image. | |
VXLIB_histogram | |
Kernel for creating a histogram distribution from an image based on a given given offset, range, and number of bins. | |
VXLIB_magnitude | |
Kernel for adding two input vector data. | |
VXLIB_meanStdDev | |
Kernel for computing the mean and standard deviation of input vector. | |
VXLIB_median | |
Kernel for computing the median pixel over a window of imput image, for each pixel. | |
VXLIB_minMaxLoc | |
Kernel for finding minimum and maximum values in an image and a location for each. | |
VXLIB_multiply | |
Kernel for multiplying two input vector data. | |
VXLIB_normL1 | |
Kernel for computing the L1 norm of given 2 signed inputs, resulting in an unsigned norm result. | |
VXLIB_normL2 | |
Kernel for computing the L2 norm of given 2 signed inputs resulting in an unsigned norm result. | |
VXLIB_not | |
Kernel for computing bitwise not of two input vector data. | |
VXLIB_or | |
Kernel for computing bitwise or of two input vector data. | |
VXLIB_subtract | |
Kernel for subtracting two input vector data. | |
VXLIB_tableLookup | |
Kernel for mapping an input pixel value to another value via lookup table. | |
VXLIB_thresholdBinary | |
Kernel for Thresholding an input image and produces an output Boolean image. | |
VXLIB_thresholdRange | |
Kernel for Thresholding an input image and produces an output Boolean image. | |
VXLIB_xor | |
Kernel for computing bitwise xor of two input vector data. | |