MATHLIB Release Notes
Version: 09.02.00.04
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Deprecation
- Known Issues
- Technical Support
- Package Versioning
Introduction
The MATHLIB package consists of the Texas Instruments optimized kernels for floating point Math algorithms.
Licensing
The licensing information of this library and a complete manifest along with export control information is detailed here [HTML].
Getting Started
The MATHLIB User Guide [USER_GUIDE] provides the documentation and references necessary to begin development on TI's platforms. Currently, Windows build is not supported.
Documentation
Refer to following documentation for further details:
| MATHLIB User Guide | Build instructions, API Guide | [USER_GUIDE] |
| Software Manifest | Licenses, terms of use | [HTML] |
What's New
API changes from 02_06_01_00:
MATHLIB no longer has <kernel>_init and <kernel>_exec functions. Its replaced with a single API. For example, MATHLIB_cos_init and MATHLIB_cos_exec do not exist anymore. Instead, they are replaced with one API in MATHLIB_cos. The SE0/SA0 settings which was previously a part of MATHLIB_init is now part of MATHLIB_cos.
In order to perform elementwise cosine of a given vector, please call MATHLIB_cos as follows:
MATHLIB_cos(length, in, out); where, 'length' is the size of input vector pointed to by buffer pointer 'in', and 'out' is the pointer to buffer with elementwise cosine of input vector. Please refer to <mathlib root>/examples/<kernel>/<kernel>_example.cpp for more details on how to call the API.
New Kernels:
- MATHLIB_atanh
- MATHLIB_sinh
- MATHLIB_cosh
- MATHLIB_acosh
- MATHLIB_exp10
- MATHLIB_tanh
- MATHLIB_rsqrt
Upgrade and Compatibility Information
| File | Change description | User application change required | User application recompile required |
Device Support
| SoC | Host (OS) | Target (OS) | Test Platform |
| C7x | No OS | No OS |
Validation Information
This release was built and validated using the following tools:
Build Tools (NOT included in MATHLIB):
- C7x CGT C7000-CGT-4.1.0.LTS
Supported Kernels
- [XLIB-21] MATHLIB_cosh single precision
- [XLIB-23] MATHLIB_tanh single precision
- [XLIB-19] MATHLIB_rsqrt single precision
- [XLIB-22] MATHLIB_sinh single precision
- [XLIB-14] MATHLIB_atanh single precision
- [XLIB-12] MATHLIB_acosh single precision
- [XLIB-17] MATHLIB_exp10 single precision
- [XLIB-15] MATHLIB_atan2 single precision
- [XLIB-13] MATHLIB_asinh single precision
- [XLIB-2] MATHLIB_sin single precision
- [XLIB-6] MATHLIB_atan single precision
- [XLIB-7] MATHLIB_div single precision
- [XLIB-5] MATHLIB_asin single precision
- [XLIB-4] MATHLIB_acos single precision
- [XLIB-8] MATHLIB_sqrt single precision
- [XLIB-3] MATHLIB_tan single precision
Fixed Issues
Known Issues
Technical Support
For technical support, please post your questions on TI E2E Forum for Processors.
For additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b
[M.m.p.b]. The table below provides a descriptive reference regarding package version
numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2023, Texas Instruments Incorporated