Imaging Release Notes
Version: 09.02.00
Contents
- Introduction
- Licensing
- Getting Started
- Documentation
- What's New
- Upgrade and Compatibility Information
- Device Support
- Supported Image Sensors PSDK RTOS
- Supported Image Sensors EdgeAI
- Supported Image Sensors by Third Party
- Validation Information
- Fixed Issues
- Change Requests
- Known Issues
- Technical Support
- Package Versioning
Introduction
The Imaging package consists of the Texas Instruments OpenVX conformant implementation for J7 EVM and AM6xA EVM platforms
Licensing
The licensing information of this library, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here [HTML].
Getting Started
The Imaging User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using Imaging.
Documentation
Refer to following documentation for further details:
| Imaging User Guide for J7 and AM6xA | Build instructions, additional information related to J7 and AM6xA platform | [HTML] |
| Software Manifest | Licenses, terms of use | [HTML] |
| ISP Tuning Guide for J7/TDA4 | Work flow of tuning the ISP related to J7/TDA4 platform | [HTML] |
| ISP Tuning Guide for AM6xA | Work flow of tuning the ISP related to AM6xA platform | [HTML] |
| Tuning Tool Request Form | Tuning Tool Request Form | [LINK] |
| Static Analysis Report | C and C++ Taxonomy Report | [XLSX] |
| Bidirectional Traceability Report | Mapping of requirements to test cases | [XLSX] |
| Test Reports | Conformance test reports, TI platform test reports | [XLSX] |
What's New
Here is a list of the new feature(s) supported in this release:
- IMX390 Discovery module narrow, mid, and wide sensor driver support
- Note: Only sensor driver was added. Tuning will come from D3 in future release
- OX05B driver and tuning on AM62A-SK board
- Imaging support on J722S (IMX219, IMX390, OV2312, AR0233)
- DCC Tuning Tool v3.1 is verified for J722S (VPAC3L). This includes live tuning
- Added PC Emulation support for J722S and AM62A
Upgrade and Compatibility Information
Device Support
| SoC | HOST (OS) | Target (OS) | Test Plaform |
| J7 | x86_64 (Linux) | A72 (Linux) | J721E/J721S2/J722S/J784S4 EVM + Fusion board Revision 1C and 2. Older Fusion boards are not supported. |
| AM6xA | x86_64 (Linux) | A53 (Linux) | AM62A EVM |
Supported Image Sensors PSDK RTOS
| Image Sensor | Max Instances | Supported Platform | Module | Ordering Info |
| IMX390 | 8 Note: j784s4 + Fusion2 can support up to 12 |
J721E/J721S2/J722S/J784S4 EVMs | D3RCM-IMX390-953 | D3RCM-IMX390-953 |
| AR0233 | 1 | J721E/J721S2/J784S4 EVMs | MARS (MARS1-TI953-GEVK, MARS1-AR0233ATSCS-GEVB) | Please contact OnSemi |
| AR0820 | 1 | J721E/J721S2/J784S4 EVMs | LI-AR0820-FPDLINKIII | LI-AR0820-FPDLINKIII |
| GW5200-AR0233 YUV422 | 1 | J721E/J721S2/J784S4 EVMs | LI-GW5200-AR0233 | LI-GW5200-AR0233 |
| IMX390 DesignCore® Discovery Series (55° HFOV, 100° HFOV, 174° HFOV) | 4 | J721E/J721S2/J784S4 EVMs + Fusion1 | IMX390 DesignCore® Discovery Series | IMX390 DesignCore® Discovery Series |
Supported Image Sensors EdgeAI
Only DCC XML and binary configuration files are provided in Imaging for the sensors listed below. V4L2 Sensor drivers are provided by Processor SDK Linux.
Supported Image Sensors by Third Party
The listed sensors are supported by third-parties.
| Image Sensor | Max Instances | Module | Ordering Info |
| IMX623 | 1 | Sony module w/ SR1069A Lens | Please contact Sony for SDK 8.1 driver Registration flow | Developer World (sony.com) |
Validation Information
This release was built and validated using the following tools:
Build Tools (included in Processor SDK RTOS):
- ARM R5F Code Generation Tools version: Same as Processor SDK RTOS
Dependencies (included in Processor SDK RTOS):
- TIOVX version: Same as Processor SDK RTOS
- VXLIB version: Same as Processor SDK RTOS
- Processor SDK RTOS version: 09.02.00
Fixed Issues
| ID | Summary |
|---|---|
| ISS-498 | Some IMX390 Camera Modules output corrupted images in Multi Cam app on j784s4 + Fusion2 |
| ISS-504 | Fcp_EeConfig.lut is of type int32_t instead of int16_t |
| ISS-506 | default_DCC_profile_gen python script does not support user input of pre-gamma |
| ISS-507 | VISS node unnecessarily copies several DCC tables |
| ISS-509 | Unnecessary cache invalidate call after VISS config dma completion |
| ISS-510 | Nsf4HistLutConfig.tableAddr is of type uint32_t instead of uint16_t |
| ISS-530 | Multi-cam app shows black screen on AEN |
| ISS-542 | VPAC3L DPC mode is not backward compatible |
| ISS-546 | Define a macro for the number of knee-points in DPC LUT |
| ISS-548 | CAC, RAWHIST and CFAI3 were not considered valid VISS dcc plugins for VPACv3L |
| ADASVISION-6205 | [J7AEN] Multicam demo does not display when graphics enabled |
| SITSW-3484 | Incorrect configuration of LSEOUT_MUX_CNTL and IR_OUT_CNTL for VPAC3L from TIOVX. |
| SITSW-3549 | Change signatures of the functions Fvid2Utils_memset() and Fvid2Utils_memcpy() for VPAC3L Host emulation support on AM62A and J7AEN |
| SITSW-3632 | [VISS] Two and Three frame merge test cases are disabled on J7AEN and AM62A |
| SITSW-3656 | LSC module is not properly applied to image |
| SITSW-3680 | 16bit IR only output is not valid. |
Change Requests
- Scope In - None.
- Scope Out - None.
- Scope Modifications - None.
Known Issues
| ID | Summary |
|---|---|
| ADASVISION-4923 | Single cam error on ports other than port 1 after running multi cam |
| ADASVISION-5774 | Glitches seen on stereo app for J784S4 with safertos |
| ADASVISION-6080 | Multi Cam application capture error |
| ADASVISION-6243 | app_dof does not work or compile properly on j722s |
| ADASVISION-6243 | app_stereo does not show graphics or compile properly on j722s |
| ISS-288 | AR0820 Camera does not work with Fusion-2 board |
| ISS-371 | [VISS]: VISS node does not support histogram module |
| ISS-474 | Interpolation method should be configurable from Imaging for VPAC3L |
| ISS-497 | Imaging CAC conformance tests are disabled. |
| ISS-515 | RGBIr test case failure on J7AEN |
| ISS-529 | single-cam app freezes with IMX390 running at 60fps |
| ISS-547 | Multi-cam app doesn't exit clean on AEN |
| ISS-549 | GLBCE ctx save/restore is not enabled for J722S |
| SITSW-1663 | VISS tiovx conformance tests resulting in hang after process request transfer to VPAC driver |
| SITSW-3179 | DPC_STATS_CFG is not configurable from VHWA |
Technical Support
For technical support and additional assistance, contact E2E Forum
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.
| Digit | Meaning | Description |
|---|---|---|
| 1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
| 2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
| 3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
| 4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2024, Texas Instruments Incorporated