2.6. Release Notes - 08_01_00

2.6.1. Introduction

This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

2.6.2. What’s New

ID

Description

Module

Supported Platforms

JACINTOREQ-1168

SDK shall support migration to LLVM/TI CLANG

COMMON

J721E, J7200, AM65XX

JACINTOREQ-473

MCU only mode - Ability to restart Main domain

LPM

J721E

JACINTOREQ-1162

PDK shall support FreeRTOS on the C7x for CPU

FreeRTOS

J721E

PDK-10387

PDK OSAL Support for FreeRTOS on C66x/C7x

OSAL

J721E

JACINTOREQ-1229

PDK shall support migration of C6x/C7x drivers to FreeRTOS

COMMON

J721E

PDK-9714

FreeRTOS ROV Support

FreeRTOS

J721E

PDK-9546

SafeRTOS Support on R5 for CPU

SafeRTOS

J721E

PDK-9534

PDK shall support running SafeRTOS Integration Tests running on R5F

SafeRTOS

J721E

JACINTOREQ-1098

PMIC LLD shall configure voltage, current, power good and thermal monitor

PMIC

J721E, J7200

JACINTOREQ-1090

PMIC LLD shall support Watchdog in Trigger and Q&A Mode

PMIC

J721E, J7200

JACINTOREQ-1086

PMIC LLD shall support TPS6594x Leo PMIC

PMIC

J721E, J7200

JACINTOREQ-1092

PMIC LLD shall decipher error events and call out to application with error code

PMIC

J721E, J7200

JACINTOREQ-1097

PMIC LLD shall support CRC

PMIC

J721E, J7200

JACINTOREQ-1088

PMIC LLD shall support I2C and SPI communication interface

PMIC

J721E, J7200

JACINTOREQ-1104

PMIC LLD shall support PFSM states

PMIC

J721E, J7200

JACINTOREQ-1094

PMIC LLD shall support Low Power modes

PMIC

J721E, J7200

JACINTOREQ-1089

PMIC LLD shall configure RTC for PMIC low power

PMIC

J721E, J7200

JACINTOREQ-1416

PMIC LLD shall support DDR Retention mode

PMIC

J721E, J7200

JACINTOREQ-1091

PMIC LLD shall configure GPIO Pin Functionality

PMIC

J721E, J7200

JACINTOREQ-1093

PMIC LLD shall configure BUCK and LDO regulator output voltages

PMIC

J721E, J7200

JACINTOREQ-1103

PMIC LLD shall support ESM for MCU and SOC Errors

PMIC

J721E, J7200

JACINTOREQ-494

Enet LLD: CPSW Inter clients (cores) packet communication

ENET

J721E, J7200

ETHFW-1711

Enet LLD: Support MAC only mode of operation for few CPSW switch ports

ENET

J721E, J7200

2.6.3. Upgrade and Compatibility

2.6.3.1. FreeRTOS

  • This release introduces FreeRTOS Support for J721E PDK Drivers/Examples on C66x/C7x cores.

  • PDK drivers/examples are migrated and validated with FreeRTOS running in C66x/C7x cores.

  • FreeRTOS is not supported on A72 core.

  • FreeRTOS support is availble on all other cores. ( R5F, C66x, C7x )

  • FreeRTOS Real-time Object View (ROV) in CCS IDE is available for R5F, C66x cores.

See FreeRTOS Chapter for more details.

2.6.3.2. TI-RTOS(SysBIOS)

  • TI-RTOS(SysBIOS) is not supported on any cores from this release.

  • RTOS support on A72 is also descoped.

2.6.3.3. NDK

  • TI’s NDK TCP/IP stack is no longer supported on any cores.

  • lwIP is now the only TCP/IP stack supported in this release.

2.6.3.4. OSAL

Following OSAL APIs which supported only TI-RTOS(SysBIOS) are descoped in this release.

  • EventP
    • EventP_pend()

    • Migrate to similar API EventP_wait() which is supported for FreeRTOS

  • QueueP

    Descoped API

    Alternative API

    Osal_Queue_Handle

    QueueP_Handle

    Osal_Queue_Elem

    QueueP_Elem

    Osal_Queue_construct + Osal_Queue_handle

    QueueP_create

    Osal_Queue_put

    QueueP_put

    Osal_Queue_get

    QueueP_get

    Osal_Queue_empty

    QueueP_isEmpty

2.6.3.5. TI-CLANG

  • This release introduces TI ARM Clang tool-chain/compiler for MCU R5 cores

  • PDK drivers/examples are migrated from TI ARM CGT and validated with TI ARM Clang tool-chain.

  • Note: TI ARM Clang tool chain generated code/binary size is more than that of TI ARM CGT.

See TI ARM CLANG Usage and Migration Guidelines Chapter for more details.

2.6.3.6. LPM

  • LPM library provides APIs to transistion the SoC and PMIC from ACTIVE to MCU only mode and vice-versa.

  • SoC’s such as J721E, integrates a Micro Controller Unit Subsystem (MCU SS) as a chip-in-chip.

  • It can operate fully isolated from rest of the chip using a separate voltage supply, clock sources and resets and include the components needed for device management.

  • This allows the MCU SS to function continuously regardless of the state of the rest of the device.

  • Depending on the application needs, MCU only mode can be used for:

    1. Reset & recovery of main domain functionality in case of detected failure.

    2. As a low power mode of operation where in functionality implemented in MCU mode continues to be operational while rest of chip is powered down. In this case Software running on MCU domain can detect and process wakeup events and in response can reload and restart applications running in Main domain

  • See LPM Chapter for more details.

2.6.4. Device Support

  • J721E EVM SR1.0 and SR1.1, J721E-HS EVM (BOARD=j721e_evm)

  • Associated TIFS versions:

    TIFS name

    J721E SR revision

    tifs.bin

    SR1.0 & SR1.1 GP

    tifs-hs-enc.bin

    SR1.0 HS

    tifs-sr1.1-hs-enc.bin

    SR1.1 HS

2.6.5. Validation Information

For details on the validated examples refer to the platform specific test report available here.

2.6.6. Tool Chain Information

Component

Version

FreeRTOS Kernel

10.5.1

lwIP stack

2.1.2

lwIP-contrib

2.1.0

TI ARM CLANG

1.3.0.LTS

PRU code generation tools

2.3.3

GCC ARM code generation tools

ARCH64 9.2-2019.12

CGT XML Processing Scripts

2.61.00

System Analyzer (UIA Target)

2_30_01_02

Component

Version

TI C6x code generation tools

8.3.7

TI C7x code generation tools

2.0.1.STS

2.6.7. Change Request

ID

Head Line

Original Fix Version

New Fix Version

JACINTOREQ-1595

PDK: XIP With OTFA Support Descope

08.01.00

None

JACINTOREQ-2037

PMIC Safety requirements needs to be moved to 8.2 release

08.01.00

08.02.00

JACINTOREQ-1861

SBL - Support to dump EEPROM is deferred to 8.2 release

08.01.00

08.02.00

JACINTOREQ-1860

SERDES sharing feature in SBL deferred to 8.2 release

08.01.00

08.02.00

JACINTOREQ-1596

PDK: C6x/C7x SafeRTOS support descope

08.01.00

08.02.00

2.6.8. Fixed Issues

ID

Head Line

Module

Affected Versions

Affected Platforms

PDK-8601

CSL ECC test application fails on J721E

CSL

07.01.00

J721E

PDK-9947

[CSIRX]: hangs is observed when re-running example with different number of channels

CSIRX

07.03.00

J721E

ETHFW-1845

Examples: MAC loopback app test causes abort in debug mode during restart

ENET

08.00.00

J721E

ETHFW-1534

[CPSW] Packet drop with QSGMII ports IPerf

ENET

06.02.00

J721E, J7200

PDK-10377

PLL1, PLL3 not enabled after MCU only to Active mode switch

SCICLIENT

08.00.00

J721E

PDK-10871

[DSS_M2M]: Assertion is observed in the DSS M2M driver when using it in multi-handle mode

DSS

08.00.00

J721E

PDK-10536

CUST SBL with SBL_SKIP_MCU_RESET should release MCU R5 before jumping to application

SBL

08.00.00

J721E

PDK-10528

C66 Cache OSAL for nonos is not optimal for larger buffers

OSAL

08.00.00

J721E

PDK-10524

MCU only mode: IPC re-attached after MAIN domain restart

IPC

08.00.00

J721E

PDK-10523

eDP firmware responds wrongly to some messages

DSS

08.00.00

J721E

PDK-10425

Make for sbl_multicore_amp fails with proper last core of mpu1_1

SBL

08.00.00

J721E, J7200, AM65xx

PDK-10423

IPC: RPMessage heap is sized wrong and is causing heap corruption of Rx messages

IPC

08.00.00

J721E, J7200, AM65xx

PDK-10880

[DSS] Incorrect offset calculation in DSS for H/V flip

DSS

08.00.00

J721E

2.6.9. Known Issues

ID

Head Line

Module

Reported in Release

Affected Platforms

Impact

Workaround in this release

PDK-6975

Pulsar (R5F) : High priority interrupt is missed by VIM

CSL, OSAL

07.00.00

J721E, J7200, AM65xx

Baremetal implementation is pending

Use RTOS instead of baremetal

PDK-8320

ICSS V1 CSL not up to date with ICSSG

CSL

07.00.00

J721E, AM65xx

None

Patch available. Will be included in next release

PDK-9676

UART : Potential interrupt storm

UART

07.02.00

J7200, J721E

Error interrupt resulting in hang.

None

PDK-9696

[SPI] DMA mode does not work for SPI5

McSPI

07.01.00

J721E

Cannot use DMA with SPI5

Disable DMA for SPI5 OR use another instance of SPI

PDK-9571

[SPI] Transfer stalls when transfer length is not multiple of FIFO length in DMA mode

McSPI

07.02.00

J721E

Cannot transfer data if data size is not multiple of FIFO length in DMA mode

Use transfer size in multiple of FIFO length

PDK-8407

J721E: MCU Timer 0 is not usable from application (sysbios) with SBL

OSAL, SBL

07.01.00

J721E

None

Use any other timer

PDK-8300

UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader.

UDMA

07.01.00

J721E

Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader.

Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5.

PDK-6789

MCU/Main NAVSS UDMA memcpy from L2SRAM fails

UDMA

07.00.00

J721E

Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location

Use ring memory from non-L2SRAM location

PDK-6549

MCU2 core diagnostic tests not running through sbl

BOARD

07.00.00

J721E

None

Use CCS/JTAG to run the tests

PDK-6548

Display port (eDP) diagnostic test failure

BOARD

07.00.00

J721E

None

Use display sample application

PDK-5228

Output mismatch when each region requiring 3 TRs

VHWA

01.00.00

J721E

In multi-region mode with more then 3 TR per region can’t be used

In multi-region mode for each region less than 3 TR should be used

PDK-9528

SBL prebuild binary for J721E HS doesn’t work from package

SBL

07.03.00

J721E-HS

None

Cleanup the SBL library and re-build the SBL image for HS. Commands: - Clean sbl_lib_uart (make sbl_lib_uart_clean) - Build for HS (make -sj sbl_uart_img_hs)

PDK-10292

Sciclient Firewall Testapp Fails on HS Device

SCICLIENT

07.03.00

J721E-HS

None

None

PDK-10533

MCU only mode: handler for TISCI_MSG_SYS_RESET should clear current owner from ACL for MAIN cores

SCICLIENT

08.00.00

J721E

None

None

PDK-10537

[CSITX]: Infinite loop when initializing csitx driver, in lane ready function

CSI2TX

07.03.00

J721E

Driver hangs in failure scenario instead of timeout

None

PDK-10518

Incorrect bin file for encrypting binary image

COMMON

07.03.00

J721E

None

None

PDK-10925

IPC Performance Test hangs after loading the binary

IPC

08.01.00

J721E, J7200, AM65xx

The app won’t work for this release

None

PDK-10844

Conflicting library definitions for __mpu_init() when using Clang compiler

CSL

08.01.00

J721E, J7200, AM65xx

User should link libraries in correct order

Ensure ti.csl.init.aer5f is the first library included and use –priority flag

PDK-10342

[DSSM2M] DSS M2M driver does not return error for unsupported format

DSS

07.03.00

J721E

User can pass wrong inputs to driver and driver will not throw error

User should pass correct parameters

PDK-10314

[DSS]: Add support for lane speed for the DSI output

DSS

07.03.00

J721E

DSI driver cannot be used for different lane speeds

None

ETHFW-1904

Enet: High packet drop in iperf UDP test

ENET

08.01.00

J721E, J7200, AM65xx

iperf UDP test will not run successfully

None

2.6.10. Limitations

2.6.10.1. PDK

  • PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.

  • TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J721E

  • C++ build is not supported in this release for TI Clang compiler. It will be added back in next release.

2.6.10.2. ENET

  • lwIP stack integration doesn’t support checksum hardware-offload feature.