2.11. Release Notes - 06_02_00

2.11.1. Introduction

This release notes provides important information that will assist you in using the PDK software package. This document provides the product information and known issues that are specific to the PDK software package.

2.11.2. What’s New

  • CPSW
    • SGMII mode

    • QSGMII mode

    • CPTS time stamping

    • Hardware-offload checksum

    • PHY MII loopback

    • Debug and diagnostic features

    • Debug GEL files: SGMII config, diagnostic, status

  • CSI2 RX
    • Added Error handling and recovery support

    • Driver now can recover from CRC, ECC, FIFO overflow and Data ID errors

  • CSI2 TX
    • Added FVID2 CSIRX driver support

    • Validated RAW8, RAW12, RGB888, YUV422 data formats with single channel transmit on J721E EVM.

  • DSS
    • Added DSS DSI Support

2.11.3. Upgrade and Compatibility

  • CPSW
    • PHY loopback configuration parameter renamed from isLoopback to CpswPhy_Config.enableLoopback

    • QSGMII is no longer part of CpswMac_VariantType. Two sub-layer types are now used to describe QSGMII interface: CpswMac_SublayerType.CPSW_MAC_SUBLAYER_QUAD_SERIAL_MAIN and CpswMac_SublayerType.CPSW_MAC_SUBLAYER_QUAD_SERIAL_SUB

2.11.4. Device Support

  • J721E EVM (BOARD=j721e_evm)

2.11.5. Validation Information

This release is validated on J721E EVM for the applicable components. For details on the validated examples refer to the platform specific test report present in PDK_INSTALL_DIR/docs/test_report folder.

2.11.6. Tool Chain Information

Refer to SDK level documentation for Tool Chain and dependent component version used to validate this release.

2.11.7. Fixed Issues

ID

Head Line

Module

Affected Versions

Affected Platforms

PRSDK-7120

SPI master slave test fails in non-dma callback mode

PDK

PROCESSOR-SDK_06.01.00

J721E

PRSDK-7713

Proxy access causes hard fault in the MCU2_0

SCIClient

PROCESSOR-SDK_06.01.00

J721E

PRSDK-5935

Flashing speed for OSPI with Uniflash 5.0 is very poor (about 7KB/s)

UNIFLASH

PROCESSOR-SDK_05.03.00

J721E

PRSDK-7495

Userguide updates for J7 Uniflash are missing

UNIFLASH

PROCESSOR-SDK_06.01.00

J721E

ADASVISION-3275

cpsw - Nimu example hangs if CPSWNIMUAPP_RESTART_PERIOD is low

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3277

cpsw - RTOS/Baremetal loopback test fails in second iteration - mcu2_1/mcu2_0

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3280

Cpsw2G - Interrupts won’t work for main domain cores(mcu2_1, mpu1_0)

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3282

cpsw - mpu1_0 loopback test fails for heap memory match

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3283

cpsw nimu - dma descriptor not freed error

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3285

CPSW: Cpsw_handleLinkUp assert randomly

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3290

[CPSW] [UT]Max Rx frame payload size limited to 1486 instead of 1500 if RxFlowPrms rxMtu not explicitly configured

CPSW

SDK_J7_00_09_01_00

J721E

ADASVISION-3785

[cpsw] Incorrect memcpy for macport list in mcm & CPSW examples

CPSW

SDK_J7_01_00_00_00

J721E

ADASVISION-3799

CPSW: PHY loopback fails with RMII PHY in GESI board

CPSW

SDK_J7_06_01_01

J721E

ADASVISION-3867

CPSW Nimu - assert in cpsw memutils due to descriptor mismatch

CPSW

SDK_J7_06_01_01

J721E

ADASVISION-3868

cpsw - Nimu example aborts when run on A72

CPSW

SDK_J7_06_02_00

J721E

ADASVISION-3936

Assertion in CSI2 Rx driver

CSI2-RX

SDK_J7_06_01_01

J721E

ADASVISION-3691

[CSIRX DRV]capture with 2.5 Gbps DDR lane speed is failing

CSI2-RX

SDK_J7_00_09_00_00

J721E

ADASVISION-3781

VHWA SDE Foco buffers are not aligned

VHWA_SDE

SDK_J7_00_09_01_00

J721E

PDK-4767

QSPI flash writer and diagnostic test failure

BOARD

PDK_J7_01.00.00_RTM

J721E

2.11.8. Known Issues

ID

Head Line

Module

Reported in Release

Affected Platforms

Workaround in this release

ADASVISION-3745

Output mismatch when each region requiring 3 TRs

VHWA_LDC

PDK_J7_01.00.00_RTM

J721E

None

ADASVISION-3747

DMPAC DOF driver doesn’t handle certain SOF case properly

VHWA_DOF

PDK_J7_00.09.01

J721E

This issue is due to shift in flowvector out buffer. While generating the SOF binary map make sure that Paxel rows without any pixel enabled should be in consecutive pair.

ADASVISION-3747

Active DP -> HDMI adapter doesn’t work

DSS

PDK_J7_00.09.01

J721E

Use the display that supports Active DP

PROC_BRDS-658

J7 GESI DB - MAC PORT 0 packet drop seen of 1Gbps Speed

CPSW

PDK_J7_00.09.00_Bringup

J721E

MAC port 0 configured at 100Mbps in J721E EVM alpha version (already taken care in driver)

PROC_BRDS-659

J7 Ethernet expansion board causing interference in the GESI MDIO phys

CPSW

PDK_J7_00.09.00_Bringup

J721E

QSGMII ports should be disabled in J721E EVM alpha version

ADASVISION-3286

Max Length test Tx completion hangs if cpswHostPort maxRxMtu is exceeded

CPSW

PDK_J7_00.09.00_Bringup

J721E

Host core should not send packet more than maxRxMtu

ADASVISION-3287

CPSW MAC loopback fails at RMII mode

CPSW

PDK_J7_00.09.00_Bringup

J721E

None

ADASVISION-3819

CPSW SGMII FIFO loopback fails

CPSW

SDK_J7_06_02_00

J721E

None

ADASVISION-3974

CPSW nimu example app hangs when running on A72

CPSW

SDK_J7_06_02_00

J721E

None

PRSDK-7893

Using PROXY 1 for Pinmux cause crash in SDK use cases

BOARD

PDK_TDA_01.09.00

J721E

Use Proxy 0. (Already taken care in driver)

PRSDK-7892

Noisy output for digital audio diagnostic test

BOARD

PDK_J7_00.09.00_Bringup

J721E

None

PRSDK-7891

CPSW RGMII diagnostic test failure

BOARD

PDK_J7_01.00.00_RTM

J721E

None

ADASVISION-3744

VPAC VISS driver doesn’t support several valid mux combinations for outputs

VHWA_VISS

PDK_J7_00.09.01

J721E

None

ADASVISION-3746

NF de-queue fails after 30 interation

VHWA_NF

PDK_J7_00.09.01

J721E

None

ADASVISION-3754

ipc remote cores does work on 2nd boot

IPC

PDK_J7_00.09.00

J721E

None

ADASVISION-3755

IPC: IPC is not functional in remoteproc mode with current BTCM images

IPC

PDK_J7_00.09.01

J721E

None

PRSDK-8007

IPC does not allow more than one simultaneous core announcement for all cores

IPC

PROCESSOR-SDK_06.01.00

J721E

None

PRSDK-7220

Warning when LEO PMIC is not present

PM

PROCESSOR-SDK_06.01.00

J721E

None

PRSDK-7677

udma dru tests are failing on c66x and c7x

UDMA

PROCESSOR-SDK_06.02.00

J721E

Sample application works. This is a unit test issue

PRSDK-7872

udma HC channel configuration hangs with default parameters

UDMA

PROCESSOR-SDK_06.01.00

J721E

After param init explicitly set burstSize = 0x01 (both Tx and Rx param) and burstSize = 128 (for Tx param)

PRSDK-7747

MCASP_DeviceLoopback_Test: mcaspCreateChan for McASP2 Rx Failed

MCASP

PROCESSOR-SDK_06.02.00

J721E

None

PRSDK-7890

QSPI flash operations are failing in DDR & DMA mode

SPI

PROCESSOR-SDK_06.01.00

J721E

None

2.11.9. Limitations

  • Active DP -> HDMI adapter doesn’t work. As a workaround use the display that supports Active DP