![]() |
SDL API Guide for J721E
|
This file contains the prototypes of the APIs present in the device abstraction layer file of MCRC. This also contains some related macros.
MCRC programming sequence:
MCRC signature generated depends on amount of data copied into PSA register at a time/in single write. Though data pattern can be 8, 16, 32, or 64 bit, data copied into PSA register is always 64 bit wide. If data pattern is less than 64 bit, then it is padded with zeros to make it 64 bit write.
Sub Modules | |
MCRC Data Structures | |
MCRC Enumerated Data Types | |
MCRC Functions | |
MCRC Macros | |
Files | |
file | sdl_mcrc.h |
This file contains the prototypes of the APIs present in the device abstraction layer file of MCRC. This also contains some related macros. | |