4.11. Release notes - 06_01_01¶
4.11.1. Features¶
Note
New features vs previous release are marked in bold
4.11.1.1. Hardware support¶
J721E Alpha and Beta EVM support with Leo PMIC processor board
Fusion1 RevC daughter card with UB960 FPDLink deserializer
IMX390 2MP CSI2 image sensor + UB953 FPDLink serializer
AR0233 2.5MP CSI2 image sensor + UB953 FPDLink serializer
AR0820 8MP CSI2 image sensor + UB953 FPDLink serializer
GESI(Gateway/Ethernet Switch/Industrial) daughter card (for additional ethernet and CAN ports)
Infotainment daughter card (for HDMI output)
4.11.1.2. Software features¶
Important
Below is a summary of key features. Refer individual SDK Components release notes for more details
4.11.1.2.1. Vision Apps (ADAS, Vision, DL demos)¶
OpenVX based demos for ADAS, Vision, deep learning applications
TI-RTOS on C7x, C6x, R5F and Linux on A72
Integrates all major PSDKRA and PSDKLA SW components like TIDL, MMALIB, PDK, OpenVX, OpenGL, video codec, C6x algorithms, imaging/sensors, IPC, Linux, TI-RTOS, SPL/uboot.
Integrates all major HW components like CSI2 camera, eDP/HDMI display, UART, I2C, ethernet, SD card
Deep learning demos
Image Classification demo
Auto valet parking (AVP) demo
semantic segmentation, Parking spot detect and Vehicle detect algorithms
1 channel, 3 algo @ 56 fps mode
3 channel, 3 algo @ 28 fps mode (combined network for parking spot and vehicle detect)
Surround view demos
3D surround view using GPU on 4x 2MP 30fps live camera input
3D surround view calibration application
ADAS/Vision demos
Dense optical flow (DOF) demo
Stereo disparity engine demo
Single and multi camera CSI2RX + VISS + LDC + MSC + Display demo
C7x algorithm offload demo
Perception Toolkit (PTK) Demos
Camera based SFM and occupancy grid mapping using Dense optical flow HW engine
Radar and lidar occupancy grid mapping
Camera SFM, radar, lidar fusion for occupancy grid mapping
OpenVX target nodes
image pre-processing (YUV 2 RGB) nodes for DL demos
image post-processing and visualization nodes for deep learning, DOF, Stereo demos
lidar, radar, camera SFM nodes for PTK demos
OpenGL nodes for surround view
Profiling, logging and other utility APIs
4.11.1.2.2. Gateway Demos¶
CAN-Ethernet gateway demo to showcase P2P (Protocol to Protocol) translation
Full duplex routing between: CAN-to-Ethernet, Ethernet-to-CAN and CAN-to-CAN.
4.11.1.2.3. Platform Development Kit (PDK)¶
RTOS device drivers running on R5F, C6x, C7x, A72
Supported drivers and modules
Board diagnostic library
CPSW (2G and 9G)
CSI2 camera
CSL-FL (Chip support library)
DSS display (eDP and HDMI, BT601 discrete sync mode)
GPIO
I2C
IPC (inter processor communication)
McASP
MMCSD with FATFS (A72 with RTOS)
OSAL
SBL secondary bootloader
SCI Client (DMSC interface)
SPI driver (SPI, QSPI, OSPI, Hyperflash)
UART
UDMA and DRU
VPAC and DMAC (VHWA)
4.11.1.2.4. MCU Software (MCU SW)¶
AutoSAR MCAL driver and demo applications running on R5F
AutoSAR MCAL driver for Adc, Can, CDD IPC,Dio, Eth, Gpt, Pwm, Spi & Wdg
MCU Demo Applications
CAN Profiling Application
CDD IPC Profiling Application
SPI IPC Profiling Application
4.11.1.2.5. TI Deep learning Library (TIDL) and MMALIB¶
TIDL deep learning inference engine library running on C7x/MMA
MMALIB for accelerating convolution, deconvolution layers on MMA (used by TIDL internally)
TIDL network import tool and performance analyzer tool
Supports Caffe, ONXX, TFlite network import formats
Supported layers: Convolution, deconvolution, pooling, ReLU, Elt-wise, Inner product, Soft-max, and many more, refer TIDL user guide (LINK)
Custom / User defined layer Call-back to plugin user specific layers
4.11.1.2.6. TI OpenVX (TIOVX)¶
OpenVX v1.1 compliant implementation with graph pipelining and user data object extension support
OpenVX API on A72 running Linux
OpenVX target kernels on C7x, C6x, R5F, A72
OpenVX v1.1 C6x kernels
OpenVX nodes for
TIDL (C7x)
VISS (R5F)
LDC (R5F)
MSC (multi-scalar) (R5F)
Pyramid (using MSC) (R5F)
BLNF (bilateral noise filter) (R5F)
CSI2 camera (R5F)
Display (eDP and HDMI) (R5F)
Video decode (R5F)
OpenVX tutorials for getting started
PyTIOVX tools for target kernel code generation
4.11.1.2.7. Imaging¶
IMX390 2MP sensor driver (30/60fps) with IQ tuning
AR0233 2.5MP sensor driver with IQ tuning
AR0820 8MP sensor driver with IQ tuning
TI Auto-exposure and auto white-balance algorithms
4.11.1.2.8. Ethernet Switch Firmware (ETHFW)¶
Ethernet switch firmware running on R5F for CPSW9G
Layer 2 switching
NDK integration
Remote switch configuration server
GUI switch configuration tool
Inter VLAN routing
IP next header filtering
Rate limiting
4.11.1.2.9. TI Autonomous Driving Algorithms (TIADALG)¶
Image pre-processing APIs for color plane conversion and separation YUV to RGB for DL applications (C6x optimized)
Camera Pose estimation API using solve pnp technique (C6x optimized)
Visual localization algorithm (C6x optimized)
4.11.1.2.10. Video Codecs¶
Single and multi channel H264 decoder on RTOS R5F
Upto 1080p 30fps resolution, I and I+P frame
NV12 and 8b output
4.11.1.2.11. TI-RTOS¶
SysBIOS for R5F, C6x, C7x, A72
Network developer kit (NDK) on R5F
4.11.1.2.12. Code Gen Tools (CGT)¶
TI Compiler, assembler, linker for R5F, C6x, C7x
GCC compiler for A72 (needs to be downloaded separately)
4.11.2. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Plaform |
---|---|---|---|
J721e |
x86_64 (Linux Ubuntu 18.04) |
R5F, C6x, C7x running TI-RTOS A72 running Linux |
J721e EVM with daughter cards |
PC emulation mode |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
4.11.3. Known Issues¶
Refer to individual SDK Components release notes for known issues in each component